This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: Maximum GPIO source current

Part Number: AM3352


I understand that the GPIO is rated at 6mA and at this level the CMOS voltage threshold spec's are met.

I am interested in an absolute max. spec. I would like to understand what the maximum current the GPIO on the Sitara can source without damage. It does not need to be within its voltage interface spec. in this case.

Thanks,

Brian