This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEVM572X: Design queries

Part Number: TMDSEVM572X
Other Parts Discussed in Thread: AM5728

Hi TI Support,

1. TPS22965DSG has slew rate control with 220pF capacitor in evaluation board while our custom design will have 3100mA on 3.3V through this IC, so do you any slew rate change is required for any power sequencing, etc or 220pF should be fine.

2. We want to interface 16Gb NAND Flash MT29F16G16ADACAH4-IT  as 2GByte X 16 on GPMC, are there any Linux drivers available for that?

3. eMMC NAND flash used in evaluation board is MTFC4GACAJCN-1M WT which is -25'C to +85'C, can we replace directly with -40'C to +85'C P/N: MTFC4GACAJCN-4M IT of any driver changes will be required?

4. How can we implement USB OTG configuration in AM5728, Mux utility tool doesn't shows separate USB_ID pin.?

Thanks,

jagdish