This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/BEAGLEBK: Unable to connect through Remote System Explorer

Part Number: BEAGLEBK

Tool/software: Code Composer Studio

Hi,

I am unable to connect  from CCS through the Remote System Explorer to Beaglebone Black booted from SD card with bone-debian-9.1-lxqt-armhf-2017-08-31-4gb image. I used the default user:password debian:temppwd. I am able to connect though using putty or WinSCP, so the problem is not the connection itself.

If I boot from eMMC (old 3.8 kernel) or from the SD card with the previous image bone-debian-8.6-lxqt-4gb-armhf-2016-11-06-4gb, I can connect with no problem.

I am using Windows 10, and CCS 6.1.0.00104 (I can only use that version)

I wish to use the newer image as it contains the PRU support out of the box.

Adam