Part Number: 66AK2G02
Other Parts Discussed in Thread: FFTLIB, , TMS320C6748, 66AK2G12
We are trying to use this chip for a new DSP project. We need to read data at over 100 Mbytes per second from FPGA (ADC samples).
Bus width should be 16 or 32 bits.
I was wondering if there is any parallel interface which can read at that data rate in this microprocessor?
In this project, we need to do 1 Meg FFT (1024K).
Can we use hte routines in FFTLIB for this CPU?
On the FFTLIB page it says that it works with 66AK2E02 (With "E" not with "G") : http://www.ti.com/tool/FFTLIB
Is it because this library was posted in 2014 before the 66AK2G02 was released?
If it does not wirk with the G02, I would like to know which FFT library works with that CPU?
What is the time required to do 1024K FFT on that processor?