Tool/software: Code Composer Studio
Hi,
My CCS version is 5.2. I'm looking for a dsp library that will be appropriate for C5509A CPU. With the newest one (dsplib 3.0) when i try to use some dsp functions it shouts me an error :
"C:\c55_lp\c55_dsplib_3.00\lib\55xdspx_r3.lib<fir2.obj>" specifies "C55x CPU Rev 3.x", which is not compatible with "C55x CPU Rev 2.x" specified in a previous file or on the command line.
When i specify in a compiler options other device (from v3 revision - eg. 5515) it builds without any problems.
my question is :
1. I cannot get the link of dsplib 2.40 or earilier viersion
2. If I want to use the dsplib 3.00, which sllicon version is better(such as 5505 ,or 5515)