This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Experts,
According to the following document http://focus.ti.com/general/docs/lit/getliterature.tsp?literatureNumber=spraaz3&fileType=pdf the VPFE and VPBE on DM6467 is compatible with that available on DM6446. I would like to confirm if DM6467 supports Alpha Blending?
-Regards
Vallabha
The document you referred to describes compatibility at the software level (codec engine APIs, driver APIs....); however, the hardware back end of DM6467 is quite different than that of DM6446. DM6467 does not have built-in alpha blending capabilities built into the hardware like DM6446
The VDCE on DM6467 supports hardware for 2-bit overlay function. Can the DMAI's Blend functionality support higher bit-depths at the expense of software overhead?