Part Number: 66AK2G02
I have the same question as a previous poster, and the response on the previous thread does not answer my question.
See https://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/613768
The previous poster asked about the voltage levels for a single-ended input to the SYSOSC_IN pin, and the TI employee answered ambiguously, saying that it's a 1.8V input and that it is LVCMOS-compatible. But the LVCMOS family is often used as 3.3V I/O, so it's not very clear to say it's "LVCMOS-compatible."
The problem is that the K2G datasheet SPRS932E says that the pin has 1.8V levels (see the description of ball AC19 in Table 4-1 on page 36) and also that it supports LVCMOS-compatible levels when an external oscillator is used (see Table 4-24 and section 5.9.3.1.2. Indeed, Table 5-14 specifically calls out "3.3V mode" for the pin in the row describing the input current. The mention of "3.3V mode" in table 5-14 and the description of the pin as "LVCMOS-compatible" makes it sound like the pin supports 3.3V levels.
Regards,
Debora