Tool/software: TI-RTOS
I just downloaded and installed the "processor_sdk_rtos_am335x_4_02_00_09" and now I am trying to build the "pdk_am335x_1_0_9" example files and I get a lot of these errors:
Detected Test Project: UART_BasicExample_bbbAM335x_armExampleProject
--------------------------------------------------------------------------------
Creating project 'UART_BasicExample_bbbAM335x_armExampleProject'...
!ERROR: Version 2.21.2.07 (or equivalent) of product-type 'com.ti.uia' is not currently installed!
NOTE: Refer to the following list of available 'com.ti.uia' versions:
2.20.0.02
Copying macro.ini
The system cannot find the path specified.
The problem is that I looked and there is no UIA version 2.21.2.07!
What should I do?
Thanks!