Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI-RTOS
I recently built the Processor SDK TIRTOS PDK 1.0.9 examples with UIA 2.21.02.07 installed.
I opened up the GPIO_LedBlink example, enabled UIA LoggingSetup in Logger stop mode and successfully compiled.
However, when I run the program, pause and try to use RTOS analyzer I get the following error:
"Could not detect a UIA configuration. One of the following is required:
- Either load a program with UIA instrumentation turned on
- Or specify a custom UIA configuration"
I should also note that if I try to use the Runtime Object Viewer I also get the following error:
"Failed to start ROV using 'comm=DSLite:1,wsPort=53331':: Can't extract RTSC configuration package path from 'C:/Users...out"