This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello I am using DM6467 and codec engine version 2.10.02.
My application is video analytics.
In the code, I am running the video analytics algorithm and copy the input frame buff into output frame buff with memcpy function. The code is work fine.
When I use EDMA3 to copy input frame buff into output frame buff instead of memcpy function then code is not working. It is stuck in between. But if I use only the EDAM3 to copy input frame into output frame without running algorithm (only loopback with EDAM3) then its work fine.
some times its work for some n number of frames and then stuck( some times work up to 300, 400 number of frames).
memcpy (that works) and the EDMA3 copy inside the video analytics algorithm and all in the DSP side.
I am using IDMA3.
I am using framework provided library (e.g. ACPY3 start, configure and wait etc..)
I dont know why this happen.
Can anyone help me? What is the problem and how to debug the code.
Regards,
Naresh
This link has some information on common issues leading to hangs, when using ACPY3.
http://processors.wiki.ti.com/index.php/Framework_Components_FAQ#ACPY3_Questions
Thank you for your prompt response gunjan,
I m copying DDR to DDR. both the buffers in external memory. i am not hanging on ACPY3_wait function.
The process hangs immediately after a single transfer is apparently completed (we don’t get a chance to see if it got transferred correctly or not). We have put breakpoints in the code using CCS and a JTAG emulator. We have two such transfers lined up sequentially. The code hits the breakpoints before the ACPY3 params are configured and after the transfer is completed for the 1st one but doesn’t even hit the breakpoint to begin the next transfer.
here is my configuration
var DMAN3 = xdc.useModule('ti.sdo.fc.dman3.DMAN3');
DMAN3.heapInternal = "IRAM";
DMAN3.heapExternal = "DDRALGHEAP";
DMAN3.idma3Internal = false;
DMAN3.scratchAllocFxn = "DSKT2_allocScratch";
DMAN3.scratchFreeFxn = "DSKT2_freeScratch";
// DMAN3 will inclusively manage PaRAMs 78-125, QDMA channels 0-7, tcc's 32-63
DMAN3.paRamBaseIndex = 80;
DMAN3.numPaRamEntries = 48;
DMAN3.numQdmaChannels = 8;
DMAN3.qdmaChannels = [0,1,2,3,4,5,6,7];
DMAN3.tccAllocationMaskL = 0;
DMAN3.tccAllocationMaskH = 0xffffffff;
// DMAN3.trace = true; // false; //true;
DMAN3.trace = false;
/*
* ======== DSKT2 and RMAN Configuration ========
* XDAIS Algorithm Memory and DMA allocation
*/
var DSKT2 = xdc.useModule('ti.sdo.fc.dskt2.DSKT2');
DSKT2.DARAM0 = "IRAM";
DSKT2.DARAM1 = "IRAM";
DSKT2.DARAM2 = "IRAM";
DSKT2.SARAM0 = "IRAM";
DSKT2.SARAM1 = "IRAM";
DSKT2.SARAM2 = "IRAM";
DSKT2.ESDATA = "DDRALGHEAP";
DSKT2.IPROG = "IRAM";
DSKT2.EPROG = "DDR2";
DSKT2.DSKT2_HEAP = "DDR2"; /* to allocate internal DSKT2 object */
DSKT2.trace = false;
DSKT2.debug = false;
DSKT2.DARAM_SCRATCH_SIZES = [ 32768, 16384, 0,0,0,0,0, /* ... */ 0 ];
DSKT2.SARAM_SCRATCH_SIZES = [ 32768, 16384, 0,0,0,0,0, /* ... */ 0 ];
// DSKT2.DARAM_SCRATCH_SIZES = [ 65536, 16384, 0,0,0,0,0, /* ... */ 0 ];
// DSKT2.SARAM_SCRATCH_SIZES = [ 65536, 16384, 0,0,0,0,0, /* ... */ 0 ];
var RMAN = xdc.useModule('ti.sdo.fc.rman.RMAN');
RMAN.useDSKT2 = true;
RMAN.tableSize = 10;
RMAN.semCreateFxn = "Sem_create";
RMAN.semDeleteFxn = "Sem_delete";
RMAN.semPendFxn = "Sem_pend";
RMAN.semPostFxn = "Sem_post";
RMAN.debug = false;
RMAN.trace = false;
var EDMA3 = xdc.useModule('ti.sdo.fc.edma3.Settings');
EDMA3.maxPaRams[0] = 384;
EDMA3.maxTccs[0] = 24; // 49;
EDMA3.maxEdmaChannels[0] = 24; // 49;
EDMA3.maxQdmaChannels[0] = 0;
EDMA3.trace = false; //true;
EDMA3.debug = false; //true;
var EDMA3CHAN = xdc.useModule('ti.sdo.fc.ires.edma3chan.EDMA3CHAN');
EDMA3CHAN.debug = false;
EDMA3CHAN.trace = false;
// handle configuration
dmaTab[i].handle = fcpy->dmaHandle2D[i];
dmaTab[i].numTransfers = 1;
dmaTab[i].numWaits = 1;
dmaTab[i].priority = IDMA3_PRIORITY_LOW; //IDMA3_PRIORITY_HIGH;
dmaTab[i].protocol = &ACPY3_PROTOCOL;
dmaTab[i].persistent = FALSE; //TRUE
Hi Naresh,
Inside your algorithm can you check the and see if the 'env' field of the IDMA3_Handle that you are passing to the ACPY3 functions is an internal memory address?
The 'env' should be allocated in internal memory, and you could get stuck if it has been allocated in external memory due to some configuration issue or running out of internal heap.
Best regards,
Murat
Thank you Murat for your response.
I am new to this DSP DM6467. Can you please guide me how to check t 'env' field of the IDMA3_handle is in internal memory and how to configure it.
here is the .cfg file content of combo module.
Regards,
Naresh
var DMAN3 = xdc.useModule('ti.sdo.fc.dman3.DMAN3');
DMAN3.heapInternal = "IRAM";
DMAN3.heapExternal = "DDRALGHEAP";
DMAN3.idma3Internal = false;
DMAN3.scratchAllocFxn = "DSKT2_allocScratch";
DMAN3.scratchFreeFxn = "DSKT2_freeScratch";
// DMAN3 will inclusively manage PaRAMs 78-125, QDMA channels 0-7, tcc's 32-63
DMAN3.paRamBaseIndex = 80;
DMAN3.numPaRamEntries = 48;
DMAN3.numQdmaChannels = 8;
DMAN3.qdmaChannels = [0,1,2,3,4,5,6,7];
DMAN3.tccAllocationMaskL = 0;
DMAN3.tccAllocationMaskH = 0xffffffff;
// DMAN3.trace = true; // false; //true;
DMAN3.trace = false;
/*
* ======== DSKT2 and RMAN Configuration ========
* XDAIS Algorithm Memory and DMA allocation
*/
var DSKT2 = xdc.useModule('ti.sdo.fc.dskt2.DSKT2');
DSKT2.DARAM0 = "IRAM";
DSKT2.DARAM1 = "IRAM";
DSKT2.DARAM2 = "IRAM";
DSKT2.SARAM0 = "IRAM";
DSKT2.SARAM1 = "IRAM";
DSKT2.SARAM2 = "IRAM";
DSKT2.ESDATA = "DDRALGHEAP";
DSKT2.IPROG = "IRAM";
DSKT2.EPROG = "DDR2";
DSKT2.DSKT2_HEAP = "DDR2"; /* to allocate internal DSKT2 object */
DSKT2.trace = false;
DSKT2.debug = false;
DSKT2.DARAM_SCRATCH_SIZES = [ 32768, 16384, 0,0,0,0,0, /* ... */ 0 ];
DSKT2.SARAM_SCRATCH_SIZES = [ 32768, 16384, 0,0,0,0,0, /* ... */ 0 ];
// DSKT2.DARAM_SCRATCH_SIZES = [ 65536, 16384, 0,0,0,0,0, /* ... */ 0 ];
// DSKT2.SARAM_SCRATCH_SIZES = [ 65536, 16384, 0,0,0,0,0, /* ... */ 0 ];
var RMAN = xdc.useModule('ti.sdo.fc.rman.RMAN');
RMAN.useDSKT2 = true;
RMAN.tableSize = 10;
RMAN.semCreateFxn = "Sem_create";
RMAN.semDeleteFxn = "Sem_delete";
RMAN.semPendFxn = "Sem_pend";
RMAN.semPostFxn = "Sem_post";
RMAN.debug = false;
RMAN.trace = false;
var EDMA3 = xdc.useModule('ti.sdo.fc.edma3.Settings');
EDMA3.maxPaRams[0] = 384;
EDMA3.maxTccs[0] = 24; // 49;
EDMA3.maxEdmaChannels[0] = 24; // 49;
EDMA3.maxQdmaChannels[0] = 0;
EDMA3.trace = false; //true;
EDMA3.debug = false; //true;
var EDMA3CHAN = xdc.useModule
Via a breakpoint in your algorithm, at the point where you call ACPY3_configure (or any other ACPY3 function) look at the fields of the IDMA3_Handle you are passing to the ACPY3 function. The 'env' field is a pointer containing the address of the memory allocated for the handle's env structure, this address must be an internal memory address. So, you should check and make sure this is the case.
Regards, Murat
Naresh850 said:Thank you Murat for your response.
I am new to this DSP DM6467. Can you please guide me how to check t 'env' field of the IDMA3_handle is in internal memory and how to configure it.
here is the .cfg file content of combo module.
Regards,
Naresh
var DMAN3 = xdc.useModule('ti.sdo.fc.dman3.DMAN3');
DMAN3.heapInternal = "IRAM";
DMAN3.heapExternal = "DDRALGHEAP";
DMAN3.idma3Internal = false;
DMAN3.scratchAllocFxn = "DSKT2_allocScratch";
DMAN3.scratchFreeFxn = "DSKT2_freeScratch";
// DMAN3 will inclusively manage PaRAMs 78-125, QDMA channels 0-7, tcc's 32-63
DMAN3.paRamBaseIndex = 80;
DMAN3.numPaRamEntries = 48;
DMAN3.numQdmaChannels = 8;
DMAN3.qdmaChannels = [0,1,2,3,4,5,6,7];
DMAN3.tccAllocationMaskL = 0;
DMAN3.tccAllocationMaskH = 0xffffffff;
// DMAN3.trace = true; // false; //true;
DMAN3.trace = false;
/*
* ======== DSKT2 and RMAN Configuration ========
* XDAIS Algorithm Memory and DMA allocation
*/
var DSKT2 = xdc.useModule('ti.sdo.fc.dskt2.DSKT2');
DSKT2.DARAM0 = "IRAM";
DSKT2.DARAM1 = "IRAM";
DSKT2.DARAM2 = "IRAM";
DSKT2.SARAM0 = "IRAM";
DSKT2.SARAM1 = "IRAM";
DSKT2.SARAM2 = "IRAM";
DSKT2.ESDATA = "DDRALGHEAP";
DSKT2.IPROG = "IRAM";
DSKT2.EPROG = "DDR2";
DSKT2.DSKT2_HEAP = "DDR2"; /* to allocate internal DSKT2 object */
DSKT2.trace = false;
DSKT2.debug = false;
DSKT2.DARAM_SCRATCH_SIZES = [ 32768, 16384, 0,0,0,0,0, /* ... */ 0 ];
DSKT2.SARAM_SCRATCH_SIZES = [ 32768, 16384, 0,0,0,0,0, /* ... */ 0 ];
// DSKT2.DARAM_SCRATCH_SIZES = [ 65536, 16384, 0,0,0,0,0, /* ... */ 0 ];
// DSKT2.SARAM_SCRATCH_SIZES = [ 65536, 16384, 0,0,0,0,0, /* ... */ 0 ];
var RMAN = xdc.useModule('ti.sdo.fc.rman.RMAN');
RMAN.useDSKT2 = true;
RMAN.tableSize = 10;
RMAN.semCreateFxn = "Sem_create";
RMAN.semDeleteFxn = "Sem_delete";
RMAN.semPendFxn = "Sem_pend";
RMAN.semPostFxn = "Sem_post";
RMAN.debug = false;
RMAN.trace = false;
var EDMA3 = xdc.useModule('ti.sdo.fc.edma3.Settings');
EDMA3.maxPaRams[0] = 384;
EDMA3.maxTccs[0] = 24; // 49;
EDMA3.maxEdmaChannels[0] = 24; // 49;
EDMA3.maxQdmaChannels[0] = 0;
EDMA3.trace = false; //true;
EDMA3.debug = false; //true;
var EDMA3CHAN = xdc.useModule
Thanks Marut for your early response.
I test the code as per your guidance and check the memory address of 'env' field .
Please look the below code. THere I mentioned the location of break point.
Void VCA_ALGORITHMS_MT_doCopy2D2D(IDMA3_Handle dmaHandle, Void *in, Void *out, ElemStruct *elem)
{ // first break point
ACPY3_Params params;
/*
* Activate Channel scratch DMA channels.
*/
ACPY3_activate(dmaHandle);
/* Configure the logical channel */
params.transferType = ACPY3_2D2D;
params.srcAddr = (void *)in;
params.dstAddr = (void *)out;
params.elementSize =(elem->LineLength);
params.numElements =(elem->NumLines);
params.numFrames = 1;
params.srcElementIndex = elem->srcLineOffset;
params.dstElementIndex = elem->dstLineOffset;
params.srcFrameIndex = 0;
params.dstFrameIndex = 0;
params.waitId = 0;
/* Configure logical dma channel */
ACPY3_configure(dmaHandle, ¶ms, 0);
/* Use DMA to fcpy input buffer into working buffer */
ACPY3_start(dmaHandle);
/* Check that dma transfer has completed before finishing "processing" */
//secound break point
while (!ACPY3_complete(dmaHandle)) {
;
};
/*
* DeActivate Channel scratch DMA channels.
*/
ACPY3_deactivate(dmaHandle);
}// third break point
Memory address of 'env' field
at Break point 1
memory address of env: 0x8c131cc0 (external memory)
memory address of dmahandle[0]->env: can't load from non primitive location
at Break point 2
memory address of env: 0x118118020 (internal memory)
memory address of dmahandle[0]->env: can not load from non primitive location
at Break point 3
memory address of env: ox8c131cc0 (external memory)
memory address of dmahandle[0]->env: can not load from non primitive location
Now how can i decided the actual memory addres of env field? IS it internal or external?
Can you please guide me in this regard?
thanks
Naresh
Naresh850 said:Thanks Marut for your early response.
I test the code as per your guidance and check the memory address of 'env' field .
Hi Naresh,
Once the channel is activated via ACPY3_activate the 'env' field is assigned an internal memory address, so that doesn't seem to be a problem. I am not sure what the issue is at this point. Are you still stuck with the problem?
Murat
Please look the below code. THere I mentioned the location of break point.
Void VCA_ALGORITHMS_MT_doCopy2D2D(IDMA3_Handle dmaHandle, Void *in, Void *out, ElemStruct *elem)
{ // first break point
ACPY3_Params params;
/*
* Activate Channel scratch DMA channels.
*/
ACPY3_activate(dmaHandle);
/* Configure the logical channel */
params.transferType = ACPY3_2D2D;params.srcAddr = (void *)in;
params.dstAddr = (void *)out;params.elementSize =(elem->LineLength);
params.numElements =(elem->NumLines);
params.numFrames = 1;params.srcElementIndex = elem->srcLineOffset;
params.dstElementIndex = elem->dstLineOffset;params.srcFrameIndex = 0;
params.dstFrameIndex = 0;params.waitId = 0;
/* Configure logical dma channel */
ACPY3_configure(dmaHandle, ¶ms, 0);
/* Use DMA to fcpy input buffer into working buffer */
ACPY3_start(dmaHandle);/* Check that dma transfer has completed before finishing "processing" */
//secound break point
while (!ACPY3_complete(dmaHandle)) {
;
};/*
* DeActivate Channel scratch DMA channels.
*/
ACPY3_deactivate(dmaHandle);}// third break point
Memory address of 'env' fieldat Break point 1
memory address of env: 0x8c131cc0 (external memory)
memory address of dmahandle[0]->env: can't load from non primitive location
at Break point 2
memory address of env: 0x118118020 (internal memory)
memory address of dmahandle[0]->env: can not load from non primitive location
at Break point 3
memory address of env: ox8c131cc0 (external memory)
memory address of dmahandle[0]->env: can not load from non primitive locationNow how can i decided the actual memory addres of env field? IS it internal or external?
Can you please guide me in this regard?
thanks
Naresh
Hi MArut,
Yes, I am still stuck with the problem.
Please do needful ASAP
regards,
NAresh
Can you please show exactly which lines of code get stuck? Perhaps copy/paste your code and highlight put a comment somewhere like "never gets here". I apologize if you already gave that info. I've been hunting through your code but couldn't find it. Does it always get stuck at the same place? Just so I understand correctly, you never hit your breakpoint at all correct, as opposed to hitting the breakpoint but the data not copying correctly?
Hi
Here is the code. I highlited the breakpoint with yellow colour.
After few frames code get stuck at the same place every time.(number of frame is not consistent ). code get stuck so we can not verify the data, its correct or wrong.
#define USE_EDMA
U32 MT_HD (VCA_ALGORITHMS_MT_Obj *obj,XDM1_BufDesc *inBufs, XDM1_BufDesc *outBufs,
VCA_MT_Ext_InArgs *InArgs,
VCA_MT_Ext_OutArgs *OutArgs)
{
U8 *img;
U8 *imguv;
FRAME sOutputframeYUV;
FRAME sOutputframeUV;
//ElemStruct elem,elem_uv; // for edma parameters
ElemStruct elem,elem_uv; // for edma parameters
U8 * restrict pu8ImDiff;
U32 u32FrameHeight, u32FrameWidth;
U16 FrameWidth;
FRAME *psBinaryIpFrame;
FRAME *psBgrndFrame;
FRAME * restrict psTempImage;
U16 *u16RefBgnd;
U8 *ReTrain; //Persistent Variable to indicate automatic retraining of HD
int u32inx;
int u32x1;
int u32x2;
int u32y1;
int u32y2;
int j = 0;
XYCOORDINATES roiCord;
StructComponentBuffer *componentInfo;
StructRegionArea *puRegionAreaInfo;
Strel *puStrel;
ImageStats *psImSt;
U32 u32NActPixels = 0;
U32 u32FrameSize , u32i = 0;//, u32NumFrames = 0;
ROI sRoi, psROI; /* To hold all ROI */
int u32numComps, u32CC;
#ifdef NEW_CC1
stConnectedComponent *psTempImgComponent = NULL;
#else /* NEW_CC1 */
StructImgComponent *psTempImgComponent = NULL;
#endif /* NEW_CC1 */
U32 u32j;
U8 u8Salient = 0;
U32 roi_num = 0; /* roi counter -- Sriraja*/
U32 u32FGperc = 0;
U32 u32Drawflg = 0;
U16 *ps16TempTrain;
U8 *RoiActivity;
/* TW strcuture - Pradeep */
SZ_RoI SZRoI[4];
U16 i = 0;//, j =0;
conf_parameters *conf_data1;
struct RegOfInterest *HD_Rois;
struct RegOfInterest *GID_Rois;
//struct RegOfInterest *TW_Rois;
ROI_DB *SZ_Rois;
ROI_DB *SZ_RoisT;
U8 *image;
U32 u32k = 0;
#ifdef NEW_CC1
stCCUserConfig sConfig;
stCCHandle *psCCHandle;
int s32Ret = 0;
stConnectedComponent *psCCOutNode,*psCCTempNode;
U16 *pu16ScratchBuff;
U8 *buf;
IplImage1 *inpImg;
#endif
U32 u32sizestr = sizeof(StructComponentBuffer);
u32sizestr = sizeof(StructRegionArea);
//////////////////////////////////////////////////////////////////
u32FrameHeight = obj->frameHeight;
u32FrameWidth = obj->frameWidth;
FrameWidth = obj->frameWidth;
u32FrameSize = obj->frameHeight*obj->frameWidth;
conf_data1 = &conf_data[InArgs->confg_param_index];
/*************************************************************************/
/* assigning malloc'ed memory pointers to the frame buffers and structures */
img = (U8 *) inBufs->descs[0].buf;
imguv = (U8 *) inBufs->descs[1].buf;
sOutputframeYUV.u8FrameData = (U8 *)outBufs->descs[0].buf;
sOutputframeUV.u8FrameData = (U8 *)outBufs->descs[1].buf;//v
u16RefBgnd = (U16 *)( obj->HD_Persistent); //persistent
psBgrndFrame = (FRAME *)( (U8 *)u16RefBgnd + sizeof(U16)*u32FrameSize); //persistent
psBgrndFrame->u8FrameData = (U8 *)((U8 *)psBgrndFrame + sizeof(FRAME));
psImSt = (ImageStats *)( (U8*)(psBgrndFrame->u8FrameData) + u32FrameSize); //
#ifdef NEW_CC1
sConfig.s16ConnectivityType = 8; //define connectivity 8 or4
sConfig.s16Foreground = 1; // 1 or 0
sConfig.s32Height = u32FrameHeight;
sConfig.s32Width = u32FrameWidth;
sConfig.u16BitsPerPixel = 1;
sConfig.u16MaxCompAllowed = 2500;
inpImg = (IplImage1*)((U8*)psImSt + 24);
inpImg->imageData = (char*)((U8*)inpImg + 256);
pu16ScratchBuff = (U16*)((U8*)inpImg->imageData + (u32FrameHeight * u32FrameWidth));
inpImg->height = u32FrameHeight;
inpImg->width = u32FrameWidth;
inpImg->widthStep = u32FrameWidth;
inpImg->imageSize = u32FrameWidth * u32FrameHeight;
buf = (U8*)pu16ScratchBuff + (u32FrameHeight * (u32FrameWidth<<2) );
s32Ret = mt_cc_CreateHandle(&sConfig,&psCCHandle, buf);
if(s32Ret != ROK)
{
DEBUG_PRINT("<- mt_cc_CreateHandle: Connected component handle Failed");
return s32Ret;
}
buf = buf + (120252 + (u32FrameHeight * (u32FrameWidth<<1) ));
// Initialize output node pointer with Head node
psCCOutNode = psCCHandle->psCtrlNode->psCCHeadNext[0];
#endif
#ifdef REMOVE_BOX
#ifdef NEW_CC1
ps16TempTrain = (U16 *)buf;
#else
ps16TempTrain = (U16 *)((U8*)puRegionAreaInfo + sizeof(StructRegionArea));
#endif
#endif
#if 1
/* settings ROIs for HD , GID and SZ */
HD_Rois = (struct RegOfInterest *)obj->ROI_Persistent;
GID_Rois = (struct RegOfInterest *) ((U8*)(obj->ROI_Persistent) + 400*1);
SZ_Rois = (ROI_DB *) ((U8*)(obj->ROI_Persistent) + 400*2);
RoiActivity = (U8*)GID_Rois+308;
ReTrain = (U8 *)GID_Rois+340;
#endif
image = (U8 *)(obj->scratch);
psBinaryIpFrame = (FRAME *)(image + u32FrameSize);
psBinaryIpFrame->u8FrameData = (U8 *)((U8 *)psBinaryIpFrame + sizeof(FRAME));
pu8ImDiff = (U8 *)((U8*)psBinaryIpFrame->u8FrameData + u32FrameSize );
memset(pu8ImDiff, 0, u32FrameSize);
psTempImage = (FRAME *)(pu8ImDiff + u32FrameSize);
psTempImage->u8FrameData = (U8 *)((U8 *)psTempImage + sizeof(FRAME));
SCRATCH_2 = (U8*)(psTempImage->u8FrameData ) + u32FrameSize;
SCRATCH_3 = SCRATCH_2 + (sizeof(U8) * (u32FrameSize +12));
SCRATCH_6 = (U16*)(SCRATCH_3 + (sizeof(U8*) * u32FrameHeight));
/*************************************************************************/
/* memory allocated for Sterile zone */
//image = (U8 *)(obj->scratch);
puStrel = (Strel *)SCRATCH_3;
puStrel->u32SizeX = 4;
puStrel->u32SizeY = 9;
puStrel->u8StrelData = NULL;
/***********************
* frame to draw activity
************************/
psBinaryIpFrame->u32FrameHeight = u32FrameHeight;
psBinaryIpFrame->u32FrameWidth = u32FrameWidth;
psTempImage->u32FrameHeight = u32FrameHeight;
psTempImage->u32FrameWidth = u32FrameWidth;
psBgrndFrame->u32FrameHeight = u32FrameHeight;
psBgrndFrame->u32FrameWidth = u32FrameWidth;
// Replaced static variable "u32PrevFrCnt" with persistent structure member
u32i = InArgs->u32Frameno - psImSt->u32PrevFrCnt;
psImSt->u32Threshold = u32thresh[InArgs->light_sensitivity_index];
if(1 == InArgs->scene_changed)
{
/* Copied from new version */
memset(psBgrndFrame->u8FrameData, 0, u32FrameSize);
memset(u16RefBgnd, 0, sizeof(U16)*u32FrameSize);
HD_FrameMean(psBgrndFrame, psImSt);
if(InArgs->u32Frameno > 0)
{
/* Size 48116 is the size of memories for componentInfo and puRegionAreaInfo buffers */
memset(componentInfo, 0, 48116);
psImSt->u32PrevFrCnt = InArgs->u32Frameno;
}
return 0;
}
if( (u32i % HD_FRAME_EXEC_RATE) == 0)
{
if (HD_Rois->u32NumCordinates == 0) /* Default case */
{
sRoi.Cord[0].u32x1 = 0;
sRoi.Cord[0].u32y1 = 0;
sRoi.Cord[0].u32x2 = (u32FrameWidth - 1);
sRoi.Cord[0].u32y2 = (u32FrameHeight - 1);
sRoi.u32NumCordinates = 0;
}
else
{
for (roi_num=0;roi_num < HD_Rois->u32NumCordinates;roi_num++)
{
sRoi.Cord[roi_num].u32x1 = HD_Rois->Cord[roi_num].u32x1;
sRoi.Cord[roi_num].u32x2 = HD_Rois->Cord[roi_num].u32x2;
sRoi.Cord[roi_num].u32y1 = HD_Rois->Cord[roi_num].u32y1;
sRoi.Cord[roi_num].u32y2 = HD_Rois->Cord[roi_num].u32y2;
}
sRoi.u32NumCordinates = HD_Rois->u32NumCordinates;
}
}/* if( (u32i % HD_FRAME_EXEC_RATE) == 0) */
#ifdef USE_EDMA
elem.LineLength = obj->frameWidth;
elem.NumLines = obj->frameHeight;
elem.srcLineOffset = obj->frameWidth;
elem.dstLineOffset = obj->frameWidth;
elem_uv.LineLength = obj->frameWidth;
elem_uv.NumLines = obj->frameHeight/2;
elem_uv.srcLineOffset = obj->frameWidth;
elem_uv.dstLineOffset = obj->frameWidth;
VCA_ALGORITHMS_MT_doCopy2D2D(dmaHandle2D[0],(U8 *)inBufs->descs[0].buf,(U8 *) outBufs->descs[0].buf,&elem);
VCA_ALGORITHMS_MT_doCopy2D2D(dmaHandle2D[0],(U8 *)inBufs->descs[1].buf,(U8 *) outBufs->descs[1].buf,&elem_uv);
#else
memcpy(sOutputframeYUV.u8FrameData, img, u32FrameSize);
memcpy(sOutputframeUV.u8FrameData, imguv, (u32FrameSize)>>1);
#endif
if( (u32i % AD_FRAME_EXEC_RATE) == 0)
{ /* TBD = to include counting of active pixels (u32NActPixels)*/
u32NActPixels = HD_VOIDDiffUpdate (img, //this is "inargs-buff" //forth breakpoint is oppining brace of this function. Never gets here
pu8ImDiff,
psBgrndFrame,
&sRoi,
psImSt,
u16RefBgnd,//Aug removed psRefBgnd
psTempImage,
ps16TempTrain,
conf_data1->thr_re_train,
u32i //Aug added
);
}/* if( (u32i % AD_FRAME_EXEC_RATE) == 0) */
}// end of function
This is the EDMA transfer call.
Void VCA_ALGORITHMS_MT_doCopy2D2D(IDMA3_Handle dmaHandle, Void *in, Void *out, ElemStruct *elem)
{ // first break point
ACPY3_Params params;
/*
* Activate Channel scratch DMA channels.
*/
ACPY3_activate(dmaHandle);
/* Configure the logical channel */
params.transferType = ACPY3_2D2D;
params.srcAddr = (void *)in;
params.dstAddr = (void *)out;
params.elementSize =(elem->LineLength);
params.numElements =(elem->NumLines);
params.numFrames = 1;
params.srcElementIndex = elem->srcLineOffset;
params.dstElementIndex = elem->dstLineOffset;
params.srcFrameIndex = 0;
params.dstFrameIndex = 0;
params.waitId = 0;
/* Configure logical dma channel */
ACPY3_configure(dmaHandle, ¶ms, 0);
/* Use DMA to fcpy input buffer into working buffer */
ACPY3_start(dmaHandle);
/* Check that dma transfer has completed before finishing "processing" */
//secound break point
while (!ACPY3_complete(dmaHandle)) {
;
};
/*
* DeActivate Channel scratch DMA channels.
*/
ACPY3_deactivate(dmaHandle);
}// third break point
Thanks
Naresh
I don't see anything that jumps out with your EDMA code. Based on the fact that it fails after a random number of frames I suspect something like a stack overflow, etc. You should go through some of the steps listed here:
http://processors.wiki.ti.com/index.php?title=DSP_BIOS_Debugging_Tips
Hello Brad,
As per your guidence, I check the stacks in the CCS. but there is no any stack obverflow occured.
Still stuck with the same problem.
plz guide me furthere.
regards,
Naresh
The Codec Engine and Framework Components you are using are 2.5 years old. Please update to the latest version as there have been numerous bug fixes in that time. Note that dsplink is no longer bundled as part of Codec Engine so you'll need download that too. The latest versions can be downloaded here.