This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: GP EVM camera question

Part Number: AM5728

Hello,

        How can i use camera to capture image or video using AM5728 EVM board.

        I have tried to use camera by sending some command from console terminal.

        You can check the command as below:

         root@am57xx-evm:~# /usr/share/qt5/examples/multimediawidgets/camera/camera

        You can also check debug print of console terminal as below:

        (camera:1381): GStreamer-CRITICAL **: gst_pad_get_current_caps: assertion 'GST_IS_PAD (pad)' failed

(camera:1381): GLib-GObject-CRITICAL **: g_object_set: assertion 'G_IS_OBJECT (object)' failed

(camera:1381): GLib-GObject-CRITICAL **: g_object_set: assertion 'G_IS_OBJECT (object)' failed

Using Wayland-EGL

wlpvr: PVR Services Initialised

CameraBin error: "GStreamer error: negotiation problem."

Unable to query the parameter info: "Inappropriate ioctl for dev[ 2039.957406] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1 ice"

Unable to query the parameter info: "Inappropriate ioctl for device"

Unable to query the parameter info: "Inappropriate ioctl for device"

Unable to query the parameter info: "Inappropriate ioctl for device"

Unable to query the parameter info: "Inappropriate ioctl for device"

Unable to query the parameter info: "Inappropriate ioctl for device"

CameraBin error: "Internal data flow error."

      On the LCD,i can see one push button to capture image.

      But it is not visible properly(disable). Means i can not press it.

    If any configuration or some other commands to use camera device.Let me inform.

Thanks in advance.