Part Number: 66AK2H14
Other Parts Discussed in Thread: UCD9244, , TPS53659, UCD9244-EP, LM10011, UCD74120, TPS544C25
Hello, I would like to get some more information on how implement the Smart Reflex on the 66AK2H14 processor. I have looked at the schematics for the EVM board and see that they use two UCD9244 devices page 40 and 41. I can understand page 40 but not page 41. On page 41 the UCD9244 has it VID pins tide to VCC3V3_AUX and I don't see how that is functioning as a Smart Reflex. Can some one clear that up for me and is this the only Smart Reflex implementation for the 66AK2H14?
I have look at the Hardware Design Guide for KeyStone II Devices pages 10 - 14 and see other implementations of the Smart Reflex that see easier to understand than the 66AK2H14 EVM schematics. I think once I understand page 41 in the schematics things may be better understood.
Thanks,
Joe