This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Pin drive strength

Part Number: AM5728

Hi,

I would like to know the pin drive strength of AM5728.

I already asked this in my previous thread (https://e2e.ti.com/support/arm/sitara_arm/f/791/t/666206 ). And I got some information.

But I need more information regarding "Idrive" parameter.



My customer would like to know "Idrive" . What is "Idrive" used to describe what parameters?

In AM5728 DM, Table 5-17, "Idrive" is written in the below.

"Pin Drive strength at PAD Voltage = 0.45V or VDDS-0.45V"

In datil, where is "PAD voltage" ?

Idrvie =6 mA (min.) with PAD voltage =0.45V or VDDS-0.45V, does this current value shows for each pin? Or does it shows total current value for all pins using same VDDS?

I think this pin is not needed to have the buffer if it is used as 6mA source. Is my understanding right?

Please advise me.

I appreciate your quick reply.


Best regards,
Michi