Part Number: TMS320C5534
Tool/software: TI-RTOS
Hello,
I am trying to hook the Timer1 interrupt (of a C55x) to an HWI of DSP/BIOS.
As my system already uses the HW_INT8 for the DMA interrupts, i first used the same construct but this time with HW_INT4
for the timer interrupt. It didnt work, as if the tconf was not happy with HW_INT4. Then, in some DSP/BIOS doc (refman), i understood
this has to be HW_TINT ..... but this also didnt succeeded. Basically i always get the same tconf error
"cannot assign "fxn' of undefined to timerHwiHandler (this is my handler).
Note also that, i am under Linux, so cannot use the graphical gconf under windows.
Is there anything special with Timer1 ?
Thanks,
Jacques