Part Number: AM3358
Other Parts Discussed in Thread: AM3352, TPS65910
Tool/software: Linux
Hello, I am newbie here.
We developed the custom board based on AM335x board. Everything run well. But after a random amount of time, CPU freezed without any log.
Platform: AM335x
SDK: TI processor SDK 04.02.00.09
OSC0 frequency: 24M Hz.
DDR frequency: 400M Hz.
W followed this article: processors.wiki.ti.com/.../Sitara_Linux_Training:_Tuning_the_DDR3_Timings_on_BeagleBoneBlack
We used kingston's D2516EC4BXGGB 4G bits DDR3L SDRAM which is used by Beagle Bone Black.
We attched DDR3L schematics.
DS_CBN_CORE_R0.1_17.08.25-1.pdf
P.S The odd things is that the custom board is working without freezing if OSC0 frequency is 24M Hz but SYSBOOT[15:14] is 26MHz.
I would appreciate your advice.