This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA3XEVM: Usecase generator in Radar SDK 3.03

Expert 7040 points
Part Number: TDA3XEVM

Hi Experts,

 

When I run usecase generator (vsdk_win32.exe) in Radar SDK 3.03, I see the following error message:

  

 

Pre-built usecase generator in Radar SDK 3.02 works well on my PC. Do you have a plan to release 64-bit compatible version for Radar SDK 3.03?

 

Best regards,

Ken

  • Hi Ken,

    We can plan to add out of box support for the 64 bit build from the next release onwards. For now, you can also build a 64 bit version of the code. The source code is available in PROCESSOR_SDK_RADAR_03_03_00_00\vision_sdk\apps\tools\vision_sdk_usecase_gen

    Thanks and Regards,
    Piyali