Part Number: TDA2
Tool/software: Linux
Hello,
We wanted to use the network_tx tool and therefore we tried to set a static IPv4 address for the Board.
We followed the instructions in the "VisionSDK_UserGuide_NetworkTools" userguide, but still the board only has a local link IPv6 address (fe80::...).
In the file .../vision_sdk/links_fw/src/rtos/bios_app_common/tda2xx/cfg/NDK_config.cfg we set var enableStaticIP = 1 and modified
if (enableStaticIP)
{
/* Settings for static IP configuration */
Ip.address = "192.168.1.200";
Ip.mask = "255.255.255.0";
Ip.gatewayIpAddr = "192.168.1.1";
Ip.ifIdx = 1;
}
After the board has booted we logged in as root and started the script vision_sdk_demo.sh. Then we used the given function to show the ip address but no ip was shown. With the command "ip addr show" we found out the board had still an IPv6 address.
We are using the VisionSDK version 03.02.00 on linux in a virtual machine on windows and use teraterm (on the windows host os) for the communication with the board.
Kind Regards and thanks
P.s. We are completely new to work with EVM from TI and vision_sdk etc. We use it for a study project.