Part Number: AM4377
Other Parts Discussed in Thread: AM4372
Tool/software: Linux
Dear Sir:
We make AM437X StarterKit EVM as reference board.
we use SDK ti-processor-sdk-linux-am437x-evm-04.03.00.05-Linux-x86-Install.bin
our custom board use gmii1 connected to PHY IC RTL8201F. Now it is eth0 interface, it is ok to ping PC via eth0.
our custom board use rgmii2 connected to PHY IC RTL8211F.Now it is eth1 interface. it fail to ping PC via eth1. we check the detail info.
we ping PC from target board. it can send ARP request to PC, PC receive the ARP Request, then reply to target board via eth1.
but board can't get any packet. RX show no any packets.
please help to show your advice. thank you very mcuh.
our device tree configuration as below:
am4372.dtsi
mac: ethernet@4a100000 {
compatible = "ti,am4372-cpsw","ti,cpsw";
reg = <0x4a100000 0x800
0x4a101200 0x100>;
interrupts = <GIC_SPI 40 IRQ_TYPE_LEVEL_HIGH
GIC_SPI 41 IRQ_TYPE_LEVEL_HIGH
GIC_SPI 42 IRQ_TYPE_LEVEL_HIGH
GIC_SPI 43 IRQ_TYPE_LEVEL_HIGH>;
#address-cells = <1>;
#size-cells = <1>;
ti,hwmods = "cpgmac0";
clocks = <&cpsw_125mhz_gclk>, <&cpsw_cpts_rft_clk>,
<&dpll_clksel_mac_clk>;
clock-names = "fck", "cpts", "50mclk";
assigned-clocks = <&dpll_clksel_mac_clk>;
assigned-clock-rates = <50000000>;
status = "disabled";
cpdma_channels = <8>;
ale_entries = <1024>;
bd_ram_size = <0x2000>;
mac_control = <0x20>;
slaves = <2>;
active_slave = <0>;
cpts_clock_mult = <0x80000000>;
cpts_clock_shift = <29>;
ranges;
syscon = <&scm_conf>;
davinci_mdio: mdio@4a101000 {
compatible = "ti,am4372-mdio","ti,cpsw-mdio","ti,davinci_mdio";
reg = <0x4a101000 0x100>;
#address-cells = <1>;
#size-cells = <0>;
ti,hwmods = "davinci_mdio";
bus_freq = <1000000>;
status = "disabled";
};
cpsw_emac0: slave@4a100200 {
/* Filled in by U-Boot */
mac-address = [ 00 00 00 00 00 00 ];
};
cpsw_emac1: slave@4a100300 {
/* Filled in by U-Boot */
mac-address = [ 00 00 00 00 00 00 ];
};
phy_sel: cpsw-phy-sel@44e10650 {
compatible = "ti,am43xx-cpsw-phy-sel";
reg= <0x44e10650 0x8>;
reg-names = "gmii-sel";
};
};
am437x-sk-evm.dts
cpsw_default: cpsw_default {
pinctrl-single,pins = <
/* Slave 1 */
AM4372_IOPAD(0x92c, PIN_INPUT_PULLUP | MUX_MODE0) /* mii1_txclk.gmii1_txclk */
AM4372_IOPAD(0x914, PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* mii1_txen.gmii1_txen */
AM4372_IOPAD(0x928, PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* mii1_txd0.gmii1_txd0 */
AM4372_IOPAD(0x924, PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* mii1_txd1.gmii1_txd1 */
AM4372_IOPAD(0x920, PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* mii1_txd0.gmii1_txd2 */
AM4372_IOPAD(0x91c, PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* mii1_txd1.gmii1_txd3 */
AM4372_IOPAD(0x930, PIN_INPUT_PULLUP | MUX_MODE0) /* mii1_rxclk.gmii1_rcclk */
AM4372_IOPAD(0x918, PIN_INPUT_PULLUP | MUX_MODE0) /* mii1_rxdv.gmii1_rxdv */
AM4372_IOPAD(0x940, PIN_INPUT_PULLUP | MUX_MODE0) /* mii1_rxd0.gmii1_rxd0 */
AM4372_IOPAD(0x93c, PIN_INPUT_PULLUP | MUX_MODE0) /* mii1_rxd1.gmii1_rxd1 */
AM4372_IOPAD(0x938, PIN_INPUT_PULLUP | MUX_MODE0) /* mii1_rxd0.gmii1_rxd2 */
AM4372_IOPAD(0x934, PIN_INPUT_PULLUP | MUX_MODE0) /* mii1_rxd1.gmii1_rxd3 */
AM4372_IOPAD(0x90c, PIN_INPUT_PULLUP | MUX_MODE0) /* mii1_crs.gmii1_crs */
AM4372_IOPAD(0x910, PIN_INPUT_PULLUP | MUX_MODE0) /* mii1_rxerr.gmii1_rxer */
AM4372_IOPAD(0x908, PIN_INPUT_PULLUP | MUX_MODE0) /* mii1_col.gmii1_col */
/* Slave 2 */
AM4372_IOPAD(0x858, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a6.rgmii2_tclk */
AM4372_IOPAD(0x840, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a0.rgmii2_tctl */
AM4372_IOPAD(0x854, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a5.rgmii2_td0 */
AM4372_IOPAD(0x850, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a4.rgmii2_td1 */
AM4372_IOPAD(0x84c, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a3.rgmii2_td2 */
AM4372_IOPAD(0x848, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a2.rgmii2_td3 */
AM4372_IOPAD(0x85c, PIN_INPUT_PULLUP | MUX_MODE2) /* gpmc_a7.rgmii2_rclk */
AM4372_IOPAD(0x844, PIN_INPUT_PULLUP | MUX_MODE2) /* gpmc_a1.rgmii2_rtcl */
AM4372_IOPAD(0x86c, PIN_INPUT_PULLUP | MUX_MODE2) /* gpmc_a11.rgmii2_rd0 */
AM4372_IOPAD(0x868, PIN_INPUT_PULLUP | MUX_MODE2) /* gpmc_a10.rgmii2_rd1 */
AM4372_IOPAD(0x864, PIN_INPUT_PULLUP | MUX_MODE2) /* gpmc_a9.rgmii2_rd2 */
AM4372_IOPAD(0x860, PIN_INPUT_PULLUP | MUX_MODE2) /* gpmc_a8.rgmii2_rd3 */
>;
};
cpsw_sleep: cpsw_sleep {
pinctrl-single,pins = <
/* Slave 1 reset value */
AM4372_IOPAD(0x92c, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x914, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x928, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x924, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x920, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x91c, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x930, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x918, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x940, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x93c, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x938, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x934, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x90c, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x910, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x908, PIN_INPUT_PULLDOWN | MUX_MODE7)
/* Slave 2 reset value */
AM4372_IOPAD(0x858, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x840, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x854, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x850, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x84c, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x848, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x85c, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x844, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x86c, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x868, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x864, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x860, PIN_INPUT_PULLDOWN | MUX_MODE7)
>;
};
davinci_mdio_default: davinci_mdio_default {
pinctrl-single,pins = <
/* MDIO */
AM4372_IOPAD(0x948, PIN_INPUT | SLEWCTRL_FAST | MUX_MODE0) /* mdio_data.mdio_data */
AM4372_IOPAD(0x94c, PIN_OUTPUT | MUX_MODE0) /* mdio_clk.mdio_clk */
>;
};
davinci_mdio_sleep: davinci_mdio_sleep {
pinctrl-single,pins = <
/* MDIO reset value */
AM4372_IOPAD(0x948, PIN_INPUT_PULLDOWN | MUX_MODE7)
AM4372_IOPAD(0x94c, PIN_INPUT_PULLDOWN | MUX_MODE7)
>;
};
&mac {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&cpsw_default>;
pinctrl-1 = <&cpsw_sleep>;
dual_emac = <1>;
status = "okay";
};
&davinci_mdio {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&davinci_mdio_default>;
pinctrl-1 = <&davinci_mdio_sleep>;
status = "okay";
};
&cpsw_emac0 {
phy_id = <&davinci_mdio>, <1>;
phy-mode = "mii";
dual_emac_res_vlan = <1>;
};
&cpsw_emac1 {
phy_id = <&davinci_mdio>, <4>;
phy-mode = "rgmii";
dual_emac_res_vlan = <2>;
};
Debug info as below:
root@am437x-evm:~# ifconfig
eth0 Link encap:Ethernet HWaddr 60:64:05:5D:3F:69
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:139
eth1 Link encap:Ethernet HWaddr 60:64:05:5D:3F:6B
inet addr:192.168.1.4 Bcast:192.168.1.255 Mask:255.255.255.0
inet6 addr: fe80::6264:5ff:fe5d:3f6b%763860/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:132 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:23546 (22.9 KiB)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1%763860/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:14130 errors:0 dropped:0 overruns:0 frame:0
TX packets:14130 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1
RX bytes:1075424 (1.0 MiB) TX bytes:1075424 (1.0 MiB)
root@am437x-evm:~# ethtool eth1
Settings for eth1:
Supported ports: [ TP MII ]
Supported link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
1000baseT/Full
Supported pause frame use: No
Supports auto-negotiation: Yes
Advertised link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
1000baseT/Full
Advertised pause frame use: No
Advertised auto-negotiation: Yes
Link partner advertised link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
Link partner advertised pause frame use: Symmetric
Link partner advertised auto-negotiation: Yes
Speed: 100Mb/s
Duplex: Full
Port: MII
PHYAD: 4
Transceiver: external
Auto-negotiation: on
Supports Wake-on: d
Wake-on: d
Current message level: 0x00000000 (0)
Link detected: yes
root@am437x-evm:~# ethtool -S eth1
NIC statistics:
Good Rx Frames: 0
Broadcast Rx Frames: 0
Multicast Rx Frames: 0
Pause Rx Frames: 0
Rx CRC Errors: 0
Rx Align/Code Errors: 337
Oversize Rx Frames: 0
Rx Jabbers: 0
Undersize (Short) Rx Frames: 0
Rx Fragments: 0
Rx Octets: 0
Good Tx Frames: 132
Broadcast Tx Frames: 81
Multicast Tx Frames: 51
Pause Tx Frames: 0
Deferred Tx Frames: 0
Collisions: 0
Single Collision Tx Frames: 0
Multiple Collision Tx Frames: 0
Excessive Collisions: 0
Late Collisions: 0
Tx Underrun: 0
Carrier Sense Errors: 0
Tx Octets: 24074
Rx + Tx 64 Octet Frames: 59
Rx + Tx 65-127 Octet Frames: 226
Rx + Tx 128-255 Octet Frames: 129
Rx + Tx 256-511 Octet Frames: 55
Rx + Tx 512-1023 Octet Frames: 0
Rx + Tx 1024-Up Octet Frames: 0
Net Octets: 70621
Rx Start of Frame Overruns: 0
Rx Middle of Frame Overruns: 0
Rx DMA Overruns: 0
Rx DMA chan 0: head_enqueue: 1
Rx DMA chan 0: tail_enqueue: 127
Rx DMA chan 0: pad_enqueue: 0
Rx DMA chan 0: misqueued: 0
Rx DMA chan 0: desc_alloc_fail: 0
Rx DMA chan 0: pad_alloc_fail: 0
Rx DMA chan 0: runt_receive_buf: 0
Rx DMA chan 0: runt_transmit_bu: 0
Rx DMA chan 0: empty_dequeue: 0
Rx DMA chan 0: busy_dequeue: 0
Rx DMA chan 0: good_dequeue: 0
Rx DMA chan 0: requeue: 0
Rx DMA chan 0: teardown_dequeue: 0
Tx DMA chan 0: head_enqueue: 132
Tx DMA chan 0: tail_enqueue: 0
Tx DMA chan 0: pad_enqueue: 0
Tx DMA chan 0: misqueued: 0
Tx DMA chan 0: desc_alloc_fail: 0
Tx DMA chan 0: pad_alloc_fail: 0
Tx DMA chan 0: runt_receive_buf: 0
Tx DMA chan 0: runt_transmit_bu: 35
Tx DMA chan 0: empty_dequeue: 132
Tx DMA chan 0: busy_dequeue: 0
Tx DMA chan 0: good_dequeue: 132
Tx DMA chan 0: requeue: 0
Tx DMA chan 0: teardown_dequeue: 0
root@am437x-evm:~#