Part Number: TDA3XEVM
Tool/software: Code Composer Studio
Hello,
We have enabled the network_rx_tx app to work with the network_rx tool in the SDK. But we are getting the following error when we run it. What is going wrong?
[IPU1-0] 569.371378 s: Chains: Using TFDTP. Ensure using ��–-usetfdtp with network tools..
[IPU1-0] 569.394131 s: CAPTURE: Create in progress !!!
[IPU1-0] 569.394314 s: CAPTURE: VIP1 Slice0 PortA capture mode is [ 8-bit] !!!
[IPU1-0] 569.394436 s: captdrv/src/vpsdrv_capturePriv.c @ Line 266:
[IPU1-0] 569.394528 s: Invalid number of streams(0) - Supported max streams 8
[IPU1-0] 569.394619 s: Assertion @ Line: 548 in captureLink_drv.c: pInst->captureVipHandle != NULL : failed !!!
-siddarth