Part Number: BEAGLEBK
Tool/software: Linux
Hello,
I'm trying to put my BeagleBone Black into 24-bit LCD mode, but it isn't working. Instead, I get 16-bit mode. I'm driving an all Red test pattern and get all Blue on screen due to the Sitara Errata notes in 3.1.1. If the Sitara would go into 24-bit mode, I should have the correct color. I have also probed the LCD lines and found that only LCD_Data0 - LCD_Data15 are active.
I am running Kernel 4.9.79 from the Processor SDK.
Here is my Device Tree, shouldn't this put it into 24-bit mode?
/dts-v1/;
#include "am33xx.dtsi"
#include "am335x-bone-common.dtsi"
#include <dt-bindings/display/tda998x.h>
/ {
model = "TI AM335x BeagleBone Black";
compatible = "ti,am335x-bone-black", "ti,am335x-bone", "ti,am33xx";
};
&ldo3_reg {
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
regulator-always-on;
};
&mmc1 {
vmmc-supply = <&vmmcsd_fixed>;
};
&mmc2 {
vmmc-supply = <&vmmcsd_fixed>;
pinctrl-names = "default";
pinctrl-0 = <&emmc_pins>;
bus-width = <8>;
status = "okay";
};
&cpu0_opp_table {
/*
* All PG 2.0 silicon may not support 1GHz but some of the early
* BeagleBone Blacks have PG 2.0 silicon which is guaranteed
* to support 1GHz OPP so enable it for PG 2.0 on this board.
*/
oppnitro@1000000000 {
opp-supported-hw = <0x06 0x0100>;
};
};
&am33xx_pinmux {
lcd_pins: lcd_pins {
pinctrl-single,pins = <
AM33XX_IOPAD(0x8a0, PIN_OUTPUT | MUX_MODE0) /* lcd_data0.lcd_data0 */
AM33XX_IOPAD(0x8a4, PIN_OUTPUT | MUX_MODE0) /* lcd_data1.lcd_data1 */
AM33XX_IOPAD(0x8a8, PIN_OUTPUT | MUX_MODE0) /* lcd_data2.lcd_data2 */
AM33XX_IOPAD(0x8ac, PIN_OUTPUT | MUX_MODE0) /* lcd_data3.lcd_data3 */
AM33XX_IOPAD(0x8b0, PIN_OUTPUT | MUX_MODE0) /* lcd_data4.lcd_data4 */
AM33XX_IOPAD(0x8b4, PIN_OUTPUT | MUX_MODE0) /* lcd_data5.lcd_data5 */
AM33XX_IOPAD(0x8b8, PIN_OUTPUT | MUX_MODE0) /* lcd_data6.lcd_data6 */
AM33XX_IOPAD(0x8bc, PIN_OUTPUT | MUX_MODE0) /* lcd_data7.lcd_data7 */
AM33XX_IOPAD(0x8c0, PIN_OUTPUT | MUX_MODE0) /* lcd_data8.lcd_data8 */
AM33XX_IOPAD(0x8c4, PIN_OUTPUT | MUX_MODE0) /* lcd_data9.lcd_data9 */
AM33XX_IOPAD(0x8c8, PIN_OUTPUT | MUX_MODE0) /* lcd_data10.lcd_data10 */
AM33XX_IOPAD(0x8cc, PIN_OUTPUT | MUX_MODE0) /* lcd_data11.lcd_data11 */
AM33XX_IOPAD(0x8d0, PIN_OUTPUT | MUX_MODE0) /* lcd_data12.lcd_data12 */
AM33XX_IOPAD(0x8d4, PIN_OUTPUT | MUX_MODE0) /* lcd_data13.lcd_data13 */
AM33XX_IOPAD(0x8d8, PIN_OUTPUT | MUX_MODE0) /* lcd_data14.lcd_data14 */
AM33XX_IOPAD(0x8dc, PIN_OUTPUT | MUX_MODE0) /* lcd_data15.lcd_data15 */
/* elinux.org/24bit_LCD_for_BBB */
0x3c 0x09 /* lcd_data16.lcd_data16, OMAP_MUX_MODE1 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0x38 0x09 /* lcd_data17.lcd_data17, OMAP_MUX_MODE1 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0x34 0x09 /* lcd_data18.lcd_data18, OMAP_MUX_MODE1 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0x30 0x09 /* lcd_data19.lcd_data19, OMAP_MUX_MODE1 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0x2c 0x09 /* lcd_data20.lcd_data20, OMAP_MUX_MODE1 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0x28 0x09 /* lcd_data21.lcd_data21, OMAP_MUX_MODE1 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0x24 0x09 /* lcd_data22.lcd_data22, OMAP_MUX_MODE1 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
0x20 0x09 /* lcd_data23.lcd_data23, OMAP_MUX_MODE1 | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA */
AM33XX_IOPAD(0x8e0, PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* lcd_vsync.lcd_vsync */
AM33XX_IOPAD(0x8e4, PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* lcd_hsync.lcd_hsync */
AM33XX_IOPAD(0x8e8, PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* lcd_pclk.lcd_pclk */
AM33XX_IOPAD(0x8ec, PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* lcd_ac_bias_en.lcd_ac_bias_en */
AM33XX_IOPAD(0x878, PIN_OUTPUT_PULLDOWN | MUX_MODE7)
>;
};
backlight_pin: backlight_pin {
pinctrl-single,pins = <
AM33XX_IOPAD(0x848, PIN_OUTPUT_PULLUP | MUX_MODE6)
>;
};
bb_spi0_pins: pinmux_bb_spi0_pins {
pinctrl-single,pins = <
0x150 0x30 /* spi0_sclk.spi0_sclk, INPUT_PULLUP | MODE0 */
0x154 0x30 /* spi0_d0.spi0_d0, INPUT_PULLUP | MODE0 */
0x158 0x10 /* spi0_d1.spi0_d1, OUTPUT_PULLUP | MODE0 */
0x15c 0x10 /* spi0_cs0.spi0_cs0, OUTPUT_PULLUP | MODE0 */
>;
};
};
&spi0 {
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&bb_spi0_pins>;
channel@0 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "spidev";
reg = <0>;
spi-max-frequency = <16000000>;
};
};
&lcdc {
status = "okay";
};
&epwmss1 {
status = "okay";
};
&ehrpwm1 {
pinctrl-names = "default";
pinctrl-0 = <&backlight_pin>;
status = "okay";
};
&rtc {
system-power-controller;
};
&sgx {
status = "okay";
};
/ {
lcd0: display {
status = "okay";
compatible = "ti,tilcdc,panel";
label = "lcd";
pinctrl-names = "default";
pinctrl-0 = <&lcd_pins>;
panel-info {
ac-bias = <255>;
ac-bias-intrpt = <0>;
dma-burst-sz = <16>;
bpp = <24>;
fdd = <0x80>;
sync-edge = <0>;
sync-ctrl = <1>;
raster-order = <0>;
fifo-th = <0>;
};
display-timings {
native-mode = <&timing0>;
timing0: 240x320 {
clock-frequency = <7200000>;
hactive = <240>;
vactive = <320>;
hfront-porch = <38>;
hback-porch = <10>;
hsync-len = <10>;
vback-porch = <4>;
vfront-porch = <8>;
vsync-len = <4>;
hsync-active = <0>; // Low active
vsync-active = <0>; // Low active
de-active = <1>; // The data DB17-0 is written when ENABLE = “1”. Disable data write operation when ENABLE = “0”.
pixelclk-active = <1>; // The data is input on the positive edge of DOTCLK
};
};
};
fb {
compatible = "ti,am33xx-tilcdc";
reg = <0x4830e000 0x1000>;
interrupt-parent = <&intc>;
interrupts = <36>;
ti,hwmods = "lcdc";
};
backlight {
status = "okay";
compatible = "pwm-backlight";
pwms = <&ehrpwm1 0 500000 0>;
brightness-levels = <
0 1 2 3 4 5 6 7 8 9
10 11 12 13 14 15 16 17 18 19
20 21 22 23 24 25 26 27 28 29
30 31 32 33 34 35 36 37 38 39
40 41 42 43 44 45 46 47 48 49
50 51 52 53 54 55 56 57 58 59
60 61 62 63 64 65 66 67 68 69
70 71 72 73 74 75 76 77 78 79
80 81 82 83 84 85 86 87 88 89
90 91 92 93 94 95 96 97 98 99
100
>;
default-brightness-level = <100>;
};
};