Other Parts Discussed in Thread: ADS1606, , 66AK2H14, 66AK2E05
Hello
I'm thinking of a new project with a TMS320C6678, in which the input data is provided by a ADS1606 (). the data sheet of the latter states that it is easy to connect to the 6600 DSP family.
Contrete I would like to ask:
1- are there examples (HW / SW), or application notes?
2- does it connect to the parallel port or to the EMIF-16?
3- would it be possible to use more than one at the same time, both connected to same bus, but with independent CS (chip select) signal? May this question should go to another thread. If so, do please tell me which one.
4- Do you think it would be easier if I consider the 66K2 family instead?
5- It would be ideal if I were able to build a prototype around an evaluation board.
Thankyou very much in advance.
Kind regards,
Pablo