Tool/software: Linux
The kernel stalled abnormally in the part of mmc for a long time
[ 2.489711] mmcblk1: p1 p2
What could be the reason for this?
reading single-stage-boot.dtb
reading uImage
reading uImage
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpuset
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.84-00018-gd326d64-dirty (root@autorad-VirtualBox) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #4 SMP PREEMPT Thu Jun 21 11:34:11 CST 2018
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] Machine model: TI DRA722 Rev C EVM
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000040300000, size 3 MiB
[ 0.000000] Reserved memory: initialized node cmem@40300000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: regions without no-map are not yet supported
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 80 MiB
[ 0.000000] Reserved memory: initialized node ipu2_cma@99000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: regions without no-map are not yet supported
[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000a1000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node dsp1_cma@a1000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a9000000, size 64 MiB
[ 0.000000] Reserved memory: initialized node cmem@A9000000, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 24 MiB at 0x00000000be400000
[ 0.000000] Forcing write-allocate cache policy for SMP
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] OMAP4: Map 0x00000000bfd00000 to fe600000 for dram barrier
[ 0.000000] Hit pending asynchronous external abort (FSR=0x00000211) during first unmask, this is most likely caused by a firmware/bootloader bug.
[ 0.000000] DRA722 ES2.0
[ 0.000000] PERCPU: Embedded 11 pages/cpu @ef667000 s14912 r8192 d21952 u45056
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 243008
[ 0.000000] Kernel command line: console=ttyO0,115200n8 vram=16M root=/dev/mmcblk0p2 rw rootwait ip=none mem=1024M
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 541536K/978944K available (6303K kernel code, 296K rwdata, 2212K rodata, 340K init, 300K bss, 298144K reserved, 139264K cma-reserved, 233472K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0858ffc (8516 kB)
[ 0.000000] .init : 0xc0859000 - 0xc08ae000 ( 340 kB)
[ 0.000000] .data : 0xc08ae000 - 0xc08f80e0 ( 297 kB)
[ 0.000000] .bss : 0xc08fa000 - 0xc0945054 ( 301 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] RCU restricting CPUs from NR_CPUS=2 to nr_cpu_ids=1.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=1
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] ti_dt_clocks_register: failed to lookup clock node gmac_gmii_ref_clk_div
[ 0.000000] OMAP clockevent source: timer1 at 32786 Hz
[ 0.000000] Architected cp15 timer(s) running at 6.14MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[ 0.000005] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[ 0.000016] Switching to timer-based delay loop, resolution 162ns
[ 0.000334] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000341] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000740] Console: colour dummy device 80x30
[ 0.000757] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000763] This ensures that you still see kernel messages. Please
[ 0.000768] update your kernel commandline.
[ 0.000781] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[ 0.000795] pid_max: default: 32768 minimum: 301
[ 0.000895] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000905] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001451] Initializing cgroup subsys io
[ 0.001468] Initializing cgroup subsys memory
[ 0.001493] Initializing cgroup subsys devices
[ 0.001505] Initializing cgroup subsys freezer
[ 0.001516] Initializing cgroup subsys perf_event
[ 0.001527] Initializing cgroup subsys pids
[ 0.001553] CPU: Testing write buffer coherency: ok
[ 0.001762] /cpus/cpu@0 missing clock-frequency property
[ 0.001775] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.001809] Setting up static identity map for 0x80008380 - 0x800083e0
[ 0.050034] Brought up 1 CPUs
[ 0.050045] SMP: Total of 1 processors activated (12.29 BogoMIPS).
[ 0.050052] CPU: All CPU(s) started in HYP mode.
[ 0.050058] CPU: Virtualization extensions available.
[ 0.050375] devtmpfs: initialized
[ 0.080055] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.080867] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.171261] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.171285] futex hash table entries: 256 (order: 2, 16384 bytes)
[ 0.183110] pinctrl core: initialized pinctrl subsystem
[ 0.184053] NET: Registered protocol family 16
[ 0.184980] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.210106] cpuidle: using governor ladder
[ 0.240126] cpuidle: using governor menu
[ 0.247001] platform 43300000.edma: Cannot lookup hwmod 'tpcc'
[ 0.247288] platform 43400000.tptc: Cannot lookup hwmod 'tptc0'
[ 0.247565] platform 43500000.tptc: Cannot lookup hwmod 'tptc1'
[ 0.248628] OMAP GPIO hardware version 0.1
[ 0.254955] irq: no irq domain found for /ocp/l4@4a000000/scm@2000/pinmux@1400 !
[ 0.275809] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.275821] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.276253] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[ 0.276264] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[ 0.276857] OMAP DMA hardware revision 0.0
[ 0.360544] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[ 0.361084] edma3-tptc 43400000.tptc: _od_fail_runtime_resume: FIXME: missing hwmod/omap_dev info
[ 0.361135] edma3-tptc 43500000.tptc: _od_fail_runtime_resume: FIXME: missing hwmod/omap_dev info
[ 0.361363] edma 43300000.edma: _od_fail_runtime_resume: FIXME: missing hwmod/omap_dev info
[ 0.361374] edma 43300000.edma: pm_runtime_get_sync() failed
[ 0.365304] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[ 0.365496] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[ 0.365666] omap-iommu 58882000.mmu: 58882000.mmu registered
[ 0.365833] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 0.368593] omap_i2c 4807c000.i2c: bus 4 rev0.12 at 100 kHz
[ 0.368770] media: Linux media interface: v0.10
[ 0.368822] Linux video capture interface: v2.00
[ 0.368862] pps_core: LinuxPPS API ver. 1 registered
[ 0.368869] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.368894] PTP clock support registered
[ 0.368943] EDAC MC: Ver: 3.0.0
[ 0.370825] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[ 0.371010] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[ 0.372026] clocksource: Switched to clocksource arch_sys_counter
[ 0.382108] NET: Registered protocol family 2
[ 0.382607] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.382671] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.382796] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.382853] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.382884] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.383030] NET: Registered protocol family 1
[ 0.393385] RPC: Registered named UNIX socket transport module.
[ 0.393395] RPC: Registered udp transport module.
[ 0.393401] RPC: Registered tcp transport module.
[ 0.393408] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.394395] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[ 0.414170] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.424852] NFS: Registering the id_resolver key type
[ 0.424880] Key type id_resolver registered
[ 0.424889] Key type id_legacy registered
[ 0.424951] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.426495] bounce: pool size: 64 pages
[ 0.426651] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[ 0.426666] io scheduler noop registered
[ 0.426680] io scheduler deadline registered
[ 0.426715] io scheduler cfq registered (default)
[ 0.431194] pinctrl-single 4a003400.pinmux: 282 pins at pa fc003400 size 1128
[ 0.431315] pinctrl-single 4a002e8c.pinmux: 1 pins at pa fc002e8c size 4
[ 0.434474] PCI host bridge /ocp/axi@0/pcie_rc@51000000 ranges:
[ 0.434488] No bus range found for /ocp/axi@0/pcie_rc@51000000, using [bus 00-ff]
[ 0.434522] IO 0x20003000..0x20012fff -> 0x00000000
[ 0.434543] MEM 0x20013000..0x2fffffff -> 0x20013000
[ 0.464475] dra7-pcie 51000000.pcie_rc: link is not up
[ 0.464653] dra7-pcie 51000000.pcie_rc: PCI host bridge to bus 0000:00
[ 0.464665] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 0.464676] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 0.464686] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[ 0.465097] PCI: bus0: Fast back to back transfers disabled
[ 0.465214] PCI: bus1: Fast back to back transfers enabled
[ 0.465307] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
[ 0.465321] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
[ 0.465334] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 0.465561] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
[ 0.521130] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.523965] omap8250 4806a000.serial: Can't verify DMA configuration (-19)
[ 0.524481] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 301, base_baud = 3000000) is a 8250
[ 1.510524] console [ttyS0] enabled
[ 1.514488] omap8250 48020000.serial: Can't verify DMA configuration (-19)
[ 1.521857] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 302, base_baud = 3000000) is a 8250
[ 1.531161] omap8250 48066000.serial: Can't verify DMA configuration (-19)
[ 1.538551] 48066000.serial: ttyS4 at MMIO 0x48066000 (irq = 303, base_baud = 3000000) is a 8250
[ 1.548508] [drm] Initialized drm 1.1.0 20060810
[ 1.554086] 58000000.dss supply vdda_video not found, using dummy regulator
[ 1.561221] OMAP DSS rev 6.1
[ 1.565038] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
[ 1.617610] brd: module loaded
[ 1.705925] loop: module loaded
[ 1.709367] vmemexp device MAJOR num = 246
[ 1.713535] vmemexp class registered
[ 1.717237] /dev/vmemexp device registered
[ 1.721351] ioctl DBUFIOC_EXPORT_VIRTMEM = -1072899120
[ 1.728988] libphy: Fixed MDIO Bus: probed
[ 1.734402] i2c /dev entries driver
[ 1.742510] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.750575] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 1.755643] vsys_3v3: supplied by evm_12v0
[ 1.759809] evm_3v3: supplied by vsys_3v3
[ 1.763891] evm_3v3_sd: supplied by evm_3v3
[ 1.802741] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[ 1.809127] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[ 1.852704] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.859972] omap_rproc_probe=============================
[ 1.882016] omap_rproc_get_firmware================
[ 1.886920] rproc_alloc=============================
[ 1.902023] omap-rproc 55020000.ipu: assigned reserved memory node ipu2_cma@99000000
[ 1.909842] remoteproc0: 55020000.ipu is available
[ 1.922018] remoteproc0: Note: remoteproc is still under development and considered experimental.
[ 1.931015] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 1.962139] remoteproc0: direct-loading firmware out===============
[ 1.968519] remoteproc0: if (ret) out========
[ 1.973065] omap_rproc_probe=============================
[ 1.978484] omap_rproc_get_firmware================
[ 1.992040] remoteproc0: if (ret) in========
[ 1.996415] remoteproc0: ========Direct firmware load for dra7-ipu2-fw.xem4 failed with error -2
[ 2.012023] rproc_alloc=============================
[ 2.017119] omap-rproc 40800000.dsp: assigned reserved memory node dsp1_cma@a1000000
[ 2.032019] remoteproc0: Falling back to user helper
[ 2.037228] remoteproc1: 40800000.dsp is available
[ 2.052049] remoteproc1: Note: remoteproc is still under development and considered experimental.
[ 2.061045] remoteproc1: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 2.092112] remoteproc1: direct-loading firmware out===============
[ 2.098493] remoteproc1: if (ret) out========
[ 2.104193] NET: Registered protocol family 10
[ 2.112079] remoteproc1: if (ret) in========
[ 2.116458] remoteproc1: ========Direct firmware load for dra7-dsp1-fw.xe66 failed with error -2
[ 2.125631] sit: IPv6 over IPv4 tunneling driver
[ 2.130820] NET: Registered protocol family 17
[ 2.152033] can: controller area network core (rev 20120528 abi 9)
[ 2.158398] NET: Registered protocol family 29
[ 2.162883] remoteproc1: Falling back to user helper
[ 2.172035] can: raw protocol (rev 20120528)
[ 2.176330] can: broadcast manager protocol (rev 20120528 t)
[ 2.192037] can: netlink gateway (rev 20130117) max_hops=1
[ 2.202220] Key type dns_resolver registered
[ 2.206517] NET: Registered protocol family 41
[ 2.211110] omap_voltage_late_init: Voltage driver support not added
[ 2.233829] Power Management for TI OMAP4+ devices.
[ 2.238949] Registering SWP/SWPB emulation handler
[ 2.263720] dmm 4e000000.dmm: initialized all PAT entries
[ 2.273727] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 2.280395] [drm] No driver support for vblank timestamp query.
[ 2.289929] [drm] Initialized omapdrm 1.0.0 20110917 on minor 0
[ 2.316644] hctosys: unable to open rtc device (rtc0)
[ 2.323672] mmc0: host does not support reading read-only switch, assuming write-enable
[ 2.342177] mmc0: new high speed SDHC card at address 1234
[ 2.348272] aic_dvdd: disabling
[ 2.351431] vmmcwl_fixed: disabling
[ 2.355949] omap8250 4806a000.serial: failed to request DMA
[ 2.365234] mmcblk0: mmc0:1234 SA08G 7.21 GiB
[ 2.371070] mmcblk0: p1 p2
[ 2.375787] EXT4-fs (mmcblk0p2): couldn't mount as ext3 due to feature incompatibilities
[ 2.425589] mmc1: MAN_BKOPS_EN bit is not set
[ 2.435235] mmc1: new HS200 MMC card at address 0001
[ 2.451690] mmcblk1: mmc1:0001 IS008G 7.28 GiB
[ 2.466570] mmcblk1boot0: mmc1:0001 IS008G partition 1 4.00 MiB
[ 2.482807] mmcblk1boot1: mmc1:0001 IS008G partition 2 4.00 MiB
[ 2.489711] mmcblk1: p1 p2
[ 8.161662] EXT4-fs (mmcblk0p2): recovery complete
[ 8.174088] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 8.182265] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 8.189921] devtmpfs: mounted
[ 8.193132] Freeing unused kernel memory: 340K
[ 8.197593] This architecture does not have kernel memory protection.
[ 8.230005] Kernel Entry time 169703 ticks
[ 8.452117] systemd[1]: System time before build time, advancing clock.
[ 8.486109] random: systemd: uninitialized urandom read (16 bytes read, 12 bits of entropy available)
[ 8.499103] random: systemd: uninitialized urandom read (16 bytes read, 12 bits of entropy available)
[ 8.510795] systemd[1]: systemd 229 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT +GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN)
[ 8.529393] systemd[1]: Detected architecture arm.
Welcome to Arago 2016.12!
[ 8.563366] systemd[1]: Set hostname to <dra7xx-evm>.
[ 8.602456] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 13 bits of entropy available)
[ 8.636594] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 13 bits of entropy available)
[ 8.650334] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 13 bits of entropy available)
[ 8.673720] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 14 bits of entropy available)
[ 8.692348] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 14 bits of entropy available)
[ 8.813220] random: systemd: uninitialized urandom read (16 bytes read, 17 bits of entropy available)
[ 8.823326] random: systemd: uninitialized urandom read (16 bytes read, 17 bits of entropy available)
[ 8.833004] random: systemd: uninitialized urandom read (16 bytes read, 17 bits of entropy available)
[ 8.971522] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 8.992389] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 9.012760] systemd[1]: Created slice System Slice.
[ OK ] Created slice System Slice.
[ 9.032222] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 9.052371] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ 9.082337] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 9.102372] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ 9.132330] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 9.157670] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 9.185273] systemd[1]: Starting Create list of required static device nodes for the current kernel...
Starting Create list of required st... nodes for the current kernel...
[ 9.235638] systemd[1]: Starting Setup Virtual Console...
Starting Setup Virtual Console...
[ 9.262861] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
[ 9.294508] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 9.324823] systemd[1]: Mounting Debug File System...
[ 9.335735] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
Mounting Debug File System...
[ 9.372358] systemd[1]: Reached target Paths.
[ OK ] Reached target Paths.
[ 9.392247] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 9.412924] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 9.434472] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 9.467694] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 9.498929] systemd[1]: Mounting Temporary Directory...
Mounting Temporary Directory...
[ 9.532496] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 9.564323] systemd[1]: Mounted POSIX Message Queue File System.
[ OK ] Mounted POSIX Message Queue File System.
[ 9.602483] systemd[1]: Mounted Debug File System.
[ OK ] Mounted Debug File System.
[ 9.632323] systemd[1]: Mounted Temporary Directory.
[ OK ] Mounted Temporary Directory.
[ 9.652519] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
[ OK ] Started Create list of required sta...ce nodes for the current kernel.
[ OK ] Started Setup Virtual Console.
[ OK ] Started Remount Root and Kernel File Systems.
Starting udev Coldplug all Devices...
Starting Load/Save Random Seed...
Starting Create Static Device Nodes in /dev...
Starting Apply Kernel Variables...
Starting Flush Journal to Persistent Storage...
[ OK ] Started Load/Save Random Seed.
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create Static Device Nodes in /dev.
[ 10.357535] systemd-journald[122]: Received request to flush runtime journal from PID 1
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Reached target Local File Systems (Pre).
Mounting /media/ram...
Mounting /var/volatile...
Starting udev Kernel Device Manager...
[ OK ] Mounted /var/volatile.
[ OK ] Mounted /media/ram.
[ OK ] Started udev Kernel Device Manager.
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Started Create Volatile Files and Directories.
[ 11.246838] rproc_boot==================================================
Starting Update UTMP about System Boot/Shutdown...
[ 11.281455] remoteproc1: powering up 40800000.dsp
[ 11.312255] rproc_fw_boot==================================================
[ 11.319256] rproc_fw_boot============================
[ 11.456608] remoteproc1: Booting fw image dra7-dsp1-fw.xe66, size 700117
[ 11.532426] rproc_enable_iommu start============================
[ 11.538470] rproc->has_iommu====================
[ 11.599193] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
[ 11.618511] iommu_domain_alloc====================
[ 11.650583] iommu_set_fault_handler====================
[ 11.719184] iommu_attach_device1====================
[ 11.755850] iommu_group_get====================
[ 11.781901] omap_rtc 48838000.rtc: rtc core: registered 48838000.rtc as rtc0
[ 11.829486] group == NULL====================
[ 11.890627] omap-iommu 40d01000.mmu: 40d01000.mmu: version 3.0
[ 11.896648] omap-iommu 40d02000.mmu: 40d02000.mmu: version 3.0
[ 12.027664] iommu_attach_device2====================
[ 12.053714] rproc->domain = domain====================
[ 12.058885] rproc_get_boot_addr============================
[ 12.127299] rproc_find_rsc_table============================
[ 12.173629] crc32============================
[ 12.200125] rproc_handle_resources============================
[ OK ] Started udev Coldplug all Devices.
[ 12.265550] rproc_find_version_info============================
[ 12.412166] rproc_find_loaded_rsc_table============================
[ 12.418475] rproc_handle_resourcese============================
[ 12.543124] start============================
[ 12.547763] remoteproc1: remote processor 40800000.dsp is now up
[ OK ] Found device /dev/ttyS0.
[ 12.608489] CAN device driver interface
[ 12.625739] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
[ 12.700917] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 12.772914] remoteproc1: registered virtio0 (type 7)
[ 12.778170] virtio_rpmsg_bus virtio0: creating channel rpmsg-proto addr 0x50
[ 12.813766] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
[ 12.819601] omap-aes 4b500000.aes: Unable to request in DMA channel
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ 12.949498] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
[ 12.972402] omap-aes 4b700000.aes: Unable to request in DMA channel
[ 13.018742] c_can_platform 4ae3c000.can: c_can_platform device registered (regs=fce3c000, irq=349)
[ OK ] Reached target System Initialization.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
Starting rc.pvr.service...
Starting Permit User Sessions...
[ OK ] Started D-Bus System Message Bus.
[ 13.411903] [drm] Initialized pvr 1.14.3699939 20110701 on minor 1
[ 13.685965] rproc_boot==================================================
[ 13.762620] PVR_K: UM DDK-(3699939) and KM DDK-(3699939) match. [ OK ]
[ 13.774895] remoteproc0: powering up 55020000.ipu
[ 13.798610] EXT4-fs (mmcblk1p2): recovery complete
[ 13.834508] rproc_fw_boot==================================================
[ 13.870308] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
[ 13.883401] FAT-fs (mmcblk1p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 13.902442] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 13.969950] rproc_fw_boot============================
[ 14.020224] remoteproc0: Booting fw image dra7-ipu2-fw.xem4, size 6021480
Starting Login Service...
[ 14.124537] rproc_enable_iommu start============================
[ 14.181371] rproc->has_iommu====================
[ 14.231449] iommu_domain_alloc====================
[ 14.292240] iommu_set_fault_handler====================
[ 14.297498] iommu_attach_device1====================
[ 14.384927] iommu_group_get====================
[ 14.389487] group == NULL====================
[ 14.480576] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1
[ 14.541789] iommu_attach_device2====================
[ 14.582412] rproc->domain = domain====================
[ 14.587581] rproc_get_boot_addr============================
[ 14.623953] rproc_find_rsc_table============================
[ 14.629648] crc32============================
[ 14.664809] rproc_handle_resources============================
[ 14.713632] rproc_find_version_info============================
[ 14.719595] rproc_find_loaded_rsc_table============================
[ OK ] Started rc.pvr.service.
[ 14.784432] rproc_handle_resourcese============================
[ 14.790385] start============================
[ 14.825854] remoteproc0: remote processor 55020000.ipu is now up
[ 14.850479] virtio_rpmsg_bus virtio1: rpmsg host is online
[ 14.874980] remoteproc0: registered virtio1 (type 7)
[ 14.905252] virtio_rpmsg_bus virtio1: creating channel rpmsg-proto addr 0x50
[ OK ] Started Permit User Sessions.
[ OK ] Started Login Service.
[ OK ] Started Serial Getty on ttyS0.
[ OK ] Reached target Login Prompts.
[ OK ] Reached target Multi-User System.
[ OK ] Reached target Graphical Interface.
Starting Update UTMP about System Runlevel Changes...
[ OK ] Started Update UTMP about System Runlevel Changes.
[ 16.505160] usbcore: registered new interface driver usbfs
[ 16.519217] usbcore: registered new interface driver hub
[ 16.537479] usbcore: registered new device driver usb
[ 16.623526] dwc3 488d0000.usb: otg: primary host xhci-hcd.0.auto registered
[ 16.630531] dwc3 488d0000.usb: otg: shared host xhci-hcd.0.auto registered
[ 16.638859] dwc3 488d0000.usb: otg: can't start till gadget registers
[ 16.646356] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 16.651894] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 1
[ 16.660979] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x00210010
[ 16.671434] xhci-hcd xhci-hcd.1.auto: irq 456, io mem 0x48890000
[ 16.680728] hub 1-0:1.0: USB hub found
[ 16.685345] hub 1-0:1.0: 1 port detected
[ 16.690103] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 16.696813] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 2
[ 16.705150] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 16.715211] hub 2-0:1.0: USB hub found
[ 16.719011] hub 2-0:1.0: 1 port detected
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org dra7xx-evm ttyS0