This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TDA3XEVM: CCS build vocp failed

Part Number: TDA3XEVM

Tool/software: TI C/C++ Compiler

1. What difference between vcop_blockAverage2x2_uchar_cn and vcop_blockAverage2x2_uchar;

2. I can find the define of vcop_blockAverage2x2_uchar, But I can't find the diefine of  vcop_blockAverage2x2_uchar_cn, Which lib include the vcop_blockAverage2x2_uchar_cn,?

'Building target: "vcop_example.out"'
'Invoking: EVE Linker'
"C:/ti_ccs7_4/ccsv7/tools/compiler/arp32_1.0.9/bin/cl-arp32" -v210 -g --diag_warning=225 --display_error_number --diag_wrap=off -z -m"vcop_example.map" -i"C:/ti_ccs7_4/ccsv7/tools/compiler/arp32_1.0.9/lib" -i"C:/PROCESSOR_SDK_VISION_03_02_00_00/ti_components/algorithms/eve_sw_01_18_00_00/kernels/lib/debug" -i"C:/ti_ccs7_4/ccsv7/tools/compiler/arp32_1.0.9/include" --reread_libs --warn_sections --xml_link_info="vcop_example_linkInfo.xml" --rom_model -o "vcop_example.out" "./boot_arp32.obj" "./main.obj" "./vcop_blockAverage2x2_kernel.obj" "../linker_boot_cama.cmd" -llibc.a
<Linking>

undefined first referenced
symbol in file
--------- ----------------
vcop_blockAverage2x2_uchar_cn ./main.obj

error #10234-D: unresolved symbols remain
warning #10063-D: entry-point symbol other than "_c_int00" specified: "_reset_handler"
error #10010: errors encountered during linking; "vcop_example.out" not built