Part Number: TMS320C6678
Other Parts Discussed in Thread: CODECOMPOSER, SYSBIOS
Tool/software: TI-RTOS
CCSv7.3.0.00019
SDK v04.01.00.06
- CG_XML 2.41.00
- CTools Library 2.2.0.0
- DSPLIB 3.4.0.0
- EDMA3 LLD 2.12.05.29
- FFTLIB 3.1.0.0
- Framework Components 3.40.02.07
- IMGLIB 3.1.1.0
- IPC 3.46.02.04
- LIBARCH 1.0.0.0
- LINALG 1.2.0.0
- MATHLIB 3.1.1.0
- NDK 2.25.01.11
- OpenMP 2.06.02.00
- PDK C667X 2.0.7
- Processor SDK RTOS C667X 04.01.00.06
- SYS/BIOS 6.46.05.55
- TI CGT 6x 8.1.3
- UIA 2.00.06.52
- XDAIS 7.24.00.04
- XDCtools 3.32.01.22
Hello, I need to catch gpio interrupts while using NDK, so I added to the client.c the following (processors.wiki.ti.com/.../Configuring_Interrupts_on_Keystone_Devices)
-
#include <xdc/runtime/Error.h>
#include <ti/csl/csl_gpio.h>
#include <ti/csl/csl_gpioAux.h> -
void gpio_isr_handler(UArg arg)
{
printf("GPIO interrupt!!!\n");
} -
Hwi_Handle myHwi;
int init_gpio_interrupt_hwi(char pinNum, char intNum)
{
Int32 instNum = 0;
Uint8 bankNum = 0;hGpio = CSL_GPIO_open(instNum);
CSL_GPIO_setPinDirOutput (hGpio, pinNum);
CSL_GPIO_setRisingEdgeDetect (hGpio,pinNum);
CSL_GPIO_bankInterruptEnable (hGpio,bankNum);printf("Mapping GPIO%d (Event%d) to INT%d...\n",pinNum,pinNum+74,intNum);
Hwi_Params hwiParams;
Error_Block eb;Hwi_Params_init(&hwiParams);
Error_init(&eb);// set the argument you want passed to your ISR function
hwiParams.arg = 1;// set the event id of the peripheral assigned to this interrupt
hwiParams.eventId = pinNum+74;// don't allow this interrupt to nest itself
hwiParams.maskSetting = Hwi_MaskingOption_SELF;//
// Configure interrupt intNum to invoke "gpio_isr_handler".
// Automatically enables interrupt intNum by default
// set params.enableInt = FALSE if you want to control
// when the interrupt is enabled using Hwi_enableInterrupt()
//myHwi = Hwi_create(intNum, gpio_isr_handler, &hwiParams, &eb);
if (Error_check(&eb)) {
// handle the error
}return 0;
} -
int StackTest()
{
int rc;
int i;
HANDLE hCfg;
CI_SERVICE_TELNET telnet;
CI_SERVICE_HTTP http;
NIMU_QMSS_CFG_T qmss_cfg;
NIMU_CPPI_CFG_T cppi_cfg;init_gpio_interrupt_hwi(15,10);
if (setupRm ())
{
NIMU_testLog ("Function setupRm failed\n");
System_flush();
goto main_exit;
}...
I got the statement in console
Then when I tried to set the interrupt using CodeComposer Registers it seems interrupt didn't work (my gpio_isr_handler didn't print the message)
How can I achieve my goal: configure gpio interrupt while using NDK? All gpio interrupt examples I found are working standalone, so I think there's a collision between ndk interrupts and my interrupts.