Tool/software: TI-RTOS
Hello,
I am trying to build SBL components on windows and i have the following error:
gmake[1]: Leaving directory `C:/ti/pdk_am57xx_1_0_10/packages/ti/board/diag'
gmake buildtarget bboard=evmK2G btests=evmK2G_DIAG
gmake[1]: Entering directory `C:/ti/pdk_am57xx_1_0_10/packages/ti/board/diag'
gmake -C dcan BOARD=evmK2G TARGET=armv7 BOOTMODE=
gmake[2]: Entering directory `C:/ti/pdk_am57xx_1_0_10/packages/ti/board/diag/dca
n'
gmake -f ./build/evmK2G/armv7/makefile
gmake[3]: Entering directory `C:/ti/pdk_am57xx_1_0_10/packages/ti/board/diag/dca
n'
compiling /ti/PDK_AM~1/packages/ti/board/diag/common/K2G/platform.c ...
/ti/PDK_AM~1/packages/ti/board/diag/common/K2G/platform.c: In function 'platform
_delay':
/ti/PDK_AM~1/packages/ti/board/diag/common/K2G/platform.c:1063:5: warning: impli
cit declaration of function 'BOARD_delay' [-Wimplicit-function-declaration]
BOARD_delay(usecs);
^~~~~~~~~~~
/ti/PDK_AM~1/packages/ti/board/diag/common/K2G/platform.c:1064:1: warning: contr
ol reaches end of non-void function [-Wreturn-type]
}
^
At top level:
/ti/PDK_AM~1/packages/ti/board/diag/common/K2G/platform.c:168:13: warning: 'getS
erialNumber' defined but not used [-Wunused-function]
static void getSerialNumber(char *buf)
^~~~~~~~~~~~~~~
/ti/PDK_AM~1/packages/ti/board/diag/common/K2G/platform.c:59:3: warning: 'platfo
rm_mcb' defined but not used [-Wunused-variable]
} platform_mcb = {0, 0, 0};
^~~~~~~~~~~~
linking /ti/PDK_AM~1/packages/ti/board/obj/evmK2G/armv7/dcan_test.o /ti/PDK_AM~1
/packages/ti/board/obj/evmK2G/armv7/evmk2g_dcan.o /ti/PDK_AM~1/packages/ti/board
/obj/evmK2G/armv7/evmk2g_dcan_frame.o /ti/PDK_AM~1/packages/ti/board/obj/evmK2G/
armv7/evmk2g_dcan_platform.o /ti/PDK_AM~1/packages/ti/board/obj/evmK2G/armv7/dia
g_entry.ao /ti/PDK_AM~1/packages/ti/board/obj/evmK2G/armv7/platform.o /ti/PDK_AM
~1/packages/ti/board/obj/evmK2G/armv7/diag_common_cfg.o into /ti/PDK_AM~1/packag
es/ti/board/bin/evmK2G/armv7/dcan_diagExample_evmK2G_armv7.out ...
arm-none-eabi-gcc.exe: error: /ti/PDK_AM~1/packages/ti/board/lib/evmK2G/a15/rele
ase/ti.board.aa15fg: No such file or directory
arm-none-eabi-gcc.exe: error: /ti/PDK_AM~1/packages/ti/csl/lib/k2g/a15/release/t
i.csl.aa15fg: No such file or directory
arm-none-eabi-gcc.exe: error: /ti/PDK_AM~1/packages/ti/csl/lib/k2g/a15/release/t
i.csl.init.aa15fg: No such file or directory
arm-none-eabi-gcc.exe: error: /ti/PDK_AM~1/packages/ti/drv/uart/lib/k2g/a15/rele
ase/ti.drv.uart.aa15fg: No such file or directory
arm-none-eabi-gcc.exe: error: /ti/PDK_AM~1/packages/ti/drv/i2c/lib/k2g/a15/relea
se/ti.drv.i2c.aa15fg: No such file or directory
arm-none-eabi-gcc.exe: error: /ti/PDK_AM~1/packages/ti/osal/lib/nonos/k2g/a15/re
lease/ti.osal.aa15fg: No such file or directory
gmake[3]: *** [/ti/PDK_AM~1/packages/ti/board/bin/evmK2G/armv7/dcan_diagExample_
evmK2G_armv7.out] Error 1
gmake[3]: Leaving directory `C:/ti/pdk_am57xx_1_0_10/packages/ti/board/diag/dcan
'
gmake[2]: *** [build_example] Error 2
gmake[2]: Leaving directory `C:/ti/pdk_am57xx_1_0_10/packages/ti/board/diag/dcan
'
gmake[1]: *** [dcan_build] Error 2
gmake[1]: Leaving directory `C:/ti/pdk_am57xx_1_0_10/packages/ti/board/diag'
gmake: *** [evmK2G] Error 2
Please help me fix the issue. Not sure what i am missing here.
Thanks,
Deepthi