This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI-RTOS
Hello,
I need to create a project using DSP BIOS kernel on a board based upon a TMS320C6413 DSP.
With the DSP BIOS distribution I 've just downloaded, the TI available platforms do not contain (at least not directly) reference to TMS320C6413 DSP.
Which existing plateform would be the best to use for this DSP (perhaps sim64xx ?) ?
Best regards.
Paul-Henri
Hello Judah,
I use CC studio V8.1.0.
With this release, when I create a new DSP Bios configuration file project, I'm not able to select the ti platform sim6xxx (not proposed in the dialog box, even if there is a sim6xxx directory in the ti\bios_5_42_02_10\packages\ti\platforms directory.
I will continue trying to generate a configuration file which I hope will compile and work.
Thank you.
Regards.
Paul-Henri
Hi,
Not fully resolved...
I started with the 64xx platform and specify TMS C6413:
utils.loadPlatform("ti.platforms.sim64xx", {deviceName: '6413'});
/* The following DSP/BIOS Features are enabled. */
bios.enableRealTimeAnalysis(prog);
bios.enableRtdx(prog);
bios.enableTskManager(prog);
bios.MEM.instance("SDRAM").destroy();
bios.GBL.CLKIN = 33333;
bios.GBL.CLKOUT = 400.0000;
bios.GBL.ENDIANMODE = "big";
bios.GBL.ENABLEINST = 0;
bios.GBL.INSTRUMENTED = 0;
bios.GBL.ENABLEALLTRC = 0;
// !GRAPHICAL_CONFIG_TOOL_SCRIPT_INSERT_POINT!
prog.gen();
When I try to compile my project which includes this DSP BIOS configuration file, I have some compilation errors in my .h62 genrated file. I have a first error on KNL_swi function:
;; ======== SWI_Obj KNL_swi ========
;; This Software Interrupt calls the TSK scheduler
;;
;; SWI_Obj KNL_swi (function, pri, mailbox, arg0, arg1, dorta, Order, filter, maxformat, sumformat, avgformat, filtmaxmult, filtsummult, unittype)
.global KNL_swi
.asg _KNL_run, _function
.asg 00H, _pri
.asg 00H, _mailbox
.asg 00H, _arg0
.asg 00H, _arg1
.asg 01H, _dorta
.asg 00H, _Order
.asg 02H, _filter
.asg "%g inst", _maxformat
.asg "%g inst", _sumformat
.asg "%.2f inst", _avgformat
.asg 01H, _filtmaxmult
.asg 01H, _filtsummult
.asg 00H, _unittype
SWI_Obj 1, KNL_swi, 0, _function, _pri, _mailbox, _arg0, _arg1, _dorta, _Order, _filter, _maxformat, _sumformat, _avgformat, _filtmaxmult, _filtsummult, _unittype
The compiler gives the following error:
>> Compilation failure
subdir_rules.mk:26: recipe for target 'rgwycfg.obj' failed
"rgwycfg.s62", ERROR! at line 842: [E0003] Invalid constant specification
SWI_Obj 1, KNL_swi, 0, _function, _pri, _mailbox, _arg0, _arg1, _dorta, _Order, _filter, _maxformat, _sumformat, _avgformat, _filtmaxmult, _filtsummult, _unittype
"rgwycfg.s62", REMARK at line 842: [R0001] After symbol substitution the line became:
SWI_Obj 1, KNL_swi, 0, _KNL_run, 00H, 00H, 00H, 00H, 01H, 00H, 02H, %g inst, %g inst, %.2f inst, _filtmaxmult, _filtsummult, _unittype
I suppose the problem comes from the _maxformat, _sumformat, _avgformat which are not correctly defined, but I don't know how to define them in the configuration tool.
Can you help ?
Best regards.
Paul-Henri
Paul-Henri,
Sorry, I think I was looking at BIOS 6.x instead of BIOS 5.x platforms....
So what I did was created a new CCS Project.
Under DSP/BIOS v5.xx Examples select the "hello example" from the "sim6416 Examples".
Then I took your code above and modified the hello.tcf to match it. I had to modify the hello.c and update some endian settings for my compiler options.
After doing that, my program build fine. The error you are getting is most likely due to a mismatch of DSP/BIOS version.
Could you double check that the DSP/BIOS version is the version from which you created the project?
I'm assuming you have multiple DSP/BIOS v5 in your installation.
Judah
Hello Judah,
I have try to follow your recommandation. I have created a new project based upon BDP/BIOS/sim6416/hello example project :
My project properties is the following:
When I try to compile it, I have exactly the same error as with my project:
"hellocfg.s62", ERROR! at line 887: [E0003] Invalid constant specification
SWI_Obj 1, KNL_swi, 0, _function, _pri, _mailbox, _arg0, _arg1, _dorta, _Order, _filter, _maxformat, _sumformat, _avgformat, _filtmaxmult, _filtsummult, _unittype
"hellocfg.s62", REMARK at line 887: [R0001] After symbol substitution the line became:
SWI_Obj 1, KNL_swi, 0, _KNL_run, 00H, 00H, 00H, 00H, 01H, 00H, 02H, %g inst, %g inst, %.2f inst, _filtmaxmult, _filtsummult, _unittype
I have checked that I have only one DSP BIOS distribution on my PC....
Any other idea ?
Best regards.
Paul-Henri
Paul,
Here's my full build log:
**** Build of configuration Debug for project test1 ****
"C:\\ti\\ccsv6.2.0.48\\ccsv6\\utils\\bin\\gmake" -k all
'Building file: ../hello.tcf'
'Invoking: TConf'
"C:/ti/ccsv6.2.0.48/bios_5_42_02_10/xdctools/tconf" -b -Dconfig.importPath="C:/ti/ccsv6.2.0.48/bios_5_42_02_10/packages;" "../hello.tcf"
remark:Sim64xx platform is configured for 6413 device. To change the configuration to another 64xx device, please add that device as a parameter to utils.loadPlatform() call in your TCF file. Ex:
utils.loadPlatform('ti.platforms.sim64xx', {deviceName: '###'});
For more information, please refer to Chapter 4 of the Tconf User's Guide
(SPRU007G)
'Finished building: ../hello.tcf'
' '
'Building file: ../hello.c'
'Invoking: C6000 Compiler'
"C:/ti/ccsv6.2.0.48/ccsv6/tools/compiler/c6000_7.4.18/bin/cl6x" -mv6400 --big_endian --abi=coffabi -g --include_path="C:/ti/ccsv6.2.0.48/ccsv6/tools/compiler/c6000_7.4.18/include" --include_path="C:/Users/a0783947/workspace_v6_2_0_48k/test1/Debug" --include_path="C:/ti/ccsv6.2.0.48/bios_5_42_02_10/packages/ti/bios/include" --include_path="C:/ti/ccsv6.2.0.48/bios_5_42_02_10/packages/ti/rtdx/include/c6000" --diag_wrap=off --diag_warning=225 --display_error_number --preproc_with_compile --preproc_dependency="hello.d" "../hello.c"
'Finished building: ../hello.c'
' '
'Building file: hellocfg.s??'
'Invoking: C6000 Compiler'
"C:/ti/ccsv6.2.0.48/ccsv6/tools/compiler/c6000_7.4.18/bin/cl6x" -mv6400 --big_endian --abi=coffabi -g --include_path="C:/ti/ccsv6.2.0.48/ccsv6/tools/compiler/c6000_7.4.18/include" --include_path="C:/Users/a0783947/workspace_v6_2_0_48k/test1/Debug" --include_path="C:/ti/ccsv6.2.0.48/bios_5_42_02_10/packages/ti/bios/include" --include_path="C:/ti/ccsv6.2.0.48/bios_5_42_02_10/packages/ti/rtdx/include/c6000" --diag_wrap=off --diag_warning=225 --display_error_number --preproc_with_compile --preproc_dependency="hellocfg.d" "hellocfg.s??"
'Finished building: hellocfg.s??'
' '
'Building file: hellocfg_c.c'
'Invoking: C6000 Compiler'
"C:/ti/ccsv6.2.0.48/ccsv6/tools/compiler/c6000_7.4.18/bin/cl6x" -mv6400 --big_endian --abi=coffabi -g --include_path="C:/ti/ccsv6.2.0.48/ccsv6/tools/compiler/c6000_7.4.18/include" --include_path="C:/Users/a0783947/workspace_v6_2_0_48k/test1/Debug" --include_path="C:/ti/ccsv6.2.0.48/bios_5_42_02_10/packages/ti/bios/include" --include_path="C:/ti/ccsv6.2.0.48/bios_5_42_02_10/packages/ti/rtdx/include/c6000" --diag_wrap=off --diag_warning=225 --display_error_number --preproc_with_compile --preproc_dependency="hellocfg_c.d" "hellocfg_c.c"
'Finished building: hellocfg_c.c'
' '
'Building target: test1.out'
'Invoking: C6000 Linker'
"C:/ti/ccsv6.2.0.48/ccsv6/tools/compiler/c6000_7.4.18/bin/cl6x" -mv6400 --big_endian --abi=coffabi -g --diag_wrap=off --diag_warning=225 --display_error_number -z -m"test1.map" -i"C:/ti/ccsv6.2.0.48/ccsv6/tools/compiler/c6000_7.4.18/lib" -i"C:/ti/ccsv6.2.0.48/ccsv6/tools/compiler/c6000_7.4.18/include" -i"C:/ti/ccsv6.2.0.48/bios_5_42_02_10/packages/ti/rtdx/lib/c6000" -i"C:/ti/ccsv6.2.0.48/bios_5_42_02_10/packages/ti/bios/lib" --reread_libs --diag_wrap=off --display_error_number --warn_sections --xml_link_info="test1_linkInfo.xml" --rom_model -o "test1.out" "./hello.obj" "./hellocfg.obj" "./hellocfg_c.obj" -l"./hellocfg.cmd" -llibc.a
<Linking>
'Finished building target: test1.out'
' '
**** Build Finished ****
Judah,
Thanks!
Paul-Henri,
You might want to make a "DIFF" to compare the different files of your project vs Judah's project.
This could help to highlight the config differences.
A.
A bit of additional new info. I was able to install C6000 compiler V7.3.23 and just tested my same project with a clean build.
The build is successful with the older C6000 compiler. The only configuration change I made was selecting the V7.3.23 compiler version.
I have a team member who seems to have also successfully built the same project with an older version of CCS using the V7.4.12 compiler version.
It looks like Judah did not have problems building with V7.4.18, so it looks like the problem is likely to occur somewhere between C6000 V7.4.18 and V7.4.24. CCS 8.1 doesn't let me install any other 7.4 variants prior to 7.4.24, since 7.4.24 is the latest update.
Does anyone know how to make CCS install compiler sub-releases, even if a more recent update is available? Anyone know if the test project was built successfully with a C6000 compiler version between 7.4.18 and 7.4.24?
Bob
Hi Judah,
The trouble comes from the release of the C6000 compiler.
I have no trouble with release 7.4.23. The trouble comes with 7.4.24.
Thank you for you help !
Paul-Henri