Part Number: AM5728
Other Parts Discussed in Thread: TPS659037
Hello,
1) Using AM5728 to make a core board, using the matching PMU, TPS6590376ZWSR.
2) Hardware test, TPS6590376ZWSR has no voltage output, the input is 5V, and the test crystal frequency is normal. A portion of the LDO output is hot. No short circuit was found on the board. At present, I have made 2 boards, and the phenomenon is the same.
3) The attachment is a schematic, please help us to check the problem!