Part Number: AM5716
Other Parts Discussed in Thread: AM5718,
Hi Sitara Support Team,
This post is related question of the thread.
e2e.ti.com/.../2584900
I would like to know how many planes can accept the DSS of AM571x?
My customer hope it would be realized the following requirement.
However I suppose that the maximum planes are 2 planes on one display
and the customer requirement can be accept the following status.
Can the DSS of AM571x manage the following customer's requirements?
I have referred the following documents.
-Figure 11-42. DISPC Architecture Overview
www.tij.co.jp/.../spruhz7h.pdf
-overview of the DSS hardware:
processors.wiki.ti.com/.../Linux_Core_DSS_User's_Guide
****Customer's requirement****
DSS of AM571x can realize the all planes output.
-Resolution: Main LCD(1366x768), Second LCD(1280x768 or 800x600) like VESA standard.
-Framerate: 60Hz
-Color Space Format:15bit Color RGB
-Each plane needs a transparent function
-Planes priority(overlay): Mouse(cursor)>Plane 2>Plane1>Plane0>Plane6>Plane7
-Main LCD-
Plane0 for Window
Plane1 for Floating window
Plane2 for tool bar
Plane3 for mouse (cursor)
Plane4: Unused
Plane5: Unused
Plane6 for measuring data display
Plane7 for measuring text date, grid line and so on
-Second LCD-
Plane8 (expansion1) for Window
Plane9 (expansion1) for Floating window
Plane10 (expansion1) for tool bar
Plane11 (expansion1): Unused
Plane12 (expansion1): Unused
Plane13 (expansion1): Unused
Plane14 (expansion1) for measuring data display
Plane15 (expansion1) for measuring data display
***********************************************
If their requirements are not possible,
do you have any suggestion the workaround to meet them?
Best regards,
Kanae