Part Number: PROCESSOR-SDK-AM437X
Other Parts Discussed in Thread: INA226
Tool/software: Linux
Hi,
I would like to turn on the INA266 sensors on the EVM board. But I have difficulties to map the linux kernel driver into the dts file, since there are two ina266 sensors on board, one on address 0x40, the other on address 0x41. Is it legal to map multiple devices into one driver? If not, how should I proceed this?
Thanks.
Jerry Wang