This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM385: BT.656 and LVDS design question

Part Number: DM385
Other Parts Discussed in Thread: DM388,

Hi,

I have a IC to interface camera link signals to get LVCOMS o/p

Camera link LVDS differential pair signals -->---DS90CR286A-->--- 28 bit LVCMOS o/p-->--- DM385 Video Input

Similarly can I use the same IC for BTU656 LVDS video input signals instead of camera link?

Please suggest an IC to interface BT.656 LVDS signals

BT.656 LVDS signals (There are no positive and negative signals)--->--- IC??--->--- 28 bit LVCMOS o/p--->--- DM385 Video Input

Or can the DM385 directly take BT.656 video inputs, if yes please specify the pin numbers which can take BT.656 Video inputs in DM385/DM388

Kindly answer my questions appropriately.

Thanks & Regards

Krishna