I have the following questions regarding the DSP p/n TMS320C6701GJCA120?
Please also see the attached pdf document and the below link for the data sheet for your convenience.
http://focus.ti.com/docs/prod/folders/print/tms320c6701.html
3833.4 questions regarding TI DSP P_.pdf
1. Regarding the RSV signals that specify dedicated resistors, our
legacy design uses 14 kilo-ohm pull up resistors for the past 8 years in
production efforts. Can you please tell me if there is any impact to
the DSP operation by using 14 kilo-ohm resistors instead of 20 kilo-ohm
resistors?
2. Regarding the below EMU0/EMU1 signals, our legacy design has used 3.01
kilo-ohm pull up resistors for the past 8 years in production efforts. Can
you please tell me if there is any impact to the DSP operation by using
3.01 kilo-ohm resistors instead of 20 kilo-ohm resistors?
3. Regarding the below PLLF/PLLG signals, our legacy design has uses R1 =
60.4 ohms, C2 = 560 pF, and C1 = 0.027 uF for the past 8 years in
production efforts. Our configuration is the same as the below per DSP
data sheet TMS320C6701GJCA120 except R1 and C1 are swapped. The R1 in
our legacy design is common to PLLF instead of PLLG and C1 in our legacy
design is common to PLLG instead of PLLF. Can you please let me know if
this is a problem?
4. Regarding decoupling capacitors DSP p/n TMS320C6701GJCA120, we have
been using 4 of 0.1 uF capacitors decoupling between 1.8 Vdc core voltage
and 3.3 Vdc I/O voltage in our legacy design for the past 8 years. Do
you have any idea why this is necessary or what the purpose of this
configuration is?
Tom Walker