Part Number: DRA74
Tool/software: Linux
hi ,
U-Boot SPL 2014.07-00009-g6231016-dirty (Sep 04 2018 - 19:04:05)
DRA752-GP ES2.0
Enable clock domain - 4a009700
Enable clock domain - 4a009300
Enable clock domain - 4a008b00
Enable clock domain - 4a008d00
Enable clock domain - 4a0093c0
Enable clock domain - 4a008700
Enable clock module - 4a008728
Enable clock module - 4a008b30
Enable clock module - 4a008b38
Enable clock module - 4a008d20
Enable clock module - 4ae07838
Enable clock module - 4a009760
Enable clock module - 4a009768
Enable clock module - 4a009770
Enable clock module - 4a009778
Enable clock module - 4a009780
Enable clock module - 4a009810
Enable clock module - 4a009818
Enable clock module - 4a008778
Enable clock module - 4a008780
Enable clock module - 4ae07840
Enable clock module - 4a009328
Enable clock module - 4a009330
Enable clock module - 4a009738
Enable clock module - 4ae07830
Enable clock module - 4a009850
Enable clock module - 4a0097a0
Enable clock module - 4a0093d0
Enable clock module - 4a009838
Enable clock domain - 4a009700
Enable clock domain - 4a009300
Enable clock domain - 4a008b00
Enable clock domain - 4a008d00
Enable clock domain - 4a0093c0
Enable clock domain - 4a008700
optimize_vcore_voltage:efuse 0x4a0025f4 bits=16 Vnom=1030, using efuse value 1049
do_scale_vcore: volt - 1049 offset_code - 0x3d
IODELAY: IO delay recalibration successfully completed
optimize_vcore_voltage:efuse 0x4a003b20 bits=16 Vnom=1090, using efuse value 1070
do_scale_vcore: volt - 1070 offset_code - 0x3f
optimize_vcore_voltage:efuse 0x4a003b10 bits=16 Vnom=1250, using efuse value 1075
do_scale_vcore: volt - 1075 offset_code - 0x40
optimize_vcore_voltage:efuse 0x4a0025e0 bits=16 Vnom=1060, using efuse value 990
do_scale_vcore: volt - 990 offset_code - 0x37
optimize_vcore_voltage:efuse 0x4a0025cc bits=16 Vnom=1060, using efuse value 1005
do_scale_vcore: volt - 1005 offset_code - 0x39
setup_dplls
core Dpll locked, but not for ideal M = 266,N = 4 values, current values are M = 532,N= 9Core DPLL configured
per Dpll locked, but not for ideal M = 96,N = 4 values, current values are M = 1920,N= ����N��Q??DPLL locked
mpu Dpll locked, but not for ideal M = 500,N = 9 values, current values are M = 1470,N= 24MPU DPLL locked
>>sdram_init()
in_sdram = 0
>>do_sdram_init() 4c000000
<<do_sdram_init() 4c000000
>>do_sdram_init() 4d000000
HW leveling success
<<do_sdram_init() 4d000000
get_ram_size() successful<<sdram_init()
>>spl:board_init_r()
mmc_init: 0, time 85
Using default environment
Destroy Hash Table: 4031ab30 table = 00000000
Create Hash Table: N=377
DELETE CANDIDATE: "optargs"
hdelete: DELETE key "optargs"
DELETE ERROR ##############################
INSERT: free(data = 81280170)
INSERT: done
serial# not set, setting...
Initial value for argc=3
Final value for argc=3
boot device - 5
ti_spi_set_speed: hz: 48000000, clock divider 0
spi_claim_bus: bus:0 cs:0
spi_xfer: bus:0 cs:0 bitlen:8 words:1 flags:1
tx cmd 003a0fff dc 00000005 data 9f
tx done, status 00010002
spi_xfer: bus:0 cs:0 bitlen:40 words:5 flags:2
rx cmd 00390fff dc 00000005
rx done, status 00020002, read ef
rx cmd 00390fff dc 00000005
rx done, status 00030002, read 40
rx cmd 00390fff dc 00000005
rx done, status 00040002, read 17
rx cmd 00390fff dc 00000005
rx done, status 00050002, read 00
rx cmd 00390fff dc 00000005
rx done, status 00060002, read 00
spi_cs_deactivate: 0x812801b0
SF: Got idcodes
00000000: ef 40 17 00 00 .@...
spi_claim_bus: bus:0 cs:0
spi_xfer: bus:0 cs:0 bitlen:8 words:1 flags:1
tx cmd 003a0fff dc 00000005 data 35
tx done, status 00010002
spi_xfer: bus:0 cs:0 bitlen:8 words:1 flags:2
rx cmd 00390fff dc 00000005
rx done, status 00020002, read 02
spi_cs_deactivate: 0x812801b0
spi_release_bus: bus:0 cs:0
SF: winspan: QEB is already set
spi_release_bus: bus:0 cs:0
spi_claim_bus: bus:0 cs:0
spi_xfer: bus:0 cs:0 bitlen:0 words:0 flags:8
spi_xfer: bus:0 cs:0 bitlen:0 words:0 flags:10
spi_release_bus: bus:0 cs:0
Recovery Command: "???????????????????????????????"
spl_mmc_load_image
boot mode - FAT
Using default environment
Destroy Hash Table: 4031ab30 table = 81280b40
Create Hash Table: N=377
DELETE CANDIDATE: "optargs"
hdelete: DELETE key "optargs"
DELETE ERROR ##############################
INSERT: free(data = 81283578)
INSERT: done
reading u-boot.img
VFAT Support enabled
FAT32, fat_sect: 32, fatlength: 977
Rootdir begins at cluster: 2, sector: 1986, offset: f8400
Data begins at: 1984
Sector size: 512, cluster size: 1
FAT read sect=1986, clust_size=1, DIRENTSPERBLOCK=16
RootMismatch: |mlo||
Rootvfatname: |dra7-sg00-android.dtb|
RootMismatch: |dra7-s~1.dtb|dra7-sg00-android.dtb|
RootMismatch: |dra7-s~1.dtb||
Rootvfatname: |u-boot.img|
RootName: u-boot.img, start: 0x189, size: 0x66c48
Filesize: 420936 bytes
64 bytes
gc - clustnum: 393, startsect: 2377
Size: 420936, got: 64
spl: payload image: U-Bo load addr: 0x807fffc0 size: 420936
reading u-boot.img
VFAT Support enabled
FAT32, fat_sect: 32, fatlength: 977
Rootdir begins at cluster: 2, sector: 1986, offset: f8400
Data begins at: 1984
Sector size: 512, cluster size: 1
FAT read sect=1986, clust_size=1, DIRENTSPERBLOCK=16
RootMismatch: |mlo||
Rootvfatname: |dra7-sg00-android.dtb|
RootMismatch: |dra7-s~1.dtb|dra7-sg00-android.dtb|
RootMismatch: |dra7-s~1.dtb||
Rootvfatname: |u-boot.img|
RootName: u-boot.img, start: 0x189, size: 0x66c48
Filesize: 420936 bytes
420936 bytes
gc - clustnum: 393, startsect: 2377
gc - clustnum: 10209, startsect: 12193
Size: 420936, got: 420936
Jumping to U-Boot
image entry point: 0x80800000
initcall: 8083bda0
U-Boot 2014.07-00009-g6231016-dirty (Sep 04 2018 - 19:04:05)
initcall: 80808984
U-Boot code: 80800000 -> 8085BC40 BSS: -> 810AAE74
initcall: 808009d8
CPU : DRA752-GP ES2.0
initcall: 8080099c
Board: DRA7xx
initcall: 80808aa4
I2C: ready
initcall: 80808a8c
DRAM: initcall: 8080097c
>>sdram_init()
initcall: 80808ca0
Monitor len: 008AAE74
Ram size: 7F000000
Ram top: FF000000
initcall: 8080871c
initcall: 80808904
TLB table from 00000000 to feff0000
initcall: 80808740
initcall: 808088a8
Reserving 8875k for U-Boot at: fe745000
initcall: 8080886c
Reserving 16512k for malloc() at: fd725000
initcall: 80808a44
Reserving 112 Bytes for Board Info at: fd724f90
initcall: 80808748
initcall: 80808834
Reserving 496 Bytes for Global Data at: fd724da0
initcall: 808087c0
initcall: 8080875c
initcall: 80808c88
__dram_init_banksize:
[0]start = 2147483648, size = 2130706432, [1]start = 8589934592, size = 2147483648, ram size = 4294967296
initcall: 80808b40
RAM Configuration:
Bank #0: 80000000 2 GiB
Bank #1: 00000000 2 GiB
DRAM: 4 GiB
initcall: 808087a4
New Stack Pointer is: 0000000a
initcall: 80808a14
initcall: 808089b4
Relocation Offset is: 7df45000
Relocating to 00000000, new gd at fe745000, sp at 00000000
initcall: fe74dd78
initcall: fe74ded4
initcall: 80808ec4
dram_bank_mmu_setup: bank: 0
dram_bank_mmu_setup: bank: 1
initcall: 808039e4
initcall: 80808d80
initcall: 80808eb4
initcall: 80808e98
Now running in RAM - U-Boot at: 0000000a
initcall: 80808da8
initcall: 80808e74
initcall: 80808d70
initcall: 80808db0
initcall: 80808db8
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
initcall: 80808e44
mmc_init: 0, time 56
Using default environment
Destroy Hash Table: fe79fa84 table = 00000000
Create Hash Table: N=377
DELETE CANDIDATE: "optargs"
hdelete: DELETE key "optargs"
DELETE ERROR ##############################
INSERT: free(data = fd7252d8)
INSERT: done
initcall: 80808ef8
initcall: 8081c208
initcall: 80808e34
initcall: 80819858
Initial value for argc=3
Final value for argc=3
Initial value for argc=3
Final value for argc=3
Initial value for argc=3
Final value for argc=3
initcall: 80803658
initcall: 80808e24
initcall: 80808e04
initcall: 80808de4
Net: phy_micrel reset
<ethaddr> not set. Validating first E-fuse MAC
Initial value for argc=3
Final value for argc=3
Initial value for argc=3
Final value for argc=3
Phy not found
PHY status read failed
cpsw connected to Generic PHY
cpsw
initcall: 80808dd8
Initial value for argc=3
Final value for argc=3
### main_loop entered: bootdelay=3
### main_loop: bootcmd="run mmcboot;"
Hit any key to stop autoboot: 0
mmc_init: 0, time 82
switch to partitions #0, OK
mmc0 is current device
mmc_init: 0, time 83
SD/MMC found on device 0
reading uEnv.txt
VFAT Support enabled
FAT32, fat_sect: 32, fatlength: 977
Rootdir begins at cluster: 2, sector: 1986, offset: f8400
Data begins at: 1984
Sector size: 512, cluster size: 1
FAT read sect=1986, clust_size=1, DIRENTSPERBLOCK=16
RootMismatch: |mlo||
Rootvfatname: |dra7-sg00-android.dtb|
RootMismatch: |dra7-s~1.dtb|dra7-sg00-android.dtb|
RootMismatch: |dra7-s~1.dtb||
Rootvfatname: |u-boot.img|
RootMismatch: |u-boot.img|u-boot.img|
RootMismatch: |u-boot.img||
Rootvfatname: |uimage|
RootMismatch: |uimage|uimage|
RootMismatch: |uimage||
Rootvfatname: |uenv.txt|
RootName: uenv.txt, start: 0x26ed, size: 0xc7
Filesize: 199 bytes
199 bytes
gc - clustnum: 9965, startsect: 11949
Size: 199, got: 199
199 bytes read in 64 ms (2.9 KiB/s)
Initial value for argc=3
Final value for argc=3
Loaded environment from uEnv.txt
Importing environment from mmc0 ...
INSERT: free(data = fd729910)
INSERT: done
Command failed, result=1reading uImage
VFAT Support enabled
FAT32, fat_sect: 32, fatlength: 977
Rootdir begins at cluster: 2, sector: 1986, offset: f8400
Data begins at: 1984
Sector size: 512, cluster size: 1
FAT read sect=1986, clust_size=1, DIRENTSPERBLOCK=16
RootMismatch: |mlo||
Rootvfatname: |dra7-sg00-android.dtb|
RootMismatch: |dra7-s~1.dtb|dra7-sg00-android.dtb|
RootMismatch: |dra7-s~1.dtb||
Rootvfatname: |u-boot.img|
RootMismatch: |u-boot.img|u-boot.img|
RootMismatch: |u-boot.img||
Rootvfatname: |uimage|
RootName: uimage, start: 0x467, size: 0x450bc0
Filesize: 4524992 bytes
4524992 bytes
gc - clustnum: 1127, startsect: 3111
Size: 4524992, got: 4524992
4524992 bytes read in 287 ms (15 MiB/s)
Initial value for argc=3
Final value for argc=3
Booting from mmc0 ...
Initial value for argc=3
Final value for argc=3
Initial value for argc=3
Final value for argc=3
reading dra7-sg00-android.dtb
VFAT Support enabled
FAT32, fat_sect: 32, fatlength: 977
Rootdir begins at cluster: 2, sector: 1986, offset: f8400
Data begins at: 1984
Sector size: 512, cluster size: 1
FAT read sect=1986, clust_size=1, DIRENTSPERBLOCK=16
RootMismatch: |mlo||
Rootvfatname: |dra7-sg00-android.dtb|
RootName: dra7-s~1.dtb, start: 0xc4, size: 0x18964
Filesize: 100708 bytes
100708 bytes
gc - clustnum: 196, startsect: 2180
Size: 100708, got: 100708
100708 bytes read in 48 ms (2 MiB/s)
Initial value for argc=3
Final value for argc=3
## Current stack ends at 0xfd7249e8 * kernel: cmdline image address = 0x80300000
## Booting kernel from Legacy Image at 80300000 ...
Image Name: Linux-3.14.57-00090-g525925a-dir
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 4524928 Bytes = 4.3 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
kernel data at 0x80300040, len = 0x00450b80 (4524928)
## Skipping init Ramdisk
## No init Ramdisk
ramdisk start = 0x00000000, ramdisk end = 0x00000000
* fdt: cmdline image address = 0x82f80000
## Checking for 'FDT'/'FDT Image' at 82f80000
* fdt: raw FDT blob
## Flattened Device Tree blob at 82f80000
Booting using the fdt blob at 0x82f80000
of_flat_tree at 0x82f80000 size 0x00018964
Initial value for argc=3
Final value for argc=3
Loading Kernel Image ... OK
kernel loaded at 0x80008000, end = 0x80458b80
images.os.start = 0x80300000, images.os.end = 0x80750bc0
images.os.load = 0x80008000, load_end = 0x80458b80
using: FDT
## initrd_high = 0xffffffff, copy_to_ram = 1
ramdisk load start = 0x00000000, ramdisk load end = 0x00000000
## device tree at 82f80000 ... 82f98963 (len=112996 [0x1B964])
Loading Device Tree to 8ffe4000, end 8ffff963 ... OK
Initial value for argc=3
Final value for argc=3
Updating property '/ocp/ethernet@48484000/slave@48480200/mac-address' = 4c 3f d3 05 14 96
Updating property '/ocp/ethernet@48484000/slave@48480200/local-mac-address' = 4c 3f d3 05 14 96
## Transferring control to Linux (at address 80008000)...
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 3.14.57-00090-g525925a-dirty (uidq1759@hzhrd003x608) (gcc version 4.8 (GCC) ) #1 SMP PREEMPT Tue Sep 4 11:54:54 CST 2018
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c7387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] Ignoring memory below PHYS_OFFSET: 0x00000000-0x80000000
[ 0.000000] Machine model: TI DRA742
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000095800000, size 56 MiB
[ 0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[ 0.000000] cma: CMA: reserved 24 MiB at ae000000
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] On node 0 totalpages: 519680
[ 0.000000] free_area_init_node: node 0, pgdat c0806580, node_mem_map ecff1000
[ 0.000000] Normal zone: 1520 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 194560 pages, LIFO batch:31
[ 0.000000] HighMem zone: 2544 pages used for memmap
[ 0.000000] HighMem zone: 325120 pages, LIFO batch:31
[ 0.000000] DRA752 ES2.0
[ 0.000000] PERCPU: Embedded 7 pages/cpu @ecfab000 s7872 r8192 d12608 u32768
[ 0.000000] pcpu-alloc: s7872 r8192 d12608 u32768 alloc=8*4096
[ 0.000000] pcpu-alloc: [0] 0 [0] 1
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 518160
[ 0.000000] Kernel command line: root=/dev/mmcblk0p2 rw console=ttyS2,115200 androidboot.console=ttyS2 init=/init rootfstype=ext4 rootwait drm.rnodes=1 snd.slots_reserved=1,1 androidboot.selinux=permissive debug root=/dev/mmcblk1p2 rw console=ttyS2,115200 androidboot.console=ttyS2 init=/init rootfstype=ext4 rootwait drm.rnodes=1 snd.slots_reserved=1,1 androidboot.selinux=permissive
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 1970632K/2078720K available (5795K kernel code, 294K rwdata, 1812K rodata, 287K init, 362K bss, 108088K reserved, 1300480K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xf0000000 - 0xff000000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xef800000 ( 760 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0775f74 (7608 kB)
[ 0.000000] .init : 0xc0776000 - 0xc07bdec0 ( 288 kB)
[ 0.000000] .data : 0xc07be000 - 0xc0807808 ( 295 kB)
[ 0.000000] .bss : 0xc0807814 - 0xc0862334 ( 363 kB)
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Dump stacks of tasks blocking RCU-preempt GP.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] OMAP clockevent source: timer1 at 32786 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 65536000000000ns
[ 0.000000] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000427] Architected cp15 timer(s) running at 6.14MHz (virt).
[ 0.000462] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 2794592043008ns
[ 0.000470] Switching to timer-based delay loop
[ 0.001150] Console: colour dummy device 80x30
[ 0.001174] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[ 0.001187] pid_max: default: 32768 minimum: 301
[ 0.001288] Security Framework initialized
[ 0.001302] SELinux: Initializing.
[ 0.001346] SELinux: Starting in permissive mode
[ 0.001386] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001395] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.022532] Initializing cgroup subsys freezer
[ 0.022567] CPU: Testing write buffer coherency: ok
[ 0.022845] /cpus/cpu@0 missing clock-frequency property
[ 0.022880] /cpus/cpu@1 missing clock-frequency property
[ 0.022892] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.022909] Setting up static identity map for 0x805af198 - 0x805af1f0
[ 0.080725] CPU1: Booted secondary processor
[ 0.080751] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.080881] Brought up 2 CPUs
[ 0.080896] SMP: Total of 2 processors activated (24.59 BogoMIPS).
[ 0.080903] CPU: All CPU(s) started in SVC mode.
[ 0.081341] devtmpfs: initialized
[ 0.082210] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.083751] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.094072] omap_hwmod: tptc0 using broken dt data from edma-controller
[ 0.094542] omap_hwmod: tptc1 using broken dt data from edma-controller
[ 0.193758] omap_hwmod: tpcc: _wait_target_disable failed
[ 0.262672] pinctrl core: initialized pinctrl subsystem
[ 0.263376] regulator-dummy: no parameters
[ 0.265259] NET: Registered protocol family 16
[ 0.266391] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.313858] syscon 4a002000.tisysconcore: regmap [mem 0x4a002000-0x4a0026cf] registered
[ 0.314171] syscon 4a002e00.tisyscon: regmap [mem 0x4a002e00-0x4a002e7b] registered
[ 0.316688] OMAP GPIO hardware version 0.1
[ 0.322584] irq: no irq domain found for /ocp/pinmux@4a003400 !
[ 0.328512] platform 55020000.ipu: assigned reserved memory node ipu2_cma@95800000
[ 0.346199] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.346210] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.349138] OMAP DMA hardware revision 0.0
[ 0.370532] bio: create slab <bio-0> at 0
[ 0.383524] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
[ 0.389197] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver
[ 0.389937] evm_3v3_sd: 3300 mV
[ 0.390238] evm_3v3_sw: 3300 mV
[ 0.390513] aic_dvdd: 1800 mV
[ 0.390588] aic_dvdd: supplied by evm_3v3_sw
[ 0.392560] vmmcwl_fixed: 1800 mV
[ 0.395227] i2c-core: driver [palmas] using legacy suspend method
[ 0.395236] i2c-core: driver [palmas] using legacy resume method
[ 0.395758] SCSI subsystem initialized
[ 0.396497] usbcore: registered new interface driver usbfs
[ 0.396642] usbcore: registered new interface driver hub
[ 0.396810] usbcore: registered new device driver usb
[ 0.398905] palmas 0-0058: IRQ missing: skipping irq request
[ 0.399235] palmas 0-0058: Muxing GPIO 2e, PWM 0, LED 0
[ 0.399379] prom_parse: Bad cell count for /ocp/i2c@48070000/tps659038@58
[ 0.401381] smps123: 850 <--> 1250 mV at 1070 mV
[ 0.402931] smps45: 850 <--> 1150 mV at 990 mV
[ 0.404473] smps6: 850 <--> 1250 mV at 1080 mV
[ 0.405869] smps7: 850 <--> 1060 mV at 1050 mV
[ 0.407410] smps8: 850 <--> 1250 mV at 1010 mV
[ 0.408788] smps9: 1800 mV
[ 0.411820] ldo1: 1800 <--> 3300 mV at 3000 mV
[ 0.420926] ldo2: 3300 mV
[ 0.431084] ldo3: 1800 mV
[ 0.431913] LDO4: at 1800 mV
[ 0.432465] LDO5: no parameters
[ 0.433014] LDO6: no parameters
[ 0.433571] LDO7: no parameters
[ 0.434125] LDO8: no parameters
[ 0.440948] ldo9: 1050 mV
[ 0.450969] ldoln: 1800 mV
[ 0.461033] ldousb: 3300 mV
[ 0.461710] REGEN1: no parameters
[ 0.462226] regen2: no parameters
[ 0.462771] sysen1: no parameters
[ 0.463315] sysen2: no parameters
[ 0.463893] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.464310] omap_i2c 48072000.i2c: bus 1 rev0.12 at 50 kHz
[ 0.465368] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
[ 0.466057] omap_i2c 4807a000.i2c: bus 3 rev0.12 at 400 kHz
[ 0.466330] media: Linux media interface: v0.10
[ 0.466463] Linux video capture interface: v2.00
[ 0.466674] pps_core: LinuxPPS API ver. 1 registered
[ 0.466681] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.467768] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[ 0.468510] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 0.470169] cfg80211: Calling CRDA to update world regulatory domain
[ 0.470907] Switched to clocksource arch_sys_counter
[ 0.487508] NET: Registered protocol family 2
[ 0.488187] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.488250] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.488374] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.488417] TCP: reno registered
[ 0.488428] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.488458] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.488648] NET: Registered protocol family 1
[ 0.490733] hw perfevents: enabled with ARMv7 Cortex-A15 PMU driver, 7 counters available
[ 0.491219] sv_uio_probe
[ 0.491228] sv_uio_set_gpio enter!
[ 0.491368] sv_uio_set_gpio end!
[ 0.491810] sv_watchdog_probe
[ 0.494431] futex hash table entries: 512 (order: 3, 32768 bytes)
[ 0.494488] audit: initializing netlink subsys (disabled)
[ 0.494538] audit: type=2000 audit(0.489:1): initialized
[ 0.495424] bounce pool size: 64 pages
[ 0.495668] VFS: Disk quotas dquot_6.5.2
[ 0.495771] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.496144] NTFS driver 2.1.30 [Flags: R/W].
[ 0.496196] fuse init (API version 7.22)
[ 0.496477] msgmni has been set to 1468
[ 0.496617] SELinux: Registering netfilter hooks
[ 0.498506] io scheduler noop registered
[ 0.498516] io scheduler deadline registered
[ 0.498545] io scheduler cfq registered (default)
[ 0.504474] pinctrl-single 4a003400.pinmux: 281 pins at pa fc003400 size 1124
[ 0.508266] OMAP DSS rev 6.1
[ 0.520957] tlc59108 0-0040: Successfully initialized tlc59108
[ 0.522327] pbias_mmc_omap5: 1800 <--> 3300 mV at 3000 mV
[ 0.523048] abb_mpu: 1100 <--> 1210 mV
[ 0.523385] abb_ivahd: 1060 <--> 1250 mV
[ 0.523709] abb_dspeve: 1060 <--> 1250 mV
[ 0.524039] abb_gpu: 1060 <--> 1280 mV
[ 0.524567] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.527942] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 300, base_baud = 3000000) is a 8250
[ 1.461570] console [ttyS2] enabled
[ 1.465716] 48066000.serial: ttyS4 at MMIO 0x48066000 (irq = 301, base_baud = 3000000) is a 8250
[ 1.475213] 4ae2b000.serial: ttyS9 at MMIO 0x4ae2b000 (irq = 303, base_baud = 3000000) is a 8250
[ 1.485188] OS:MSG:serial_dra7xx_init:dra7xx-serio
[ 1.490103] serial_dra7xx_probe
[ 1.493519] serial_dra7xx_probe
[ 1.498022] omap_rng 48090000.rng: OMAP Random Number Generator ver. 20
[ 1.504975] [drm] Initialized drm 1.1.0 20060810
[ 1.519374] brd: module loaded
[ 1.527592] loop: module loaded
[ 1.532691] mcu_spi_init
[ 1.537002] mcu_spi_probe
[ 1.539798]
[ 1.539798] mcu_spi_cs = 1
[ 1.557129] m25p80 spi32766.0: found s25fl064k, expected w25q64
[ 1.563102] m25p80 spi32766.0: s25fl064k (8192 Kbytes)
[ 1.568301] 6 ofpart partitions found on MTD device spi32766.0
[ 1.574171] Creating 6 MTD partitions on "spi32766.0":
[ 1.579332] 0x000000000000-0x000000020000 : "XLOADER"
[ 1.584922] 0x000000080000-0x000000100000 : "BOOTLOADER"
[ 1.590721] 0x000000120000-0x000000140000 : "MISC"
[ 1.596012] 0x000000150000-0x000000660000 : "DATA"
[ 1.601297] 0x000000670000-0x000000680000 : "FLAG"
[ 1.606568] 0x000000690000-0x000000780000 : "DATA3"
[ 1.612187] tun: Universal TUN/TAP device driver, 1.6
[ 1.617259] tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
[ 1.624253] i2c /dev entries driver
[ 1.628769] ENTER AR111,client->addr=48
[ 1.632639] node->name =camera_max96706
[ 1.636489] node->name =camera_max96706
[ 1.640361] gpio num =157
[ 1.643001] max96706_get_gpios status=0
[ 1.656859] max96706_set_gpios status=0
[ 1.660710] max96706_AR 3-0048: Camera max96706 sensor driver registered
[ 1.667584] rvc_detect_init
[ 1.670691] rvc_detect_probe
[ 1.674674] vpe 489d0000.vpe: loading firmware vpdma-1b8.bin
[ 1.681752] vip 48970000.vip: loading firmware vpdma-1b8.bin
[ 1.688474] vip 48990000.vip: loading firmware vpdma-1b8.bin
[ 1.694566] vpe 489d0000.vpe: Device registered as /dev/video0
[ 1.700610] usbcore: registered new interface driver uvcvideo
[ 1.706406] vip 48970000.vip: VPDMA firmware loaded
[ 1.711328] vip 48990000.vip: VPDMA firmware loaded
[ 1.716248] vip_of_probe no node-number
[ 1.720361] vip2-s0: Port A enabled but no endpoints found[ 1.720938] USB Video Class driver (1.1.1)
[ 1.720941] power_detect_init
[ 1.732844] vip_of_probe no node-number
[ 1.737207] vip1-s1: Using subdev max96706_AR 3-0048 for capture
[ 1.737327] power_detect_probe
[ 1.746352] max96706_enum_fmt index: 0 L.M
[ 1.750487] vip_of_probe no node-number
[ 1.754652] max96706_enum_fmt index: 1 L.M
[ 1.758781] vip2-s1: Port B enabled but no endpoints found
[ 1.764168] max96706_enum_fmt index: 2 L.M
[ 1.768485] max96706_enum_fmt index: 3 L.M
[ 1.772648] max96706_enum_fmt index: 4 L.M
[ 1.776779] max96706_enum_fmt index: 5 L.M
[ 1.776965] coproc iva_coproc: probe
[ 1.777073] Adding alias for supply vdd,iva_coproc -> vdd,4a0025cc.voltdm
[ 1.777077] Adding alias for supply vbb,iva_coproc -> vbb,4a0025cc.voltdm
[ 1.798115] max96706_enum_fmt index: 6 L.M
[ 1.802590] vip1-s1: vip Device registered as /dev/video1
[ 1.808662] coproc iva_coproc: coproc_probe result=0
[ 1.813754] coproc dsp_coproc: probe
[ 1.817421] Adding alias for supply vdd,dsp_coproc -> vdd,4a0025e0.voltdm
[ 1.824274] Adding alias for supply vbb,dsp_coproc -> vbb,4a0025e0.voltdm
[ 1.832154] coproc dsp_coproc: coproc_probe result=0
[ 1.840649] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.885910] mmc_attach_sdio enter!
[ 1.890758] mmc_attach_sdio err=-110!
[ 1.921307] 480ad000.mmc supply vmmc not found, using dummy regulator
[ 1.928027] omap_hsmmc 480ad000.mmc: could not set regulator OCR (-22)
[ 1.947654] mmc0: BKOPS_EN bit is not set
[ 1.954247] mmc0: new high speed DDR MMC card at address 0001
[ 1.960496] mmcblk0: mmc0:0001 032G34 29.1 GiB
[ 1.965236] mmcblk0boot0: mmc0:0001 032G34 partition 1 8.00 MiB
[ 1.970939] select_sdio_host: bcm_sdio_host assigned. (ecb88800)
[ 1.977452] mmcblk0boot1: mmc0:0001 032G34 partition 2 8.00 MiB
[ 1.977606] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
[ 1.990024] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
[ 1.995841] ------------------sv delay_set_gpio_work start----------------
[ 2.002824] mmcblk0: unknown partition table
[ 2.007583] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
[ 2.014173] mmcblk0boot1: unknown partition table
[ 2.020599] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
[ 2.027164] mmcblk0boot0: unknown partition table
[ 2.032387] omap-sham 4b101000.sham: initialization failed.
[ 2.038025] omap-sham: probe of 4b101000.sham failed with error -22
[ 2.041843] mmc_attach_sdio enter!
[ 2.043266] mmc_attach_sdio err=-110!
[ 2.047355] sd set 3.3V
[ 2.054354] hidraw: raw HID events driver (C) Jiri Kosina
[ 2.068374] ion_chunk_heap_create: base 2877292544 size 4194304 align 16384
[ 2.076026] ashmem: initialized
[ 2.080390] remoteproc0: 55020000.ipu is available
[ 2.085341] remoteproc0: Note: remoteproc is still under development and considered experimental.
[ 2.094387] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 2.104938] remoteproc0: Direct firmware load failed with error -2
[ 2.109824] mmc1: host does not support reading read-only switch. assuming write-enable.
[ 2.113485] mmc1: new high speed SDHC card at address aaaa
[ 2.125155] remoteproc0: Falling back to user helper
[ 2.125249] mmcblk1: mmc1:aaaa SS08G 7.40 GiB
[ 2.135472] u32 classifier
[ 2.136107] mmcblk1: p1 p2
[ 2.141054] Actions configured
[ 2.144507] Netfilter messages via NETLINK v0.30.
[ 2.149344] nf_conntrack version 0.5.0 (16384 buckets, 65536 max)
[ 2.155869] ctnetlink v0.93: registering with nfnetlink.
[ 2.160135] mmc_attach_sdio enter!
[ 2.160444] omap_hsmmc 480ad000.mmc: exceeding card's volts
[ 2.160447] mmc_sdio_init_card enter!
[ 2.169410] mmc2: queuing unknown CIS tuple 0x80 (2 bytes)
[ 2.170940] mmc2: queuing unknown CIS tuple 0x80 (3 bytes)
[ 2.172441] mmc2: queuing unknown CIS tuple 0x80 (3 bytes)
[ 2.175141] mmc2: queuing unknown CIS tuple 0x80 (7 bytes)
[ 2.196533] xt_time: kernel timezone is -0000
[ 2.201189] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 2.206658] arp_tables: (C) 2002 David S. Miller
[ 2.211363] TCP: cubic registered
[ 2.214690] Initializing XFRM netlink socket
[ 2.219055] NET: Registered protocol family 10
[ 2.224324] mip6: Mobile IPv6
[ 2.227326] ip6_tables: (C) 2000-2006 Netfilter Core Team
[ 2.230948] mmc2: queuing unknown CIS tuple 0x91 (3 bytes)
[ 2.230980] mmc2: new high speed SDIO card at address 0001
[ 2.243984] sit: IPv6 over IPv4 tunneling driver
[ 2.249102] mmc_attach_sdio: end!
[ 2.252894] NET: Registered protocol family 17
[ 2.257374] NET: Registered protocol family 15
[ 2.261914] Bridge firewalling registered
[ 2.265943] 8021q: 802.1Q VLAN Support v1.8
[ 2.270154] lib80211: common routines for IEEE802.11 drivers
[ 2.275850] lib80211_crypt: registered algorithm 'NULL'
[ 2.281139] Key type dns_resolver registered
[ 2.285427] NET: Registered protocol family 41
[ 2.290555] cpu cpu0: _opp_add_dynamic: duplicate OPPs detected. Existing: freq: 1176000000, volt: 1160000, enabled: 1. New: freq: 1176000000, volt: 1100000, enabled: 1
[ 2.305676] cpu cpu0: of_init_opp_table: Failed to add OPP 1176000000
[ 2.312247] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.voltdm
[ 2.318541] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.voltdm
[ 2.326810] Power Management for TI OMAP4+ devices.
[ 2.331905] ThumbEE CPU extension supported.
[ 2.336201] Registering SWP/SWPB emulation handler
[ 2.342519] vmmcwl_fixed: disabling
[ 2.346022] aic_dvdd: disabling
[ 2.349174] regulator-dummy: disabling
[ 2.353255] dmm 4e000000.dmm: workaround for errata i878 in use
[ 2.361294] dmm 4e000000.dmm: initialized all PAT entries
[ 2.369718] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 2.376395] [drm] No driver support for vblank timestamp query.
[ 2.406115] [drm] Enabling DMM ywrap scrolling
[ 2.486599] Console: switching to colour frame buffer device 160x45
[ 2.498554] omapdrm omapdrm.0: fb0: omapdrm frame buffer device
[ 2.504509] omapdrm omapdrm.0: registered panic notifier
[ 2.509849] [drm] Initialized omapdrm 1.0.0 20110917 on minor 0
[ 2.516079] [LYH]OS:MSG:lvds:maxim_lvds_probe:
[ 2.520680] MAXIM_LVDS 2-0040: [LYH]back light enable gpio is busy
[ 2.526915] [LYH]OS:MSG:lvds:maxim_lvds_probe: lvds->des_addr:68
[ 2.533733] sv atmel_mxt_ts_init in
[ 2.919089] atmel_mxt_ts 2-004a: Family: 164 Variant: 24 Firmware V1.0.AA Objects: 40
[ 2.931796] sv mxt_initialize_input_device call
[ 2.938056] atmel_mxt_ts 2-004a: T100 Touchscreen size X1279Y719
[ 2.944413] input: Atmel maXTouch Touchpad as /devices/44000000.ocp/48060000.i2c/i2c-2/2-004a/input/input0
[ 2.955892] sv mxt_initialize success
[ 5.354316] EXT4-fs (mmcblk1p2): recovery complete
[ 5.360833] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
[ 5.369012] VFS: Mounted root (ext4 filesystem) on device 179:26.
[ 5.376061] devtmpfs: mounted
[ 5.379221] Freeing unused kernel memory: 284K (c0776000 - c07bd000)
[ 5.421971] SELinux: 2048 avtab hash slots, 5509 rules.
[ 5.429912] SELinux: 2048 avtab hash slots, 5509 rules.
[ 5.435213] SELinux: 1 users, 2 roles, 467 types, 0 bools, 1 sens, 1024 cats
[ 5.442408] SELinux: 86 classes, 5509 rules
[ 5.447935] SELinux: Completing initialization.
[ 5.452589] SELinux: Setting up existing superblocks.
[ 5.457761] SELinux: initialized (dev rootfs, type rootfs), uses genfs_contexts
[ 5.465127] SELinux: initialized (dev bdev, type bdev), not configured for labeling
[ 5.472838] SELinux: initialized (dev proc, type proc), uses genfs_contexts
[ 5.479847] SELinux: initialized (dev tmpfs, type tmpfs), uses transition SIDs
[ 5.487131] SELinux: initialized (dev devtmpfs, type devtmpfs), uses transition SIDs
[ 5.495356] SELinux: initialized (dev debugfs, type debugfs), uses genfs_contexts
[ 5.511618] SELinux: initialized (dev sockfs, type sockfs), uses task SIDs
[ 5.518534] SELinux: initialized (dev pipefs, type pipefs), uses task SIDs
[ 5.525458] SELinux: initialized (dev anon_inodefs, type anon_inodefs), not configured for labeling
[ 5.534614] SELinux: initialized (dev aio, type aio), not configured for labeling
[ 5.542183] SELinux: initialized (dev devpts, type devpts), uses transition SIDs
[ 5.549657] SELinux: initialized (dev mqueue, type mqueue), uses transition SIDs
[ 5.557112] SELinux: initialized (dev selinuxfs, type selinuxfs), uses genfs_contexts
[ 5.565067] SELinux: initialized (dev drm, type drm), not configured for labeling
[ 5.572603] SELinux: initialized (dev mmcblk1p2, type ext4), uses xattr
[ 5.579271] SELinux: initialized (dev tmpfs, type tmpfs), uses transition SIDs
[ 5.586569] SELinux: initialized (dev sysfs, type sysfs), uses genfs_contexts
[ 5.628256] audit: type=1403 audit(5.619:2): policy loaded auid=4294967295 ses=4294967295
[ 5.675651] init: Warning! Service rvcd needs a SELinux domain defined; please fix!
[ 5.684001] audit: type=1400 audit(5.679:3): avc: denied { execute } for pid=970 comm="init" name="rvcd" dev="mmcblk1p2" ino=261124 scontext=u:r:init:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=1
[ 5.685259] audit: type=1400 audit(5.679:4): avc: denied { entrypoint } for pid=971 comm="init" path="/sbin/ueventd" dev="mmcblk1p2" ino=261128 scontext=u:r:ueventd:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=1
[ 5.723519] audit: type=1400 audit(5.719:5): avc: denied { execute_no_trans } for pid=970 comm="init" path="/sbin/rvcd" dev="mmcblk1p2" ino=261124 scontext=u:r:init:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=1
[ 5.765988] audit: type=1400 audit(5.759:6): avc: denied { read } for pid=971 comm="ueventd" path="/sbin/ueventd" dev="mmcblk1p2" ino=261128 scontext=u:r:ueventd:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=1
[ 5.789862] audit: type=1400 audit(5.779:7): avc: denied { open } for pid=971 comm="ueventd" path="/ueventd.rc" dev="mmcblk1p2" ino=1973 scontext=u:r:ueventd:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=1
[ 5.809705] audit: type=1400 audit(5.799:8): avc: denied { getattr } for pid=971 comm="ueventd" path="/ueventd.rc" dev="mmcblk1p2" ino=1973 scontext=u:r:ueventd:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=1
[ 5.881696] rvc_detect_fasync
[ 5.901577] SELinux: initialized (dev mtd_inodefs, type mtd_inodefs), not configured for labeling
[ 5.912137] SELinux: initialized (dev mtd_inodefs, type mtd_inodefs), not configured for labeling
[ 5.981511] audit: type=1400 audit(5.979:9): avc: denied { read } for pid=1191 comm="ueventd" name="etc" dev="mmcblk1p2" ino=1974 scontext=u:r:ueventd:s0 tcontext=u:object_r:unlabeled:s0 tclass=lnk_file permissive=1
[ 5.991752] max96706_s_fmt L.M
[ 5.991783] max96706_s_fmt L.M
[ 6.221393] SELinux: initialized (dev cgroup, type cgroup), uses genfs_contexts
[ 6.229168] SELinux: initialized (dev tmpfs, type tmpfs), uses transition SIDs
[ 6.263238] SELinux: initialized (dev tmpfs, type tmpfs), uses transition SIDs
[ 6.277829] SELinux: initialized (dev tmpfs, type tmpfs), uses transition SIDs
[ 6.286998] SELinux: initialized (dev cgroup, type cgroup), uses genfs_contexts
[ 6.360317] remoteproc0: powering up 55020000.ipu
[ 6.365156] remoteproc0: Booting fw image dra7-ipu2-fw.xem4, size 3894624
[ 6.372142] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1
[ 6.373694] rvc_detect_fasync
[ 6.373700] rvc_detect_release
[ 6.373702] rvc_detect_fasync
[ 6.449253] remoteproc0: remote processor 55020000.ipu is now up
[ 6.455841] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 6.461399] remoteproc0: registered virtio0 (type 7)
[ 6.464588] virtio_rpmsg_bus virtio0: creating channel rpmsg-rpc addr 0x65
[ 6.473549] rpmsg_rpc rpmsg0: probing service dce-callback with src 1024 dst 101
[ 6.481869] virtio_rpmsg_bus virtio0: creating channel rpmsg-rpc addr 0x66
[ 6.489195] rpmsg_rpc rpmsg1: probing service rpmsg-dce with src 1025 dst 102
[ 6.497130] rpmsg_rpc rpmsg0: published functions = 4
[ 6.502273] rpmsg_rpc rpmsg1: published functions = 8
[ 17.055299] omap_hwmod: mmu_ipu2: _wait_target_disable failed
[ 18.540964] random: nonblocking pool is initialized
[ 26.004291] fs_mgr: __mount(source=/dev/block/mmcblk0p9,target=/system,type=ext4)=-1
[ 26.012181] fs_mgr: Failed to mount an un-encryptable or wiped partition on/dev/block/mmcblk0p9 at /system options: (null) error: No such file or directory
[ 46.006865] fs_mgr: check_fs(): mount(/dev/block/mmcblk0p10,/cache,ext4)=-1
[ 46.014914] fs_mgr: Running /system/bin/e2fsck on /dev/block/mmcblk0p10
[ 46.101427] e2fsck: e2fsck 1.42.9 (28-Dec-2013)
[ 46.106021] e2fsck: /system/bin/e2fsck: No such file or directory while trying to open /dev/block/mmcblk0p10
[ 46.115917] e2fsck: Possibly non-existent device?
[ 46.120648] e2fsck: e2fsck terminated by exit(8)
[ 46.125522] fs_mgr: __mount(source=/dev/block/mmcblk0p10,target=/cache,type=ext4)=-1
[ 46.133352] fs_mgr: Failed to mount an un-encryptable or wiped partition on/dev/block/mmcblk0p10 at /cache options: (null) error: No such file or directory
[ 66.006899] fs_mgr: check_fs(): mount(/dev/block/mmcblk0p13,/data,ext4)=-1
[ 66.013864] fs_mgr: Running /system/bin/e2fsck on /dev/block/mmcblk0p13
[ 66.041369] e2fsck: e2fsck 1.42.9 (28-Dec-2013)
[ 66.045956] e2fsck: /system/bin/e2fsck: No such file or directory while trying to open /dev/block/mmcblk0p13
[ 66.055848] e2fsck: Possibly non-existent device?
[ 66.060581] e2fsck: e2fsck terminated by exit(8)
[ 66.065460] fs_mgr: __mount(source=/dev/block/mmcblk0p13,target=/data,type=ext4)=-1
[ 66.073199] fs_mgr: Failed to mount an un-encryptable or wiped partition on/dev/block/mmcblk0p13 at /data options: (null) error: No such file or directory
[ 66.087227] init: fs_mgr_mount_all returned an error
[ 66.092417] init: fs_mgr_mount_all returned unexpected error 255
[ 66.139410] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null)
[ 66.169790] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null)
[ 66.239799] audit: type=1400 audit(66.229:10): avc: denied { entrypoint } for pid=1564 comm="init" path="/sbin/healthd" dev="mmcblk1p2" ino=261127 scontext=u:r:healthd:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=1
[ 66.239945] init: Warning! Service servicemanager needs a SELinux domain defined; please fix!
[ 66.240523] init: Warning! Service vold needs a SELinux domain defined; please fix!
[ 66.241180] init: Warning! Service surfaceflinger needs a SELinux domain defined; please fix!
[ 66.286445] init: Warning! Service pvrsrvinit needs a SELinux domain defined; please fix!
[ 66.296267] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 66.304873] init: Warning! Service zygote needs a SELinux domain defined; please fix!
[ 66.311139] audit: type=1400 audit(66.309:11): avc: denied { read } for pid=1564 comm="healthd" path="/sbin/healthd" dev="mmcblk1p2" ino=261127 scontext=u:r:healthd:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=1
[ 66.312756] binder: 1564:1564 transaction failed 29189, size 0-0
[ 66.324542] audit: type=1400 audit(66.319:12): avc: denied { set_context_mgr } for pid=1565 comm="servicemanager" scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=binder permissive=1
[ 66.441178] PVR_K: UM DDK-(2917986) and KM DDK-(2917986) match. [ OK ]
[ 66.620428] audit: type=1400 audit(66.609:13): avc: denied { create } for pid=1580 comm="vold" name="179:24" scontext=u:r:init:s0 tcontext=u:object_r:block_device:s0 tclass=blk_file permissive=1
[ 66.654727] init: untracked pid 1563 exited with status 0
[ 66.661200] SELinux: initialized (dev configfs, type configfs), not configured for labeling
[ 66.670138] init: property 'ro.serialno' doesn't exist while expanding '${ro.serialno}'
[ 66.678659] init: cannot expand '${ro.serialno}' while writing to '/config/usb_gadget/g1/strings/0x409/serialnumber'
[ 66.694306] audit: type=1400 audit(66.689:14): avc: denied { entrypoint } for pid=1621 comm="init" path="/sbin/adbd" dev="mmcblk1p2" ino=261125 scontext=u:r:adbd:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=1
[ 66.715636] audit: type=1400 audit(66.709:15): avc: denied { entrypoint } for pid=1620 comm="init" path="/system/bin/sh" dev="mmcblk1p2" ino=1040 scontext=u:r:shell:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=1
[ 66.779350] audit: type=1400 audit(66.769:16): avc: denied { read } for pid=1620 comm="sh" path="/system/bin/linker" dev="mmcblk1p2" ino=1112 scontext=u:r:shell:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=1
[ 66.799985] audit: type=1400 audit(66.789:17): avc: denied { read } for pid=1620 comm="sh" name="vendor" dev="mmcblk1p2" ino=1976 scontext=u:r:shell:s0 tcontext=u:object_r:unlabeled:s0 tclass=lnk_file permissive=1
[ 66.819493] audit: type=1400 audit(66.809:18): avc: denied { open } for pid=1620 comm="sh" path="/system/lib/libc.so" dev="mmcblk1p2" ino=753 scontext=u:r:shell:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=1
[ 66.839698] audit: type=1400 audit(66.829:19): avc: denied { read } for pid=1621 comm="adbd" path="/sbin/adbd" dev="mmcblk1p2" ino=261125 scontext=u:r:adbd:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=1
[ 66.909668] init: Warning! Service bootanim needs a SELinux domain defined; please fix!
shell@jacinto6evm:/ $
shell@jacinto6evm:/ $
shell@jacinto6evm:/ $ [ 67.313791] healthd: No charger supplies found
[ 67.318454] healthd: No battery devices found
shell@jacinto6evm:/ $
shell@jacinto6evm:/ $
shell@jacinto6evm:/ $
shell@jacinto6evm:/ $ su
shell@jacinto6evm:/ #
shell@jacinto6evm:/ # cat /proc/meminfo[ 71.926630] init: Warning! Service uim needs a SELinux domain defined; please fix!
MemTotal: 2052836 kB
MemFree: 1621068 kB
MemAvailable: 1736804 kB
Buffers: 760 kB
Cached: 149420 kB
SwapCached: 0 kB
Active: 45604 kB
Inactive: 147480 kB
Active(anon): 42988 kB
Inactive(anon): 23800 kB
Active(file): 2616 kB
Inactive(file): 123680 kB
Unevictable: 0 kB
Mlocked: 0 kB
HighTotal: 1300480 kB
HighFree: 1071828 kB
LowTotal: 752356 kB
LowFree: 549240 kB
SwapTotal: 0 kB
SwapFree: 0 kB
Dirty: 2952 kB
Writeback: 18592 kB
AnonPages: 43060 kB
Mapped: 222920 kB
Shmem: 23812 kB
Slab: 12392 kB
SReclaimable: 4240 kB
SUnreclaim: 8152 kB
KernelStack: 744 kB
PageTables: 968 kB
NFS_Unstable: 0 kB
Bounce: 0 kB
WritebackTmp: 0 kB
CommitLimit: 1026416 kB
Committed_AS: 1504956 kB
VmallocTotal: 245760 kB
VmallocUsed: 90256 kB
VmallocChunk: 38916 kB
shell@jacinto6evm:/ #
shell@jacinto6evm:/ # [ 76.945234] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 81.963584] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 84.964510] audit_printk_skb: 30 callbacks suppressed
[ 84.969590] audit: type=1400 audit(84.959:30): avc: denied { execute } for pid=1570 comm="zygote" path="/data/dalvik-cache/arm/system@framework@boot.oat" dev="mmcblk1p2" ino=130626 scontext=u:r:init:s0 tcontext=u:object_r:dalvikcache_data_file:s0 tclass=file permissive=1
[ 85.162911] SELinux: initialized (dev tmpfs, type tmpfs), uses transition SIDs
[ 86.143296] warning: `main' uses 32-bit capabilities (legacy support in use)
[ 86.331943] audit: type=1400 audit(86.329:31): avc: denied { setcurrent } for pid=1659 comm="main" scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=process permissive=1
[ 86.347505] audit: type=1400 audit(86.339:32): avc: denied { dyntransition } for pid=1659 comm="main" scontext=u:r:init:s0 tcontext=u:r:system_server:s0 tclass=process permissive=1
[ 86.366784] audit: type=1400 audit(86.359:33): avc: denied { read } for pid=1666 comm="main" path=2F6465762F6173686D656D2F64616C76696B2D6D61696E207370616365202864656C6574656429 dev="tmpfs" ino=3587 scontext=u:r:system_server:s0 tcontext=u:object_r:init_tmpfs:s0 tclass=file permissive=1
[ 86.399304] audit: type=1400 audit(86.389:34): avc: denied { getopt } for pid=1659 comm="main" path="/dev/socket/zygote" scontext=u:r:system_server:s0 tcontext=u:r:init:s0 tclass=unix_stream_socket permissive=1
[ 86.455630] audit: type=1400 audit(86.449:35): avc: denied { execute } for pid=1659 comm="system_server" path="/system/framework/arm/services.odex" dev="mmcblk1p2" ino=1246 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=1
[ 86.486776] audit: type=1400 audit(86.479:36): avc: denied { execute_no_trans } for pid=1673 comm="system_server" path="/system/bin/patchoat" dev="mmcblk1p2" ino=1146 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=file permissive=1
[ 86.513991] audit: type=1400 audit(86.509:37): avc: denied { read } for pid=1673 comm="patchoat" name="vendor" dev="mmcblk1p2" ino=1976 scontext=u:r:system_server:s0 tcontext=u:object_r:unlabeled:s0 tclass=lnk_file permissive=1
[ 86.863199] audit: type=1400 audit(86.859:38): avc: denied { call } for pid=1659 comm="system_server" scontext=u:r:system_server:s0 tcontext=u:r:init:s0 tclass=binder permissive=1
[ 86.880097] audit: type=1400 audit(86.869:39): avc: denied { getattr } for pid=1565 comm="servicemanager" scontext=u:r:init:s0 tcontext=u:r:system_server:s0 tclass=process permissive=1
[ 86.914648] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 91.931325] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 96.359635] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 96.954815] binder: undelivered transaction 2381
[ 97.006332] binder: 1567:1636 transaction failed 29189, size 68-0
[ 97.073825] init: Warning! Service vehicle_reset needs a SELinux domain defined; please fix!
[ 97.083251] init: Warning! Service media needs a SELinux domain defined; please fix!
[ 97.092089] init: Warning! Service netd needs a SELinux domain defined; please fix!
[ 97.101727] init: Warning! Service zygote needs a SELinux domain defined; please fix!
[ 97.258686] audit_printk_skb: 9 callbacks suppressed
[ 97.263740] audit: type=1400 audit(97.249:43): avc: denied { sys_ptrace } for pid=1705 comm="vehicle.killall" capability=19 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=capability permissive=1
[ 97.317416] audit: type=1400 audit(97.309:44): avc: denied { create } for pid=1706 comm="iptables" scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=rawip_socket permissive=1
[ 97.349634] audit: type=1400 audit(97.339:45): avc: denied { getopt } for pid=1706 comm="iptables" lport=255 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=rawip_socket permissive=1
[ 97.421001] audit: type=1400 audit(97.409:46): avc: denied { execmem } for pid=1702 comm="mediaserver" scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=process permissive=1
[ 97.496666] audit: type=1400 audit(97.489:47): avc: denied { setopt } for pid=1717 comm="iptables" lport=255 scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=rawip_socket permissive=1
[ 97.562239] SELinux: initialized (dev tmpfs, type tmpfs), uses transition SIDs
130|shell@jacinto6evm:/ # [ 101.195979] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 106.155956] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 106.319438] binder: 1567:1636 transaction failed 29189, size 68-0
[ 106.342420] init: Warning! Service vehicle_reset needs a SELinux domain defined; please fix!
[ 106.354488] init: Warning! Service media needs a SELinux domain defined; please fix!
[ 106.366572] init: Warning! Service zygote needs a SELinux domain defined; please fix!
[ 106.671695] init: Warning! Service netd needs a SELinux domain defined; please fix!
[ 111.686626] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 116.701224] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 121.719620] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 124.550179] SELinux: initialized (dev tmpfs, type tmpfs), uses transition SIDs
[ 126.174893] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 127.313591] healthd: battery none chg=
[ 131.364783] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 134.542716] binder: 1567:1636 transaction failed 29189, size 68-0
[ 134.592398] init: Warning! Service vehicle_reset needs a SELinux domain defined; please fix!
[ 134.611313] init: Warning! Service netd needs a SELinux domain defined; please fix!
[ 134.621591] init: Warning! Service media needs a SELinux domain defined; please fix!
[ 134.630118] init: Warning! Service zygote needs a SELinux domain defined; please fix!
[ 135.005050] SELinux: initialized (dev tmpfs, type tmpfs), uses transition SIDs
[ 136.631227] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 141.367697] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 144.551347] binder: 1567:1636 transaction failed 29189, size 68-0
[ 144.592462] init: Warning! Service vehicle_reset needs a SELinux domain defined; please fix!
[ 144.604397] init: Warning! Service media needs a SELinux domain defined; please fix!
[ 144.613121] init: Warning! Service zygote needs a SELinux domain defined; please fix!
[ 144.881685] init: Warning! Service netd needs a SELinux domain defined; please fix!
130|shell@jacinto6evm:/ #
130|shell@jacinto6evm:/ #
130|shell@jacinto6evm:/ #
130|shell@jacinto6evm:/ # cat /proc/meminfo
MemTotal: 2052836 kB
MemFree: 1448384 kB
MemAvailable: 1664936 kB
Buffers: 1328 kB
Cached: 248888 kB
SwapCached: 0 kB
Active: 115100 kB
Inactive: 176624 kB
Active(anon): 41536 kB
Inactive(anon): 23780 kB
Active(file): 73564 kB
Inactive(file): 152844 kB
Unevictable: 0 kB
Mlocked: 0 kB
HighTotal: 1300480 kB
HighFree: 958312 kB
LowTotal: 752356 kB
LowFree: 490072 kB
SwapTotal: 0 kB
SwapFree: 0 kB
Dirty: 9756 kB
Writeback: 45824 kB
AnonPages: 41484 kB
Mapped: 302204 kB
Shmem: 23812 kB
Slab: 15088 kB
SReclaimable: 5648 kB
SUnreclaim: 9440 kB
KernelStack: 816 kB
PageTables: 1148 kB
NFS_Unstable: 0 kB
Bounce: 0 kB
WritebackTmp: 0 kB
CommitLimit: 1026416 kB
Committed_AS: 1535332 kB
VmallocTotal: 245760 kB
VmallocUsed: 91524 kB
VmallocChunk: 34284 kB
shell@jacinto6evm:/ #
shell@jacinto6evm:/ # [ 146.891201] init: Warning! Service uim needs a SELinux domain defined; please fix!
shell@jacinto6evm:/ #
shell@jacinto6evm:/ # [ 151.909746] init: Warning! Service uim needs a SELinux domain defined; please fix!
shell@jacinto6evm:/ #
shell@jacinto6evm:/ #
shell@jacinto6evm:/ #
shell@jacinto6evm:/ # [ 156.928188] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 161.932752] SELinux: initialized (dev tmpfs, type tmpfs), uses transition SIDs
[ 161.946628] init: Warning! Service uim needs a SELinux domain defined; please fix!
shell@jacinto6evm:/ #
shell@jacinto6evm:/ # [ 166.525605] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 170.312638] binder: 1567:1635 transaction failed 29189, size 68-0
[ 170.392365] init: Warning! Service vehicle_reset needs a SELinux domain defined; please fix!
[ 170.402329] init: Warning! Service zygote needs a SELinux domain defined; please fix!
[ 170.681730] init: Warning! Service netd needs a SELinux domain defined; please fix!
[ 170.690379] init: Warning! Service media needs a SELinux domain defined; please fix!
[ 170.746587] SELinux: initialized (dev tmpfs, type tmpfs), uses transition SIDs
[ 171.511230] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 176.551245] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 180.628987] binder: 1567:1635 transaction failed 29189, size 68-0
[ 180.722389] init: Warning! Service vehicle_reset needs a SELinux domain defined; please fix!
[ 180.733534] init: Warning! Service netd needs a SELinux domain defined; please fix!
[ 180.742072] init: Warning! Service zygote needs a SELinux domain defined; please fix!
[ 181.071416] init: Warning! Service media needs a SELinux domain defined; please fix!
[ 181.101550] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 186.131226] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 191.149566] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 196.167974] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 196.635232] SELinux: initialized (dev tmpfs, type tmpfs), uses transition SIDs
[ 201.211267] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 205.011000] binder: 1567:1636 transaction failed 29189, size 68-0
[ 205.062386] init: Warning! Service vehicle_reset needs a SELinux domain defined; please fix!
[ 205.075737] init: Warning! Service netd needs a SELinux domain defined; please fix!
[ 205.091686] init: Warning! Service media needs a SELinux domain defined; please fix!
[ 205.111708] init: Warning! Service zygote needs a SELinux domain defined; please fix!
[ 205.570291] SELinux: initialized (dev tmpfs, type tmpfs), uses transition SIDs
shell@jacinto6evm:/ #
shell@jacinto6evm:/ #
shell@jacinto6evm:/ #
shell@jacinto6evm:/ #
shell@jacinto6evm:/ #
shell@jacinto6evm:/ # [ 207.866273] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 212.911277] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 216.649428] binder: undelivered transaction 13361
[ 216.661629] binder: 1567:1635 transaction failed 29189, size 68-0
[ 216.722854] init: Warning! Service vehicle_reset needs a SELinux domain defined; please fix!
[ 216.734187] init: Warning! Service netd needs a SELinux domain defined; please fix!
[ 216.745910] init: Warning! Service zygote needs a SELinux domain defined; please fix!
[ 217.063082] init: Warning! Service media needs a SELinux domain defined; please fix!
[ 217.071644] init: Warning! Service uim needs a SELinux domain defined; please fix!
[ 222.111221] init: Warning! Service uim needs a SELinux domain defined; please fix!
shell@jacinto6evm:/ #
shell@jacinto6evm:/ #
shell@jacinto6evm:/ #
shell@jacinto6evm:/ # cat /proc/meminfo
MemTotal: 2052836 kB
MemFree: 1448424 kB
MemAvailable: 1665288 kB
Buffers: 1628 kB
Cached: 248892 kB
SwapCached: 0 kB
Active: 115488 kB
Inactive: 176628 kB
Active(anon): 41624 kB
Inactive(anon): 23780 kB
Active(file): 73864 kB
Inactive(file): 152848 kB
Unevictable: 0 kB
Mlocked: 0 kB
our hw board and sw is similar to http://omappedia.org/wiki/6AL.1.2_Release_Notes
uboot 2014-07
| OS Kernel: | Linux® 3.14.51 |
|---|---|
| Android: | Android Lollipop MR1 5.1.1 |
| Toolchain: | Andriod linux-x86 toolchain arm-eabi-4.8 |
| J6 Platform: | TI DRA7xxx EVM (J6 EVM) |
and we used 512Mbit * 16(bit) *4 =4GB ddr3.
we also referd to a lot of related threads like http://e2e.ti.com/support/arm/automotive_processors/f/1020/p/713799/2635617?tisearch=e2e-sitesearch&keymatch=4GB DDR#pi320098=1
and uboot can recognition 4G, whill kernel still 2G.
we need to check with you that if linux 3.14.51 when open ARM_LPAE,can support upto 4GB?
https://e2e.ti.com/support/arm/automotive_processors/f/1020/p/552861/2020130#2020130 mentioned that kernel need to >4.4 ,
is it right ? if linux 3.14.51 can support now ,could you help us to point the problem?