Part Number: PROCESSOR-SDK-AM335X
Hello
i want boot U-boot from SPI flash (nor w25q64) on Beaglebone Green Wireless (based on BBB).
we Compile U-boot with am335x_evm_defconfig (and move MLO and u-boot.img to SD-card Flash).
when using "sf probe 0" command to init SPI0 and flash MLO.byteswap into SPI flash (W25Q64FV) U-boot shows:
SF: unrecognized JEDEC id bytes: ff, ff, ff
Failed to initialize SPI flash at 0:0.
How we can Solve this Problem.(we checked spi connection and it is correct )
Thanks