Part Number: TDA2P-ABZ
Other Parts Discussed in Thread: TDA2
Tool/software: Linux
Hello TI team, we have a customer working on a high speed data transfer between a TDA2PEVM and PC using PCIe. A third party has has managed to develop a single lane implementation and this seems to be quite stable. Our customer tried to replicate the same demonstration using a very similar motherboard however for some reason the PC is not enumerating correctly with the TDA2P SOC and the PCIe root complex on the PC motherboard is not mapping the memory correctly. We need some support so that we can understand why they see a failure here, is this a software diver issue on the SOC or is this a hardware issue with the PCie . The ultimate goal is to support 2 x PCIe lanes via One Stop Systems passive PCIe extender cards although this has yet to be evaluated due to the enumeration issue that the customer is experiencing.
PC motherboard is running Ubuntu Linux
TDA2P SOC EVM running Linux
Steve