Tool/software: Linux
Hi All,
I am using TDA2PX EVM board and VSDK 3.05. All the camera and display applications are running in IPU1. The only requirement is USB support for updating the images.As per my knowledge USB is only supported in A15 which runs Linux.
Now after checking the rootfs ,it is about 630MB. Adding linux to give memory overheads also .Our NOR Flash is only 64Mb. What can be the minimum size of rootfs and how to optimize it only for USB.Can there be any other alternatives.
Currently our design only supports CAN as a network interface.
Regards,
Deepika