This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5708: Change clock frequency of CPU and DDR

Part Number: AM5708

Tool/software: Linux

Hello Experts,

We have one requirement to operate CPU and DDR at 600 Mhz and 400 Mhz respectively. Found TI's wiki http://processors.wiki.ti.com/index.php/Linux_Porting_Guide_for_AM571x/AM570x_Speed_Grades

In the above wiki for 500 Mhz structure is mentioned like 

static const struct dpll_params mpu_dpll_params_500mhz[NUM_SYS_CLKS] = {
        {-1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1},       /* 12 MHz   */
        {200, 7, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1},       /* 20 MHz   */
        {-1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1},       /* 16.8 MHz */
        {365, 13, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1},      /* 19.2 MHz */
        {-1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1},       /* 26 MHz   */
        {500, 26, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1},      /* 27 MHz   */
        {-1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1},       /* 38.4 MHz */
};

Could you please let me know what is logic for the above structure and how to create structure for 600 Mhz.

Thanks,
Gourav
  • Hi Roy,

    It depends on what is your main crystal frequency. On AM572x TI EVM we have 20MHz main clock source, thus for 1GHz we have:

    /* OPP NOM FREQUENCY for OMAP5 ES2.0, and DRA7 ES1.0 */

    static const struct dpll_params mpu_dpll_params_1ghz[NUM_SYS_CLKS] = {

    {250, 2, 1, 1, -1, -1, -1, -1, -1, -1, -1, -1}, /* 12 MHz   */

    {500, 9, 1, 1, -1, -1, -1, -1, -1, -1, -1, -1}, /* 20 MHz   */

    {119, 1, 1, 1, -1, -1, -1, -1, -1, -1, -1, -1}, /* 16.8 MHz */

    {625, 11, 1, 1, -1, -1, -1, -1, -1, -1, -1, -1}, /* 19.2 MHz */

    {500, 12, 1, 1, -1, -1, -1, -1, -1, -1, -1, -1}, /* 26 MHz   */

    {-1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1}, /* 27 MHz   */

    {625, 23, 1, 1, -1, -1, -1, -1, -1, -1, -1, -1}, /* 38.4 MHz */

    };

    This line means we have M=500, N=9, M2=1, the rest of the parameters (M3, M4, M4, M7, H21, H22, H23, H24) are not applicable, thus filled with -1.

    The formulas are:

    Fdpll  = Fref x 2 x M / (N+1) = 20 x 2 x 500 / (9 + 1) = 2000

    CLKOUT_M2 = Fdpll / (2 x M2) = 2000 / (2 x 1) = 1000 = 1GHz

     

    gourav roy said:
    static const struct dpll_params mpu_dpll_params_500mhz[NUM_SYS_CLKS] = { {-1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1}, /* 12 MHz */ {200, 7, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1}, /* 20 MHz */

     

    Here we have:

    Fdpll  = Fref x 2 x M / (N+1) = 20 x 2 x 200 / (7 + 1) = 1000

    CLKOUT_M2 = Fdpll / (2 x M2) = 1000 / (2 x 1) = 500MHz

     

    So for 600MHz with 20MHz crystal you can use the below line:

    {300, 9, 1, 1, -1, -1, -1, -1, -1, -1, -1, -1}, /* 20 MHz   */

    or

    {240, 7, 1, 1, -1, -1, -1, -1, -1, -1, -1, -1}, /* 20 MHz   */

     

    For more info check below TRM sections:

    3.6.3.3.2 DPLLs Output Clocks Parameters

    3.6.3.7 DPLL_MPU Description

     

    And below u-boot files:

    u-boot/arch/arm/mach-omap2/omap5/hw_data.c

    u-boot/arch/arm/mach-omap2/clocks-common.c

    u-boot/arch/arm/include/asm/omap_common.h

     

    Check also below e2e threads:

     

    DRA712: How to change CPU freq from 1Ghz to 600Mhz - Processors forum - Processors - TI E2E support ...

    e2e.ti.com
    Part Number: DRA712 Other Parts Discussed in Thread: DRA718 , Team, my customer needs to scaled down maximum CPU frequency from 1Ghz to 600Mhz. This is needed

     

    Linux/AM5726: Power reduction in U-boot - Processors forum - Processors - TI E2E support forums

    e2e.ti.com
    Part Number: AM5726 Tool/software: Linux Hello, I need to do power consumption at u-boot level as well as at kernel level. How can I do the lowest OPP in

     

    https://e2e.ti.com/support/legacy_forums/omap/f/885/t/338011

     

    Regards,
    Pavel

  • Thanks a lot Pavel.

    To change DDR clock frequency to 400 Mhz can i use same formula? and which structure do we need to change for ddr frequency?

    Thanks,
    Gourav
  • Gourav,

    Yes, the same formula. You can use M=200

    For AM5708 device, I think ddr_dpll_params_2664mhz should be changed.

    Regards,
    Pavel
  • Thanks Pavel,

    Could you please let me know, how to verify clock frequency of DDR once board boot up.

    We can verity cpu frequency on running board by 

    root@am57xx-evm:/sys/devices/system/cpu/cpu0/cpufreq# cat cpuinfo_cur_freq

    In similar manner is there any procedure to get DDR clock on board?

    Thanks,

    Gourav

  • Gourav,

    You can use omapconf tool.

    root@am57xx-evm:~# omapconf --help
    root@am57xx-evm:~# omapconf show dpll
    root@am57xx-evm:~# omapconf show opp

    On my side (AM572x EVM), for DPLL_DDR, it reports:

    Lock Frequency (MHz): 2128
    Clock Speed (MHz): 532

    For AM5708 device, you should use omapconf tool with "--force dra72x" option.

    Regards,
    Pavel
  • Thanks a lot for your support Pavel.