Part Number: AM5718
Tool/software: Linux
Hi
I am using Linux Processor SDK 05.01.00.11 version for developing application for AM5718 IDK EVM.
To get the source code of "kmscube" i got a directory 'tisdk'.
The kmscube source code is @
/tisdk/build/arago-tmp-external-linaro-toolchain/work/am57xx_evm-linux-gnueabi/kmscube/1.0.0-r7.tisdk0/git
Now I am modifying the same kmscube source code. Can I add "GLUT" library to it ? If yes then how can I achieve that ? (Which is the compatible version,how to access the library)
(Basically I need to draw circles and spheres and few more designs in it which is easy doing with glut.If there is any other way of doing this please let me know.)
Any help is appreciated.
Thanks and regards...
Arpita Jena