This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6678: NIMU package for Two ethernet ports

Part Number: TMS320C6678


Tool/software: Code Composer Studio

Hi,

We are using C6678 in our custom board in which we have Ethernet port SGMII1. With Default nimu package, it is working fine.

We have another board in which there will be two Ethernet ports. To support both the ports,

1. in CCS 5.2 Version, Modified NIMU package in C:\ti\pdk_C6678_1_1_2_5\packages\ti\transport\ndk\nimu\src\nimu_eth.c to support two ports(SGMII0 and SGMII1) and ports are initialized properly and we are able to ping to the SGMII1 port in the present board.

2. In CCS 7.4 version,

           a. Modified NIMU package in the same way, When we run on the board SGMII1 port is initialized successfully and SGMII0 port is failed at verify_init function.

And Ping is not working for the SGMII1 port also.

           b. When we call EmacInit only once, SGMII1 is working fine.

Please find the attached modified functions and let me know if I'm missing anything and Any other packages has to be modified.

NIMU_DEVICE_TABLE_ENTRY NIMUDeviceTable[] =
{
/**
* @brief EmacInit for the EVM
*/
EmacInit,
EmacInit,
NULL
};

/**
* @b EmacStart
* @n
* The function is used to initialize and start the EMAC
* controller and device.
*
* @param[in] ptr_net_device
* NETIF_DEVICE structure pointer.
*
* @retval
* Success - 0
* @retval
* Error - <0
*/
static int EmacStart(NETIF_DEVICE* ptr_net_device)
{
EMAC_DATA* ptr_pvt_data;
paMacAddr_t broadcast_mac_addr1 = { 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF};
paMacAddr_t broadcast_mac_addr = { 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFE};
paEthInfo_t ethInfo = { { 0x00, 0x00, 0x00, 0x00, 0x00, 0x00 }, /* Src mac = dont care */
{ 0x10, 0x11, 0x12, 0x13, 0x14, 0x15 }, /* Default Dest mac */
0, /* vlan = dont care */
0, /* ignore ether type */
0 /* MPLS tag = don't care */
};
paRouteInfo_t routeInfo = { pa_DEST_HOST, /* Route a match to the host */
0, /* Flow ID 0 */
0, /* Destination queue */
-1, /* Multi route disabled */
0xaaaaaaaa, /* SwInfo 0 */
0, /* SwInfo 1 is dont care */
0, /* customType = pa_CUSTOM_TYPE_NONE */ \
0, /* customIndex: not used */ \
0, /* pkyType: for SRIO only */ \
NULL /* No commands */
};
static int port = PORT_VAL;

/* Get the pointer to the private data */
ptr_pvt_data = (EMAC_DATA *)ptr_net_device->pvt_data;

/* Setup Tx */
if (Setup_Tx () != 0)
{
NIMU_drv_log ("Tx setup failed \n");
printf("1\n");
return -1;
}

/* Setup Rx */
if (Setup_Rx (ptr_net_device) != 0)
{
NIMU_drv_log ("Rx setup failed \n");
printf("2\n");
return -1;
}
memcpy (&ethInfo.dst[0], ptr_pvt_data->pdi.bMacAddr, sizeof(paMacAddr_t));

/* Set up the MAC Address LUT*/
if (Add_MACAddress (&ethInfo, &routeInfo, port) != 0)
{
NIMU_drv_log ("Add_MACAddress failed \n");
printf("3\n");
return -1;
}

if(port == 1)
{
memcpy (&ethInfo.dst[0], broadcast_mac_addr1, sizeof(paMacAddr_t));
}
else
{
memcpy (&ethInfo.dst[0], broadcast_mac_addr, sizeof(paMacAddr_t));
}

/* Set up the MAC Address LUT for Broadcast */
if (Add_MACAddress (&ethInfo, &routeInfo, port) != 0)
{
NIMU_drv_log ("Add_MACAddress failed \n");
printf("4\n");
return -1;
}
/* Verify the Tx and Rx Initializations */
if (Verify_Init () != 0)
{
NIMU_drv_log ("Warning:Queue handler Verification failed \n");
printf("Warning:Queue handler Verification failed \n");
}

/* Copy the MAC Address into the network interface object here. */
mmCopy(&ptr_net_device->mac_address[0], &ptr_pvt_data->pdi.bMacAddr[0], 6);

/* Set the 'initial' Receive Filter */
ptr_pvt_data->pdi.Filter = ETH_PKTFLT_MULTICAST;

ptr_pvt_data->pdi.TxFree = 1;

port--;
return 0;
}


/**
* @b EmacStop
* @n
* The function is used to de-initialize and stop the EMAC
* controller and device.
*
* @param[in] ptr_net_device
* NETIF_DEVICE structure pointer.
*
* @retval
* Success - 0
* @retval
* Error - <0
*/
static int EmacStop(NETIF_DEVICE* ptr_net_device)
{
printf("EmacStop\n");
EMAC_DATA* ptr_pvt_data;
uint16_t count, i;
Cppi_Desc* pCppiDesc;
uint8_t* bufaddr;
uint32_t bufLen;
static int port = PORT_VAL;

/* Disable event, interrupt */

/* Get the pointer to the private data */
ptr_pvt_data = (EMAC_DATA *)ptr_net_device->pvt_data;
Osal_nimuFree((Ptr)ptr_pvt_data, NIMU_roundUp(sizeof(EMAC_DATA), CACHE_LINESZ));

count = Qmss_getQueueEntryCount(gRxQHnd[port]);

/* Free the packet data buffer associated with the Rx Descriptor */
for (i=0; i < count; i++) {
/* Need to free up the PBM handle */
/* free the PBM packet */

/* Get a free descriptor from the global free queue we setup
* during initialization.
*/
if ((NIMU_qmssQPop (gRxQHnd[port], QHANDLER_QPOP_FDQ_ATTACHEDBUF, (Cppi_HostDesc **)&pCppiDesc)) == -1)
{
return -1;
}

/* Get the Address and Length for Free */
Cppi_getOriginalBufInfo(Cppi_DescType_HOST, pCppiDesc, &bufaddr, &bufLen);
Osal_nimuFree((Ptr)bufaddr, bufLen);
}

count = Qmss_getQueueEntryCount(gRxFreeQHnd[port]);
/* Free the packet data buffer associated with the Rx Descriptor */
for (i=0; i < count; i++) {
/* Need to free up the PBM handle */
/* free the PBM packet */

/* Get a free descriptor from the global free queue we setup
* during initialization.
*/
if ((NIMU_qmssQPop (gRxFreeQHnd[port], QHANDLER_QPOP_FDQ_ATTACHEDBUF, (Cppi_HostDesc **)&pCppiDesc)) == -1)
{
return -1;
}

/* Get the Address and Length for Free */
Cppi_getOriginalBufInfo(Cppi_DescType_HOST, pCppiDesc, &bufaddr, &bufLen);
Osal_nimuFree ((Ptr)bufaddr, bufLen);
}


/* tear down queues and dmas */
NIMU_stopQmss();
Qmss_queueClose (gPaCfgCmdRespQHnd[0]);
Qmss_queueClose (gTxFreeQHnd[port]);
Qmss_queueClose (gRxFreeQHnd[port]);
Qmss_queueClose (gRxQHnd[port]);
Qmss_queueClose (gTxReturnQHnd[port]);

for (i = 0; i < NSS_NUM_TX_QUEUES; i++)
Qmss_queueClose (gPaTxQHnd[i]);

NIMU_stopCppi(CPPI_CFG_PASS);
port--;

/* EMAC Controller has been stopped. */
return 0;
}

/**
* @b EmacSend0
* @n
* The function is the interface routine invoked by the NDK stack to
* pass packets to the driver.
*
* @param[in] ptr_net_device
* NETIF_DEVICE structure pointer.
* @param[in] hPkt
* Packet to be sent out on wire.
*
* @retval
* Success - 0
* @retval
* Error - <0
*/

#ifdef TIMING
#pragma DATA_SECTION(txisr_time, ".TimingSection");
uint32_t txisr_time[MAX_TIMING_PACKETS];
#pragma DATA_SECTION(txisr_time_idx, ".TimingSection");
uint32_t txisr_time_idx = 0;
#pragma DATA_SECTION(txisr_free_count, ".TimingSection");
uint32_t txisr_free_count[MAX_TIMING_PACKETS];
#endif

static int EmacSend0 (NETIF_DEVICE* ptr_net_device, PBM_Handle hPkt)
{
EMAC_DATA* ptr_pvt_data;
Cppi_Desc* pCppiDesc;
uint32_t dataBufferSize, i, count=0;
register uint8_t* buffer;
register uint32_t length;
Cppi_HostDesc* pHostDesc;
uint32_t coreNum;
Ptr key;
#ifdef TIMING
CSL_Uint64 st,et;
#endif
int port = 0;

#ifdef TIMING
st = 0;
et = 0;
#endif

#ifdef TIMING_TX
/* record start time */
if (txisr_time_idx < MAX_TIMING_PACKETS) {
st = CSL_tscRead();
}
#endif

/* Begin Critical Section before accessing shared resources. */
key = Osal_cppiCsEnter();

/* Get the core number. */
coreNum = CSL_chipReadDNUM();

count = Qmss_getQueueEntryCount (gTxReturnQHnd[port]);

/* Check if we got to free up any PBM handles? */
#ifdef TIMING_FREE
if (txisr_time_idx < MAX_TIMING_PACKETS) {
st = CSL_tscRead();
txisr_free_count[txisr_time_idx] = count;
}
#endif

for (i = 0; i < count; i++) {
PBM_Handle hPkt_to_free;

/* Need to free up the PBM handle */
/* free the PBM packet */

/* Get a free descriptor from the global free queue we setup
* during initialization.
*/
if ((NIMU_qmssQPop (gTxReturnQHnd[port], QHANDLER_QPOP_FDQ_ATTACHEDBUF, (Cppi_HostDesc **)&pCppiDesc)) == -1)
{
goto error_cond;
}
pHostDesc = (Cppi_HostDesc *)pCppiDesc;
/* Software info is intended to hold the PBM Pkt Handle for buffer management */
hPkt_to_free = (PBM_Handle ) pHostDesc->softwareInfo0;

/* Clear the PBM Handle set in the descriptor */
pHostDesc->softwareInfo0 = NULL;

/* Push descriptor to Tx free queue */
NIMU_qmssQPush (gTxFreeQHnd[port], (Ptr)pHostDesc, pHostDesc->buffLen, SIZE_HOST_DESC, Qmss_Location_TAIL);

PBM_free( (PBM_Handle) hPkt_to_free);

}

#ifdef TIMING_FREE
/* record end time */
if (txisr_time_idx < MAX_TIMING_PACKETS) {
et = CSL_tscRead();
txisr_time[txisr_time_idx++] = (uint32_t) (et - st);
}
#endif

/* Get the pointer to the private data */
ptr_pvt_data = (EMAC_DATA *)ptr_net_device->pvt_data;

/* Make sure the driver does not transmit packet less than min. as per the
* Ethernet standards. */
if( PBM_getValidLen(hPkt) < 60 )
PBM_setValidLen (hPkt, 60 );

/* We do not do any packet size checks here. If the packet
* is too big to fit in the MTU configured on the peripheral,
* then the driver/CSL layer should catch the error.
*/
if(1)
{
/* Peek into the packet to check out if any
* prioritization is needed.
*
* All raw Ethernet packets are tagged with the EMAC
* channel number onto which they need to be sent out
* in the PktPriority field.
*/
if (((PBM_Pkt *)hPkt)->PktPriority != PRIORITY_UNDEFINED)
{
/* PktPriority contains the EMAC channel number on which
* the packet needs to be txed.
*/
ptr_pvt_data->pdi.PhysIdx = (((PBM_Pkt *)hPkt)->PktPriority);
}
else
{
/* This is just a normal IP packet. Enqueue the packet in the
* Tx queue and send it for transmission.
* We are assuming here that the IP packets are transmitted
* on Channel 0 -> Core 0; Channel 1 --> Core 1; Channel 2 --> Core 2.
* and that the Raw packets can be transmitted on any channel.
*/
ptr_pvt_data->pdi.PhysIdx = 1;
}

/* Pass the packet to the controller if the transmitter is free. */
if(ptr_pvt_data->pdi.TxFree )
{
buffer = PBM_getDataBuffer(hPkt) + PBM_getDataOffset(hPkt);
length = PBM_getValidLen(hPkt);
/* Clean the cache for external/L2 addresses */
if( ((uint32_t)buffer & EMAC_EXTMEM ) ||
((uint32_t)buffer & EMAC_LL2SRAM ) ) {
OEMCacheClean( (void *)buffer, length );
}

/* Get a free descriptor from the global free queue we setup
* during initialization.
*/
if ((NIMU_qmssQPop (gTxFreeQHnd[port], QHANDLER_QPOP_FDQ_NO_ATTACHEDBUF, (Cppi_HostDesc **)&pCppiDesc)) == -1)
{
gTxDropCounter++;
goto error_cond;
}
pHostDesc = (Cppi_HostDesc *)pCppiDesc;

pHostDesc->softwareInfo0 = (uint32_t) hPkt;

dataBufferSize = length;
Cppi_setData ( Cppi_DescType_HOST,
(Cppi_Desc *) pCppiDesc,
(uint8_t *) NIMU_convertCoreLocal2GlobalAddr((uint32_t)buffer),
dataBufferSize
);
Cppi_setPacketLen (Cppi_DescType_HOST, (Cppi_Desc *)pCppiDesc, dataBufferSize);

count = Qmss_getQueueEntryCount (gTxReturnQHnd[port]);

#ifdef PA_LOOPBACK
NIMU_qmssQPush (gPaTxQHnd[0], pCppiDesc, dataBufferSize, SIZE_HOST_DESC, Qmss_Location_TAIL);
#else
Cppi_setPSFlags (Cppi_DescType_HOST, (Cppi_Desc *)pCppiDesc, (1<<gTxPort));
/* Send the packet out the mac. It will loop back to PA if the mac/switch
* have been configured properly
*/
NIMU_qmssQPush (gPaTxQHnd[8], pCppiDesc, dataBufferSize, SIZE_HOST_DESC, Qmss_Location_TAIL);
#endif

/* Increment the application transmit counter */
gTxCounter ++;
}

/* Packet has been successfully transmitted. */
/* End Critical Section */
Osal_cppiCsExit (key);

#ifdef TIMING_TX
/* record end time */
if (txisr_time_idx < MAX_TIMING_PACKETS) {
et = CSL_tscRead();
txisr_time[txisr_time_idx++] = (uint32_t) (et - st);
}
#endif
return 0;
}

error_cond:
{

/* End Critical Section */
Osal_cppiCsExit (key);

#ifdef TIMING_TX
/* record end time */
if (txisr_time_idx < MAX_TIMING_PACKETS) {
et = CSL_tscRead();
txisr_time[txisr_time_idx++] = (uint32_t) (et - st);
}

#endif
return -1;
}
}


/**
* @b EmacSend1
* @n
* The function is the interface routine invoked by the NDK stack to
* pass packets to the driver.
*
* @param[in] ptr_net_device
* NETIF_DEVICE structure pointer.
* @param[in] hPkt
* Packet to be sent out on wire.
*
* @retval
* Success - 0
* @retval
* Error - <0
*/

static int
EmacSend1 (NETIF_DEVICE* ptr_net_device, PBM_Handle hPkt)
{
EMAC_DATA* ptr_pvt_data;
Cppi_Desc* pCppiDesc;
uint32_t dataBufferSize, i, count=0;
register uint8_t* buffer;
register uint32_t length;
Cppi_HostDesc* pHostDesc;
uint32_t coreNum;
Ptr key;
#ifdef TIMING
CSL_Uint64 st,et;
#endif
int port = 1;

#ifdef TIMING
st = 0;
et = 0;
#endif

#ifdef TIMING_TX
/* record start time */
if (txisr_time_idx < MAX_TIMING_PACKETS) {
st = CSL_tscRead();
}
#endif

/* Begin Critical Section before accessing shared resources. */
key = Osal_cppiCsEnter();

/* Get the core number. */
coreNum = CSL_chipReadDNUM();

count = Qmss_getQueueEntryCount (gTxReturnQHnd[port]);

/* Check if we got to free up any PBM handles? */
#ifdef TIMING_FREE
if (txisr_time_idx < MAX_TIMING_PACKETS) {
st = CSL_tscRead();
txisr_free_count[txisr_time_idx] = count;
}
#endif

for (i = 0; i < count; i++) {
PBM_Handle hPkt_to_free;

/* Need to free up the PBM handle */
/* free the PBM packet */

/* Get a free descriptor from the global free queue we setup
* during initialization.
*/
if ((NIMU_qmssQPop (gTxReturnQHnd[port], QHANDLER_QPOP_FDQ_ATTACHEDBUF, (Cppi_HostDesc **)&pCppiDesc)) == -1)
{
goto error_cond;
}
pHostDesc = (Cppi_HostDesc *)pCppiDesc;
/* Software info is intended to hold the PBM Pkt Handle for buffer management */
hPkt_to_free = (PBM_Handle ) pHostDesc->softwareInfo0;

/* Clear the PBM Handle set in the descriptor */
pHostDesc->softwareInfo0 = NULL;

/* Push descriptor to Tx free queue */
NIMU_qmssQPush (gTxFreeQHnd[port], (Ptr)pHostDesc, pHostDesc->buffLen, SIZE_HOST_DESC, Qmss_Location_TAIL);

PBM_free( (PBM_Handle) hPkt_to_free);

}

#ifdef TIMING_FREE
/* record end time */
if (txisr_time_idx < MAX_TIMING_PACKETS) {
et = CSL_tscRead();
txisr_time[txisr_time_idx++] = (uint32_t) (et - st);
}
#endif

/* Get the pointer to the private data */
ptr_pvt_data = (EMAC_DATA *)ptr_net_device->pvt_data;

/* Make sure the driver does not transmit packet less than min. as per the
* Ethernet standards. */
if( PBM_getValidLen(hPkt) < 60 )
PBM_setValidLen (hPkt, 60 );

/* We do not do any packet size checks here. If the packet
* is too big to fit in the MTU configured on the peripheral,
* then the driver/CSL layer should catch the error.
*/
if(1)
{
/* Peek into the packet to check out if any
* prioritization is needed.
*
* All raw Ethernet packets are tagged with the EMAC
* channel number onto which they need to be sent out
* in the PktPriority field.
*/
if (((PBM_Pkt *)hPkt)->PktPriority != PRIORITY_UNDEFINED)
{
/* PktPriority contains the EMAC channel number on which
* the packet needs to be txed.
*/
ptr_pvt_data->pdi.PhysIdx = (((PBM_Pkt *)hPkt)->PktPriority);
}
else
{
/* This is just a normal IP packet. Enqueue the packet in the
* Tx queue and send it for transmission.
* We are assuming here that the IP packets are transmitted
* on Channel 0 -> Core 0; Channel 1 --> Core 1; Channel 2 --> Core 2.
* and that the Raw packets can be transmitted on any channel.
*/
ptr_pvt_data->pdi.PhysIdx = coreNum;
}

/* Pass the packet to the controller if the transmitter is free. */
if(ptr_pvt_data->pdi.TxFree )
{
buffer = PBM_getDataBuffer(hPkt) + PBM_getDataOffset(hPkt);
length = PBM_getValidLen(hPkt);
/* Clean the cache for external/L2 addresses */
if( ((uint32_t)buffer & EMAC_EXTMEM ) ||
((uint32_t)buffer & EMAC_LL2SRAM ) ) {
OEMCacheClean( (void *)buffer, length );
}

/* Get a free descriptor from the global free queue we setup
* during initialization.
*/
if ((NIMU_qmssQPop (gTxFreeQHnd[port], QHANDLER_QPOP_FDQ_NO_ATTACHEDBUF, (Cppi_HostDesc **)&pCppiDesc)) == -1)
{
gTxDropCounter++;
goto error_cond;
}
pHostDesc = (Cppi_HostDesc *)pCppiDesc;

pHostDesc->softwareInfo0 = (uint32_t) hPkt;

dataBufferSize = length;
Cppi_setData ( Cppi_DescType_HOST,
(Cppi_Desc *) pCppiDesc,
(uint8_t *) NIMU_convertCoreLocal2GlobalAddr((uint32_t)buffer),
dataBufferSize
);
Cppi_setPacketLen (Cppi_DescType_HOST, (Cppi_Desc *)pCppiDesc, dataBufferSize);

count = Qmss_getQueueEntryCount (gTxReturnQHnd[port]);

#ifdef PA_LOOPBACK
NIMU_qmssQPush (gPaTxQHnd[0], pCppiDesc, dataBufferSize, SIZE_HOST_DESC, Qmss_Location_TAIL);
#else
Cppi_setPSFlags (Cppi_DescType_HOST, (Cppi_Desc *)pCppiDesc, (1<<gTxPort));
/* Send the packet out the mac. It will loop back to PA if the mac/switch
* have been configured properly
*/
NIMU_qmssQPush (gPaTxQHnd[8], pCppiDesc, dataBufferSize, SIZE_HOST_DESC, Qmss_Location_TAIL);
#endif

/* Increment the application transmit counter */
gTxCounter ++;
}

/* Packet has been successfully transmitted. */
/* End Critical Section */
Osal_cppiCsExit (key);

#ifdef TIMING_TX
/* record end time */
if (txisr_time_idx < MAX_TIMING_PACKETS) {
et = CSL_tscRead();
txisr_time[txisr_time_idx++] = (uint32_t) (et - st);
}
#endif
return 0;
}

error_cond:
{

/* End Critical Section */
Osal_cppiCsExit (key);

#ifdef TIMING_TX
/* record end time */
if (txisr_time_idx < MAX_TIMING_PACKETS) {
et = CSL_tscRead();
txisr_time[txisr_time_idx++] = (uint32_t) (et - st);
}

#endif
return -1;
}
}

/**
* @b Description
* @n
* Call back function provided by application for EMAC driver
* to report a received packet descriptor.
*
* @retval
* None.
*/
static Bool gIsPingListUsed = 0;

#ifdef TIMING
#pragma DATA_SECTION(rxisr_time, ".TimingSection");
uint32_t rxisr_time[MAX_TIMING_PACKETS]; /* hold start time, end time, start time, end time, etc */
#pragma DATA_SECTION(rxisr_time_idx, ".TimingSection");
uint32_t rxisr_time_idx;
#pragma DATA_SECTION(rxisr_pktcount, ".TimingSection");
uint32_t rxisr_pktcount;
#endif

void EmacRxPktISR0(NETIF_DEVICE* ptr_net_device)
{
uint32_t protocol, pktLen;
uint32_t coreNum;
uint8_t* pBuffer;
Cppi_HostDesc* pHostDesc;
PBM_Handle hPkt;
Cppi_Desc* pCppiDesc;
uint32_t count, i;
uint32_t* ListAddress;
EMAC_DATA* ptr_pvt_data;
PBM_Pkt* rx_pbm_pkt;
void* accum_list_ptr;
#ifdef TIMING
CSL_Uint64 st, et;
#endif
int port = 0;

#ifdef TIMING
/* record start time */
if (rxisr_pktcount < MAX_TIMING_PACKETS) {
st = CSL_tscRead();
}
#endif

coreNum = CSL_chipReadReg (CSL_CHIP_DNUM);

/* Disable the interrupt */
coreKey [coreNum] = NIMU_osalHardwareIntDisable();
NIMU_osalHardwareIntrDisable(NIMU_ETH_INTERRUPT);
//coreKey [coreNum] = Osal_DisableInterrupt(NIMU_ETH1_INTERRUPT); //Hwi_disable();
/* Get the core number. */

/* Get the pointer to the private data */
ptr_pvt_data = (EMAC_DATA *)ptr_net_device->pvt_data;

if (!gIsPingListUsed){
accum_list_ptr = (void *)&gHiPriAccumList[0];
}
else {
accum_list_ptr = (void *)&gHiPriAccumList[MAX_HI_PRI_ACCUM_LIST_SIZE];
}


/* Invalidate cache if needed --
* if accumulator is in DDR then INV L2.
* if accumulator is in shared RAM (MSMC) invalidate L1
*/
if((uint32_t)(gHiPriAccumList) & EMAC_EXTMEM ){
CACHE_invL2(accum_list_ptr, sizeof(gHiPriAccumList)/2, CACHE_WAIT);
}

else if (((uint32_t)(gHiPriAccumList) & EMAC_MSMCSRAM) == EMAC_MSMCSRAM ) {
CACHE_invL1d(accum_list_ptr, sizeof(gHiPriAccumList)/2, CACHE_WAIT);
}

i = MAX_HI_PRI_ACCUM_LIST_SIZE - 1 - (RX_INT_THRESHOLD);
ListAddress = (uint32_t* )NIMU_convertCoreLocal2GlobalAddr((uint32_t) &gHiPriAccumList[i]);

/* Process ISR.
*
* Get the number of entries in accumulator list.
* The hardware enqueues data alternatively to Ping/Pong buffer lists in
* the accumulator. Hence, we need to track which list (Ping/Pong)
* we serviced the last time and accordingly process the other one
* this time around.
*/
if (!gIsPingListUsed)
{
/* Serviced Pong list last time. So read off the Ping list now */
count = ListAddress[0];
}
else
{
/* Serviced Pong list last time. So read off the Ping list now */
count = ListAddress[RX_INT_THRESHOLD + 1];
}

/* Nothing to receive, so return... */
if (count == 0) {
/* End Critical Section */


NIMU_osalHardwareIntrEnable(NIMU_ETH_INTERRUPT);
NIMU_osalHardwareIntRestore(coreKey[coreNum]);

//Osal_Restore(NIMU_ETH1_INTERRUPT, coreKey [coreNum]);
/* Clear INTD */
Qmss_ackInterrupt(PA_ACC_CHANNEL_NUM, 1);
Qmss_setEoiVector(Qmss_IntdInterruptType_HIGH, PA_ACC_CHANNEL_NUM);
return ; /* Not enough packets are received */
}

/* Process all the Results received
*
* Skip the first entry in the list that contains the
* entry count and proceed processing results.
*/
for (i = 1; i <= count; i ++)
{

gRxCounter ++;

/* Get the result descriptor.
*
* The hardware enqueues data alternatively to Ping/Pong buffer lists in
* the accumulator. Hence, we need to track which list (Ping/Pong)
* we serviced the last time and accordingly process the other one
* this time around.
*/
if (!gIsPingListUsed)
{
/* Serviced Pong list last time. So read off the Ping list now */
pCppiDesc = (Cppi_Desc *) ListAddress [i];
}
else
{
/* Serviced Ping list last time. So read off the Pong list now
*
* Skip over Ping list length to arrive at Pong list start.
*/
pCppiDesc = (Cppi_Desc *) ListAddress [i + RX_INT_THRESHOLD + 1];
}

/* Descriptor size appended to the address in the last 4 bits.
*
* To get the true descriptor size, always mask off the last
* 4 bits of the address.
*/
pCppiDesc = (Ptr) ((uint32_t) pCppiDesc & 0xFFFFFFF0);
pHostDesc = (Cppi_HostDesc *)pCppiDesc;

/* Invalidate cache based on where the memory is */
if((uint32_t)(pHostDesc) & EMAC_EXTMEM ){
CACHE_invL2((void *) pHostDesc, sizeof(Cppi_HostDesc), CACHE_WAIT);
}

else if (((uint32_t)(pHostDesc) & EMAC_MSMCSRAM) == EMAC_MSMCSRAM ) {
CACHE_invL1d((void *)pHostDesc, sizeof(Cppi_HostDesc), CACHE_WAIT);
}

if((uint32_t)(pHostDesc->buffPtr) & EMAC_EXTMEM ){
CSL_XMC_invalidatePrefetchBuffer();
CACHE_invL2((void *) pHostDesc->buffPtr, pHostDesc->buffLen, CACHE_WAIT);
}

else if (((uint32_t)(pHostDesc->buffPtr) & EMAC_MSMCSRAM) == EMAC_MSMCSRAM ) {
CSL_XMC_invalidatePrefetchBuffer();
CACHE_invL1d((void *)pHostDesc->buffPtr, pHostDesc->buffLen, CACHE_WAIT);
}

/*
* We should not see packets too large but check anyways ...
* Note that we are subtracting off the FCS the switch added to the frame.
* If its too large then return it to the free queue.
*/
if ((pHostDesc->buffLen-4) > (ptr_net_device->mtu + ETHHDR_SIZE)) {
/* lets try the next one... we should record this as a too large.... */
gRxDropCounter++;
pHostDesc->buffLen = pHostDesc->origBufferLen;
NIMU_qmssQPush (gRxFreeQHnd[port], (Ptr)pHostDesc, pHostDesc->buffLen, SIZE_HOST_DESC, Qmss_Location_TAIL);
continue;
}

/* Allocate the PBM packet for the Max MTU size*/
if (NULL == (hPkt = PBM_alloc(1514))) {
/* could not get a free NDK packet, maybe the next time around we can... */
gRxDropCounter++;
pHostDesc->buffLen = pHostDesc->origBufferLen;
NIMU_qmssQPush (gRxFreeQHnd[port], (Ptr)pHostDesc, pHostDesc->buffLen, SIZE_HOST_DESC, Qmss_Location_TAIL);
continue;
}

rx_pbm_pkt = (PBM_Pkt *) hPkt;

PBM_setDataOffset((PBM_Handle) hPkt, 0);

/* removing the FCS length the EMAC switch adds here */
pktLen = (pHostDesc->buffLen-4);

/* Set to minimum packet size */
if (pktLen < 60) {
pktLen = 64;
}

PBM_setValidLen((PBM_Handle) hPkt, pktLen);

/* Handle raw frames separately, i.e. check the
* Ethernet Protocol type in this packet and see
* if its a well known ether type. If so, this is normal
* IP stream, enqueue this is in usual Rx queue and let the
* stack know that a packet has arrived for it. However, if
* the Ethernet type in the packet is not a well known one,
* this could be a custom raw Ethernet packet, enqueue it
* separately in the Raw Rx queue and notify stack. The Raw
* Ethernet packets when being handed over are given
* preferential treatment and are serviced before the normal
* IP traffic. Hence the 2 queues.
*/
pBuffer = (uint8_t* )NIMU_convertCoreLocal2GlobalAddr((uint32_t) pHostDesc->buffPtr);

/* Extract the Ethernet type from the packet. */
protocol = ( pBuffer[12] << 8) | pBuffer[13] ;
protocol = (protocol & 0xFFFFu);

PBM_setIFRx((PBM_Handle) hPkt, (HANDLE) protocol );

/* Copy the data buffer received to the allocated PBM packet */
mmCopy((uint8_t* )rx_pbm_pkt->pDataBuffer, (uint8_t* )pBuffer, pktLen) ;

/* Is it a standard ethernet type? */
if (protocol != ETHERTYPE_IP && protocol != ETHERTYPE_IPv6 && protocol != ETHERTYPE_VLAN
&& protocol != ETHERTYPE_PPPOECTL && protocol != ETHERTYPE_PPPOEDATA )
{
/* This is a raw packet, enqueue in Raw Rx Queue */
PBMQ_enq( &ptr_pvt_data->pdi.PBMQ_rawrx, (PBM_Handle) hPkt);
}
else
{ /* This is a normal IP packet. Enqueue in Rx Queue */
PBMQ_enq( &ptr_pvt_data->pdi.PBMQ_rx, (PBM_Handle) hPkt );
}

/* Free the packet back to the Rx FDQ */
pHostDesc->buffLen = pHostDesc->origBufferLen;
NIMU_qmssQPush (gRxFreeQHnd[port], (Ptr)pHostDesc, pHostDesc->buffLen, SIZE_HOST_DESC, Qmss_Location_TAIL);
}

ListAddress = (uint32_t *) NIMU_convertCoreLocal2GlobalAddr((uint32_t) &gHiPriAccumList[0]);

/* Clear the accumulator list and save whether we used Ping/Pong
* list information for next time around.
*/
if (!gIsPingListUsed)
{
/* Just processed Ping list */
gIsPingListUsed = 1;

i = sizeof (gHiPriAccumList)/2;

/* Clear the accumulator list after processing */
memset ((void *) &gHiPriAccumList[0], 0, i);

if(
((uint32_t)(&gHiPriAccumList[0]) & EMAC_EXTMEM ) ||
(((uint32_t)(&gHiPriAccumList[0]) & EMAC_MSMCSRAM) == EMAC_MSMCSRAM )
)
{
/* This needs to be enabled if gHiPriAccumList is in External Memory or MSMCMEM */
CACHE_wbL2 ((void *)&gHiPriAccumList[0], i, CACHE_WAIT);
}
}
else
{
/* Just processed Pong list */
gIsPingListUsed = 0;
i = sizeof (gHiPriAccumList)/2;

/* Clear the accumulator list after processing */
memset ((void *) &gHiPriAccumList[MAX_HI_PRI_ACCUM_LIST_SIZE], 0, i);

if(
((uint32_t)(&gHiPriAccumList[MAX_HI_PRI_ACCUM_LIST_SIZE]) & EMAC_EXTMEM ) ||
(((uint32_t)(&gHiPriAccumList[MAX_HI_PRI_ACCUM_LIST_SIZE]) & EMAC_MSMCSRAM) == EMAC_MSMCSRAM )
)
{
/* This needs to be enabled if gHiPriAccumList is in External Memory or MSMCMEM */
CACHE_wbL2((void *) &gHiPriAccumList[MAX_HI_PRI_ACCUM_LIST_SIZE], i, CACHE_WAIT);
}
}

/* Notify NDK stack of pending Rx Ethernet packet */
STKEVENT_signal( ptr_pvt_data->pdi.hEvent, STKEVENT_ETHERNET, 1 );

/* End Critical Section */
NIMU_osalHardwareIntrEnable(NIMU_ETH_INTERRUPT);
NIMU_osalHardwareIntRestore(coreKey[coreNum]);
//Osal_Restore(NIMU_ETH1_INTERRUPT, coreKey [coreNum]);

#ifdef TIMING
/* record end time */
if (rxisr_pktcount < MAX_TIMING_PACKETS) {
et = CSL_tscRead();
rxisr_time[rxisr_time_idx++] = (uint32_t) (et-st);
rxisr_pktcount += count;
}
#endif

/* Clear INTD */
Qmss_ackInterrupt(PA_ACC_CHANNEL_NUM, 1);
Qmss_setEoiVector(Qmss_IntdInterruptType_HIGH, PA_ACC_CHANNEL_NUM);

return;
}



static Bool gIsPingListUsed1 = 0;

void EmacRxPktISR1(NETIF_DEVICE* ptr_net_device)
{
uint32_t protocol, pktLen;
uint32_t coreNum;
uint8_t* pBuffer;
Cppi_HostDesc* pHostDesc;
PBM_Handle hPkt;
Cppi_Desc* pCppiDesc;
uint32_t count, i;
uint32_t* ListAddress;
EMAC_DATA* ptr_pvt_data;
PBM_Pkt* rx_pbm_pkt;
void* accum_list_ptr;
#ifdef TIMING
CSL_Uint64 st, et;
#endif
int port = 1;

#ifdef TIMING
/* record start time */
if (rxisr_pktcount < MAX_TIMING_PACKETS) {
st = CSL_tscRead();
}
#endif

coreNum = CSL_chipReadReg (CSL_CHIP_DNUM);

/* Disable the interrupt */
coreKey [coreNum] = NIMU_osalHardwareIntDisable();
NIMU_osalHardwareIntrDisable(NIMU_ETH1_INTERRUPT);
//coreKey [coreNum] = Osal_DisableInterrupt(NIMU_ETH1_INTERRUPT); //Hwi_disable();
/* Get the core number. */

/* Get the pointer to the private data */
ptr_pvt_data = (EMAC_DATA *)ptr_net_device->pvt_data;

if (!gIsPingListUsed1){
accum_list_ptr = (void *)&gHiPriAccumList1[0];
}
else {
accum_list_ptr = (void *)&gHiPriAccumList1[MAX_HI_PRI_ACCUM_LIST_SIZE];
}


/* Invalidate cache if needed --
* if accumulator is in DDR then INV L2.
* if accumulator is in shared RAM (MSMC) invalidate L1
*/
if((uint32_t)(gHiPriAccumList1) & EMAC_EXTMEM ){
CACHE_invL2(accum_list_ptr, sizeof(gHiPriAccumList1)/2, CACHE_WAIT);
}

else if (((uint32_t)(gHiPriAccumList1) & EMAC_MSMCSRAM) == EMAC_MSMCSRAM ) {
CACHE_invL1d(accum_list_ptr, sizeof(gHiPriAccumList1)/2, CACHE_WAIT);
}

i = MAX_HI_PRI_ACCUM_LIST_SIZE - 1 - (RX_INT_THRESHOLD);
ListAddress = (uint32_t* )NIMU_convertCoreLocal2GlobalAddr((uint32_t) &gHiPriAccumList1[i]);

/* Process ISR.
*
* Get the number of entries in accumulator list.
* The hardware enqueues data alternatively to Ping/Pong buffer lists in
* the accumulator. Hence, we need to track which list (Ping/Pong)
* we serviced the last time and accordingly process the other one
* this time around.
*/
if (!gIsPingListUsed1)
{
/* Serviced Pong list last time. So read off the Ping list now */
count = ListAddress[0];
}
else
{
/* Serviced Pong list last time. So read off the Ping list now */
count = ListAddress[RX_INT_THRESHOLD + 1];
}

/* Nothing to receive, so return... */
if (count == 0) {
/* End Critical Section */


NIMU_osalHardwareIntrEnable(NIMU_ETH1_INTERRUPT);
NIMU_osalHardwareIntRestore(coreKey[coreNum]);

//Osal_Restore(NIMU_ETH1_INTERRUPT, coreKey [coreNum]);
/* Clear INTD */
Qmss_ackInterrupt(PA_ACC_CHANNEL_NUM_SEC_INTERFACE, 1);
Qmss_setEoiVector(Qmss_IntdInterruptType_HIGH, PA_ACC_CHANNEL_NUM_SEC_INTERFACE);
return ; /* Not enough packets are received */
}

/* Process all the Results received
*
* Skip the first entry in the list that contains the
* entry count and proceed processing results.
*/
for (i = 1; i <= count; i ++)
{

gRxCounter ++;

/* Get the result descriptor.
*
* The hardware enqueues data alternatively to Ping/Pong buffer lists in
* the accumulator. Hence, we need to track which list (Ping/Pong)
* we serviced the last time and accordingly process the other one
* this time around.
*/
if (!gIsPingListUsed1)
{
/* Serviced Pong list last time. So read off the Ping list now */
pCppiDesc = (Cppi_Desc *) ListAddress [i];
}
else
{
/* Serviced Ping list last time. So read off the Pong list now
*
* Skip over Ping list length to arrive at Pong list start.
*/
pCppiDesc = (Cppi_Desc *) ListAddress [i + RX_INT_THRESHOLD + 1];
}

/* Descriptor size appended to the address in the last 4 bits.
*
* To get the true descriptor size, always mask off the last
* 4 bits of the address.
*/
pCppiDesc = (Ptr) ((uint32_t) pCppiDesc & 0xFFFFFFF0);
pHostDesc = (Cppi_HostDesc *)pCppiDesc;

/* Invalidate cache based on where the memory is */
if((uint32_t)(pHostDesc) & EMAC_EXTMEM ){
CACHE_invL2((void *) pHostDesc, sizeof(Cppi_HostDesc), CACHE_WAIT);
}

else if (((uint32_t)(pHostDesc) & EMAC_MSMCSRAM) == EMAC_MSMCSRAM ) {
CACHE_invL1d((void *)pHostDesc, sizeof(Cppi_HostDesc), CACHE_WAIT);
}

if((uint32_t)(pHostDesc->buffPtr) & EMAC_EXTMEM ){
CSL_XMC_invalidatePrefetchBuffer();
CACHE_invL2((void *) pHostDesc->buffPtr, pHostDesc->buffLen, CACHE_WAIT);
}

else if (((uint32_t)(pHostDesc->buffPtr) & EMAC_MSMCSRAM) == EMAC_MSMCSRAM ) {
CSL_XMC_invalidatePrefetchBuffer();
CACHE_invL1d((void *)pHostDesc->buffPtr, pHostDesc->buffLen, CACHE_WAIT);
}

/*
* We should not see packets too large but check anyways ...
* Note that we are subtracting off the FCS the switch added to the frame.
* If its too large then return it to the free queue.
*/
if ((pHostDesc->buffLen-4) > (ptr_net_device->mtu + ETHHDR_SIZE)) {
/* lets try the next one... we should record this as a too large.... */
gRxDropCounter++;
pHostDesc->buffLen = pHostDesc->origBufferLen;
NIMU_qmssQPush (gRxFreeQHnd[port], (Ptr)pHostDesc, pHostDesc->buffLen, SIZE_HOST_DESC, Qmss_Location_TAIL);
continue;
}

/* Allocate the PBM packet for the Max MTU size*/
if (NULL == (hPkt = PBM_alloc(1514))) {
/* could not get a free NDK packet, maybe the next time around we can... */
gRxDropCounter++;
pHostDesc->buffLen = pHostDesc->origBufferLen;
NIMU_qmssQPush (gRxFreeQHnd[port], (Ptr)pHostDesc, pHostDesc->buffLen, SIZE_HOST_DESC, Qmss_Location_TAIL);
continue;
}

rx_pbm_pkt = (PBM_Pkt *) hPkt;

PBM_setDataOffset((PBM_Handle) hPkt, 0);

/* removing the FCS length the EMAC switch adds here */
pktLen = (pHostDesc->buffLen-4);

/* Set to minimum packet size */
if (pktLen < 60) {
pktLen = 64;
}

PBM_setValidLen((PBM_Handle) hPkt, pktLen);

/* Handle raw frames separately, i.e. check the
* Ethernet Protocol type in this packet and see
* if its a well known ether type. If so, this is normal
* IP stream, enqueue this is in usual Rx queue and let the
* stack know that a packet has arrived for it. However, if
* the Ethernet type in the packet is not a well known one,
* this could be a custom raw Ethernet packet, enqueue it
* separately in the Raw Rx queue and notify stack. The Raw
* Ethernet packets when being handed over are given
* preferential treatment and are serviced before the normal
* IP traffic. Hence the 2 queues.
*/
pBuffer = (uint8_t* )NIMU_convertCoreLocal2GlobalAddr((uint32_t) pHostDesc->buffPtr);

/* Extract the Ethernet type from the packet. */
protocol = ( pBuffer[12] << 8) | pBuffer[13] ;
protocol = (protocol & 0xFFFFu);

PBM_setIFRx((PBM_Handle) hPkt, (HANDLE) protocol );

/* Copy the data buffer received to the allocated PBM packet */
mmCopy((uint8_t* )rx_pbm_pkt->pDataBuffer, (uint8_t* )pBuffer, pktLen) ;

/* Is it a standard ethernet type? */
if (protocol != ETHERTYPE_IP && protocol != ETHERTYPE_IPv6 && protocol != ETHERTYPE_VLAN
&& protocol != ETHERTYPE_PPPOECTL && protocol != ETHERTYPE_PPPOEDATA )
{
/* This is a raw packet, enqueue in Raw Rx Queue */
PBMQ_enq( &ptr_pvt_data->pdi.PBMQ_rawrx, (PBM_Handle) hPkt);
}
else
{ /* This is a normal IP packet. Enqueue in Rx Queue */
PBMQ_enq( &ptr_pvt_data->pdi.PBMQ_rx, (PBM_Handle) hPkt );
}

/* Free the packet back to the Rx FDQ */
pHostDesc->buffLen = pHostDesc->origBufferLen;
NIMU_qmssQPush (gRxFreeQHnd[port], (Ptr)pHostDesc, pHostDesc->buffLen, SIZE_HOST_DESC, Qmss_Location_TAIL);
}

ListAddress = (uint32_t *) NIMU_convertCoreLocal2GlobalAddr((uint32_t) &gHiPriAccumList1[0]);

/* Clear the accumulator list and save whether we used Ping/Pong
* list information for next time around.
*/
if (!gIsPingListUsed1)
{
/* Just processed Ping list */
gIsPingListUsed1 = 1;

i = sizeof (gHiPriAccumList1)/2;

/* Clear the accumulator list after processing */
memset ((void *) &gHiPriAccumList1[0], 0, i);

if(
((uint32_t)(&gHiPriAccumList1[0]) & EMAC_EXTMEM ) ||
(((uint32_t)(&gHiPriAccumList1[0]) & EMAC_MSMCSRAM) == EMAC_MSMCSRAM )
)
{
/* This needs to be enabled if gHiPriAccumList1 is in External Memory or MSMCMEM */
CACHE_wbL2 ((void *)&gHiPriAccumList1[0], i, CACHE_WAIT);
}
}
else
{
/* Just processed Pong list */
gIsPingListUsed1 = 0;
i = sizeof (gHiPriAccumList1)/2;

/* Clear the accumulator list after processing */
memset ((void *) &gHiPriAccumList1[MAX_HI_PRI_ACCUM_LIST_SIZE], 0, i);

if(
((uint32_t)(&gHiPriAccumList1[MAX_HI_PRI_ACCUM_LIST_SIZE]) & EMAC_EXTMEM ) ||
(((uint32_t)(&gHiPriAccumList1[MAX_HI_PRI_ACCUM_LIST_SIZE]) & EMAC_MSMCSRAM) == EMAC_MSMCSRAM )
)
{
/* This needs to be enabled if gHiPriAccumList1 is in External Memory or MSMCMEM */
CACHE_wbL2((void *) &gHiPriAccumList1[MAX_HI_PRI_ACCUM_LIST_SIZE], i, CACHE_WAIT);
}
}

/* Notify NDK stack of pending Rx Ethernet packet */
STKEVENT_signal( ptr_pvt_data->pdi.hEvent, STKEVENT_ETHERNET, 1 );

/* End Critical Section */
NIMU_osalHardwareIntrEnable(NIMU_ETH1_INTERRUPT);
NIMU_osalHardwareIntRestore(coreKey[coreNum]);
//Osal_Restore(NIMU_ETH1_INTERRUPT, coreKey [coreNum]);

#ifdef TIMING
/* record end time */
if (rxisr_pktcount < MAX_TIMING_PACKETS) {
et = CSL_tscRead();
rxisr_time[rxisr_time_idx++] = (uint32_t) (et-st);
rxisr_pktcount += count;
}
#endif

/* Clear INTD */
Qmss_ackInterrupt(PA_ACC_CHANNEL_NUM_SEC_INTERFACE, 1);
Qmss_setEoiVector(Qmss_IntdInterruptType_HIGH, PA_ACC_CHANNEL_NUM_SEC_INTERFACE);

return;
}


/**
* @b EmacInit
* @n
* The function is used to initialize and register the EMAC
* with the Network Interface Management Unit (NIMU)
*
* @param[in] hEvent
* Stack Event Handle.
*
* @retval
* Success - 0
* @retval
* Error - <0
*/
static int EmacInit (STKEVENT_Handle hEvent)
{
EMACInit_Core(hEvent);

return 0;
}

static int EMACInit_Core (STKEVENT_Handle hEvent)
{
NETIF_DEVICE* ptr_device;
EMAC_DATA* ptr_pvt_data;
char names[6][5]={"eth0","eth1","eth2","eth3","eth4","eth5"};
uint32_t coreNum, i;
NIMU_EMAC_EXT_info emac_info;
static int port = PORT_VAL;

coreNum = CSL_chipReadDNUM();

/* Allocate memory for the private data */
ptr_pvt_data = Osal_nimuMalloc (NIMU_roundUp(sizeof(EMAC_DATA), CACHE_LINESZ), CACHE_LINESZ);

if (ptr_pvt_data == NULL)
{
NIMU_drv_log ("Error: Unable to allocate private memory data\n");
return -1;
}

/* Initialize the allocated memory block. */
mmZeroInit (ptr_pvt_data, sizeof(EMAC_DATA));

/* Initialize the RX Queue */
PBMQ_init(&ptr_pvt_data->pdi.PBMQ_rx);
PBMQ_init(&ptr_pvt_data->pdi.PBMQ_rawrx);

/* Initialize the private data */
mmZeroInit(&ptr_pvt_data->pdi, sizeof(PDINFO));

/* Set physical index */
ptr_pvt_data->pdi.PhysIdx = port;
ptr_pvt_data->pdi.hEvent = hEvent;

/* MCast List is EMPTY */
ptr_pvt_data->pdi.MCastCnt = 0;

#ifndef SIMULATOR_SUPPORT
for (i = 0; i < NIMU_MAX_EMAC_PORT_NUM; i++)
{
nimu_get_emac_info (i, &emac_info);
if (emac_info.mode == 1)
{
break;
}
}
if (i < NIMU_MAX_EMAC_PORT_NUM)
{
gTxPort = port; /* force packet out on switch port 1 */
if(gTxPort)
{
emac_info.mac_address[5]++;
}
memcpy(ptr_pvt_data->pdi.bMacAddr, emac_info.mac_address, 6);
}
else
{
NIMU_drv_log ("Error: Unable to find a TX EMAC port\n");
return -1;
}
#else
{
gTxPort = 1;
nimu_get_emac_info (1, &emac_info);
memcpy(ptr_pvt_data->pdi.bMacAddr, emac_info.mac_address, 6);
}
#endif


/* Init Logical Device */
/* ptr_pvt_data->pdi.hEther = hEther; */

/* Allocate memory for the EMAC. */
ptr_device = Osal_nimuMalloc (NIMU_roundUp(sizeof(NETIF_DEVICE), CACHE_LINESZ), CACHE_LINESZ);

if (ptr_device == NULL)
{
NIMU_drv_log ("Error: Unable to allocate memory for the EMAC\n");
return -1;
}

/* Initialize the allocated memory block. */
mmZeroInit (ptr_device, sizeof(NETIF_DEVICE));

/* Populate the Network Interface Object. */
strcpy (ptr_device->name, names[coreNum]);
ptr_device->mtu = ETH_MAX_PAYLOAD - ETHHDR_SIZE;
ptr_device->pvt_data = (void *)ptr_pvt_data;

/* Populate the Driver Interface Functions. */
ptr_device->start = EmacStart;
ptr_device->stop = EmacStop;
ptr_device->poll = EmacPoll;
if(port == 0)
{
ptr_device->send = EmacSend0;
}
else
{
ptr_device->send = EmacSend1;
}
ptr_device->pkt_service = EmacPktService;
ptr_device->ioctl = Emacioctl;
ptr_device->add_header = NIMUAddEthernetHeader;

if(port == 1)
{
/* Init PA LLD */
if (Init_PASS () != 0)
{
NIMU_drv_log ("PASS init failed \n");
return -1;
}
else
{
NIMU_drv_log ("PASS successfully initialized \n");
}

/* Initialize the CPSW switch */
if (Init_Cpsw ((uint32_t) ptr_device->mtu, ptr_pvt_data->pdi.bMacAddr) != 0)
{
NIMU_drv_log ("Ethernet subsystem init failed \n");
return -1;
}
else
{
NIMU_drv_log ("Ethernet subsystem successfully initialized \n");
}
}

/* Register the device with NIMU */
if (NIMURegister (ptr_device) < 0)
{
NIMU_drv_log ("Error: Unable to register the EMAC\n");
return -1;
}
port--;
NIMU_drv_log ("Registration of the EMAC Successful, waiting for link up ..\n");
printf ("Registration of the EMAC Successful, waiting for link up ..\n");
return 0;

}


/** ============================================================================
* @n@b Setup_Tx
*
* @b Description
* @n This API sets up all relevant data structures and configuration required
* for sending data to PASS/Ethernet. It sets up a Tx free descriptor queue,
* PASS Tx queues required for send.
*
* @param[in]
* @n None
*
* @return int32_t
* -1 - Error
* 0 - Success
* =============================================================================
*/
int32_t Setup_Tx (void)
{
uint8_t isAllocated, i;
Qmss_Queue qRetInfo;
Ptr pCppiDesc;
uint32_t mySWInfo[] = {0x00000000, 0x00000000, 0x00000000};
static int port = PORT_VAL;

/* Open all Transmit (Tx) queues.
*
* These queues are used to send data to PA PDSP/CPSW.
*/
if(port == 1)
{
for (i = 0; i < NSS_NUM_TX_QUEUES; i++)
{

if ((gPaTxQHnd[i] = Qmss_queueOpen (Qmss_QueueType_PASS_QUEUE, QMSS_PARAM_NOT_SPECIFIED, &isAllocated)) < 0)
{
NIMU_drv_log ("Error opening PA Tx queue \n");
return -1;
}
}
}

/* Open a Tx Free Descriptor Queue (Tx FDQ).
*
* This queue will be used to hold Tx free decriptors that can be filled
* later with data buffers for transmission onto wire.
*/
if ((gTxFreeQHnd[port] = Qmss_queueOpen (Qmss_QueueType_STARVATION_COUNTER_QUEUE, QMSS_PARAM_NOT_SPECIFIED, &isAllocated)) < 0)
{
NIMU_drv_log ("Error opening Tx Free descriptor queue \n");
return -1;
}

/* Open a Tx Return Descriptor Queue (Tx Transmit CompletionQ).
*
* This queue will be used to hold Tx completed decriptors that can be filled
* later with data buffers for transmission onto wire.
*/
if ((gTxReturnQHnd[port] = Qmss_queueOpen (Qmss_QueueType_GENERAL_PURPOSE_QUEUE, QMSS_PARAM_NOT_SPECIFIED, &isAllocated)) < 0)
{
NIMU_drv_log ("Error opening Tx Return descriptor queue \n");
return -1;
}

qRetInfo = Qmss_getQueueNumber (gTxReturnQHnd[port]);

/* Attach some free descriptors to the Tx free queue we just opened. */
for (i = 0; i < NIMU_NUM_TX_DESC; i++)
{
/* Get a free descriptor from the global free queue we setup
* during initialization.
*/
if ((NIMU_qmssQPop (NIMU_qmssGetFreeQ(), QHANDLER_QPOP_FDQ_NO_ATTACHEDBUF, (Cppi_HostDesc **)&pCppiDesc )) == -1)
{
break;
}

/* Setup the Completion queue:
*
* Setup the return policy for this desc to return to the completion q we just
* setup instead of the global free queue.
*/
Cppi_setReturnQueue ((Cppi_DescType) Cppi_DescType_HOST, pCppiDesc, qRetInfo);

/* Software info is inteded to hold the PBM Pkt Handle for buffer management */
mySWInfo[1] = i;
Cppi_setSoftwareInfo (Cppi_DescType_HOST, pCppiDesc, (uint8_t *) mySWInfo);

/* Push descriptor to Tx free queue */
NIMU_qmssQPushDescSize (gTxFreeQHnd[port], pCppiDesc, SIZE_HOST_DESC);
}
if (i != NIMU_NUM_TX_DESC)
{
NIMU_drv_log ("Error allocating Tx free descriptors \n");
return -1;
}

/* Open a Tx Command Free Descriptor Queue (Tx CMD FDQ).
*
* This queue will be used to hold Tx Command free decriptors
*/
if ((gTxCmdFreeQHnd[port] = Qmss_queueOpen (Qmss_QueueType_STARVATION_COUNTER_QUEUE, QMSS_PARAM_NOT_SPECIFIED, &isAllocated)) < 0)
{
NIMU_drv_log ("Error opening Tx Cmd Free descriptor queue \n");
return -1;
}

/* Open a Tx Cmd Return Descriptor Queue (Tx Cmd Completion Queue).
*
* This queue will be used to hold Tx command completed descriptors
*/
if ((gTxCmdReturnQHnd[port] = Qmss_queueOpen (Qmss_QueueType_GENERAL_PURPOSE_QUEUE, QMSS_PARAM_NOT_SPECIFIED, &isAllocated)) < 0)
{
NIMU_drv_log ("Error opening Tx Return descriptor queue \n");
return -1;
}
qRetInfo = Qmss_getQueueNumber (gTxCmdReturnQHnd[port]);

/* Attach some free descriptors to the Tx CMD free queue we just opened. */
for (i = 0; i < NIMU_MAX_NUM_TX_CMD_DESC; i++)
{
/* Get a free descriptor from the global free queue we setup
* during initialization.
*/
if ((NIMU_qmssQPop (NIMU_qmssGetFreeQ(), QHANDLER_QPOP_FDQ_NO_ATTACHEDBUF, (Cppi_HostDesc **)&pCppiDesc )) == -1)
{
break;
}

/* Setup the Completion queue:
*
* Setup the return policy for this desc to return to the completion q we just
* setup instead of the global free queue.
*/
Cppi_setReturnQueue ((Cppi_DescType) Cppi_DescType_HOST, pCppiDesc, qRetInfo);


/* Push descriptor to Tx free queue */
NIMU_qmssQPushDescSize (gTxCmdFreeQHnd[port], pCppiDesc, SIZE_HOST_DESC);
}
if (i != NIMU_MAX_NUM_TX_CMD_DESC)
{
NIMU_drv_log ("Error allocating Tx Command free descriptors \n");
return -1;
}
port--;
/* All done with Rx configuration. Return success. */
return 0;
}


int32_t setup_rx_queue(Qmss_Queue *rxQInfo, NETIF_DEVICE* ptr_net_device)
{
uint8_t isAllocated, accChannelNum;
uint16_t numAccEntries, intThreshold;
Qmss_AccCmdCfg accCfg;
int32_t vectId;
int16_t eventId;
uint32_t ListAddress;
uint32_t index;
static int port = PORT_VAL;

uint8_t coreNum = CSL_chipReadDNUM();

index = MAX_HI_PRI_ACCUM_LIST_SIZE - 1 - (RX_INT_THRESHOLD);

if(port == 0)
{
ListAddress = NIMU_convertCoreLocal2GlobalAddr((uint32_t) &gHiPriAccumList[index]);
}
else
{
ListAddress = NIMU_convertCoreLocal2GlobalAddr((uint32_t) &gHiPriAccumList1[index]);
}

/* Open a Receive (Rx) queue.
*
* This queue will be used to hold all the packets received by PASS/CPSW
*
* Open the next available High Priority Accumulation queue for Rx.
*/
if ((gRxQHnd[port] = Qmss_queueOpen (Qmss_QueueType_HIGH_PRIORITY_QUEUE, QMSS_PARAM_NOT_SPECIFIED, &isAllocated)) < 0)
{
NIMU_drv_log ("Error opening a High Priority Accumulation Rx queue \n");
return -1;
}

*rxQInfo = Qmss_getQueueNumber (gRxQHnd[port]);

/* Setup high priority accumulation interrupts on the Rx queue.
*
* Let's configure the accumulator with the following settings:
* (1) Interrupt pacing disabled.
* (2) Interrupt on every received packet
*/
intThreshold = RX_INT_THRESHOLD;
numAccEntries = (intThreshold + 1) * 2;

if(port == 0)
{
accChannelNum = PA_ACC_CHANNEL_NUM;
}
else
{
accChannelNum = PA_ACC_CHANNEL_NUM_SEC_INTERFACE;
}

/* Initialize the accumulator list memory */
memset ((void *) ListAddress, 0, numAccEntries * 4);

/* Setup the accumulator settings */
accCfg.channel = accChannelNum;
accCfg.command = Qmss_AccCmd_ENABLE_CHANNEL;
accCfg.queueEnMask = 0;
accCfg.listAddress = ListAddress;
accCfg.maxPageEntries = (intThreshold + 1); /* Add an extra entry for holding the entry count */
accCfg.timerLoadCount = 40;
accCfg.timerLoadCount = 0;
accCfg.interruptPacingMode = Qmss_AccPacingMode_LAST_INTERRUPT;
accCfg.listEntrySize = Qmss_AccEntrySize_REG_D;
accCfg.listCountMode = Qmss_AccCountMode_ENTRY_COUNT;
accCfg.multiQueueMode = Qmss_AccQueueMode_SINGLE_QUEUE;
accCfg.queMgrIndex = gRxQHnd[port];

/* Program the accumulator */
if (Qmss_programAccumulator (Qmss_PdspId_PDSP1, &accCfg) != QMSS_ACC_SOK)
{
printf("11\n");
return -1;
}

/* Register interrupts for the system event corresponding to the
* accumulator channel we are using.
*/
if(port == 0)
{
/* System event n - Accumulator Channel 0 */
eventId = NIMU_ETH_EVENTID;

/* Pick a interrupt vector id to use */
vectId = NIMU_ETH_INTERRUPT;
NIMU_osalRegisterInterruptDsp(eventId, (void*) &EmacRxPktISR0, (void*)ptr_net_device, TRUE, vectId);
}
else
{
/* System event n - Accumulator Channel 0 */
eventId = NIMU_ETH1_EVENTID;

/* Pick a interrupt vector id to use */
vectId = NIMU_ETH1_INTERRUPT;
NIMU_osalRegisterInterruptDsp(eventId, (void*) &EmacRxPktISR1, (void*)ptr_net_device, TRUE, vectId);
}
port--;
return 0;

}

/** ============================================================================
* @n@b Setup_Rx
*
* @b Description
* @n This API sets up all relevant data structures and configuration required
* for receiving data from PASS/Ethernet. It sets up a Rx free descriptor queue
* with some empty pre-allocated buffers to receive data, and an Rx queue
* to which the Rxed data is streamed for the example application. This API
* also sets up the QM high priority accumulation interrupts required to
* receive data from the Rx queue.
*
* @param[in]
* @n None
*
* @return int32_t
* -1 - Error
* 0 - Success
* =============================================================================
*/
int32_t Setup_Rx (NETIF_DEVICE* ptr_net_device)
{
uint16_t pktLen;
Qmss_Queue rxFreeQInfo, rxQInfo;
Ptr pCppiDesc;
Cppi_RxFlowCfg rxFlowCfg;
Ptr pDataBuffer;
uint32_t mySWInfo[] = {0x11112222, 0x33334444};
uint8_t isAllocated;
uint8_t i;
static int port = PORT_VAL;

if ((setup_rx_queue(&rxQInfo, ptr_net_device)) < 0)
{
NIMU_drv_log (" Error in setting up receive queue information\n");
return -1;
}
pktLen = ptr_net_device->mtu + ETHHDR_SIZE + 4; /* ETh Header + 4 bytes of FCS */

/* Open a Rx Free Descriptor Queue (Rx FDQ).
*
* This queue will hold all the Rx free descriptors. These descriptors will be
* used by the PASS CPDMA to hold data received via CPSW.
*/
if ((gRxFreeQHnd[port] = Qmss_queueOpen (Qmss_QueueType_STARVATION_COUNTER_QUEUE, QMSS_PARAM_NOT_SPECIFIED, &isAllocated)) < 0)
{
NIMU_drv_log ("Error opening Rx Free descriptor queue \n");
return -1;
}
rxFreeQInfo = Qmss_getQueueNumber (gRxFreeQHnd[port]);

/* Attach some free descriptors to the Rx free queue we just opened. */
for (i = 0; i < NIMU_NUM_RX_DESC; i++)
{
/* Get a free descriptor from the global free queue we setup
* during initialization.
*/
if ((NIMU_qmssQPop (NIMU_qmssGetFreeQ(), QHANDLER_QPOP_FDQ_NO_ATTACHEDBUF, (Cppi_HostDesc **)&pCppiDesc)) == -1)
{
break;
}

pktLen = NIMU_roundUp(pktLen, CACHE_LINESZ);
if ((pDataBuffer = Osal_nimuMalloc (pktLen, CACHE_LINESZ)) == NULL)
{
NIMU_drv_log ("Error allocating memory for Rx data buffer \n");
break;
}

/* Populate the Rx free descriptor with the buffer we just allocated. */
Cppi_setData (Cppi_DescType_HOST, pCppiDesc, (uint8_t *)NIMU_convertCoreLocal2GlobalAddr((uint32_t)pDataBuffer), pktLen);

/* Save original buffer information */
Cppi_setOriginalBufInfo (Cppi_DescType_HOST, pCppiDesc, (uint8_t *)NIMU_convertCoreLocal2GlobalAddr((uint32_t)pDataBuffer), pktLen);

/* Setup the Completion queue:
*
* Setup the return policy for this desc to return to the free q we just
* setup instead of the global free queue.
*/
Cppi_setReturnQueue (Cppi_DescType_HOST, pCppiDesc, rxFreeQInfo);

Cppi_setSoftwareInfo (Cppi_DescType_HOST, pCppiDesc, (uint8_t *) mySWInfo);

Cppi_setPacketLen (Cppi_DescType_HOST, pCppiDesc, pktLen);

/* Push descriptor to Rx free queue */
NIMU_qmssQPushDescSize (gRxFreeQHnd[port], pCppiDesc, SIZE_HOST_DESC);
//Qmss_queuePushDescSize(gRxFreeQHnd, pCppiDesc, SIZE_HOST_DESC);
}
if (i != NIMU_NUM_RX_DESC)
{
NIMU_drv_log ("Error allocating Rx free descriptors \n");
return -1;
}

/* Setup a Rx Flow.
*
* A Rx flow encapsulates all relevant data properties that CPDMA would
* have to know in order to successfully receive data.
*/
/* Initialize the flow configuration */
memset (&rxFlowCfg, 0, sizeof(Cppi_RxFlowCfg));
rxFreeQInfo = Qmss_getQueueNumber (gRxFreeQHnd[port]);

/* Let CPPI pick the next available flow */
rxFlowCfg.flowIdNum = CPPI_PARAM_NOT_SPECIFIED;

rxFlowCfg.rx_dest_qmgr = rxQInfo.qMgr;
rxFlowCfg.rx_dest_qnum = rxQInfo.qNum;

rxFlowCfg.rx_desc_type = Cppi_DescType_HOST;

rxFlowCfg.rx_ps_location = Cppi_PSLoc_PS_IN_DESC;
rxFlowCfg.rx_psinfo_present = 1; /* Enable PS info */

rxFlowCfg.rx_error_handling = 0; /* Drop the packet, do not retry on starvation by default */
rxFlowCfg.rx_einfo_present = 1; /* EPIB info present */

rxFlowCfg.rx_dest_tag_lo_sel = 0; /* Disable tagging */
rxFlowCfg.rx_dest_tag_hi_sel = 0;
rxFlowCfg.rx_src_tag_lo_sel = 0;
rxFlowCfg.rx_src_tag_hi_sel = 0;

rxFlowCfg.rx_size_thresh0_en = 0; /* By default, we disable Rx Thresholds */
rxFlowCfg.rx_size_thresh1_en = 0; /* By default, we disable Rx Thresholds */
rxFlowCfg.rx_size_thresh2_en = 0; /* By default, we disable Rx Thresholds */
rxFlowCfg.rx_size_thresh0 = 0x0;
rxFlowCfg.rx_size_thresh1 = 0x0;
rxFlowCfg.rx_size_thresh2 = 0x0;

rxFlowCfg.rx_fdq0_sz0_qmgr = rxFreeQInfo.qMgr; /* Setup the Receive free queue for the flow */
rxFlowCfg.rx_fdq0_sz0_qnum = rxFreeQInfo.qNum;
rxFlowCfg.rx_fdq0_sz1_qnum = 0x0;
rxFlowCfg.rx_fdq0_sz1_qmgr = 0x0;
rxFlowCfg.rx_fdq0_sz2_qnum = 0x0;
rxFlowCfg.rx_fdq0_sz2_qmgr = 0x0;
rxFlowCfg.rx_fdq0_sz3_qnum = 0x0;
rxFlowCfg.rx_fdq0_sz3_qmgr = 0x0;

rxFlowCfg.rx_fdq1_qnum = rxFreeQInfo.qNum; /* Use the Rx Queue to pick descriptors */
rxFlowCfg.rx_fdq1_qmgr = rxFreeQInfo.qMgr;
rxFlowCfg.rx_fdq2_qnum = rxFreeQInfo.qNum; /* Use the Rx Queue to pick descriptors */
rxFlowCfg.rx_fdq2_qmgr = rxFreeQInfo.qMgr;
rxFlowCfg.rx_fdq3_qnum = rxFreeQInfo.qNum; /* Use the Rx Queue to pick descriptors */
rxFlowCfg.rx_fdq3_qmgr = rxFreeQInfo.qMgr;

/* Configure the Rx flow */
if ((gRxFlowHnd[port] = Cppi_configureRxFlow (NIMU_cppiGetPASSHandle(), &rxFlowCfg, &isAllocated)) == NULL)
{
NIMU_drv_log ("Error configuring Rx flow \n");
return -1;
}
port--;
/* All done with Rx configuration. Return success. */
return 0;
}

/** ============================================================================

* @n@b Verify_Init
*
* @b Description
* @n This API initializes the CPPI LLD, opens the PASS CPDMA and opens up
* the Tx, Rx channels required for data transfers.
*
* @param[in]
* @n None
*
* @return int32_t
* -1 - Error
* 0 - Success
* =============================================================================
*/
int32_t Verify_Init (void)
{
int32_t count, returnVal = 0, i;
int32_t num_tx_desc = NIMU_NUM_TX_DESC;
int32_t num_rx_desc = NIMU_NUM_RX_DESC;
int32_t max_queue_number = QMSS_MAX_LOW_PRIORITY_QUEUE +
QMSS_MAX_PASS_QUEUE +
QMSS_MAX_LOW_PRIORITY_QUEUE +
QMSS_MAX_PASS_QUEUE +
QMSS_MAX_INTC_QUEUE +
QMSS_MAX_SRIO_QUEUE +
QMSS_MAX_HIGH_PRIORITY_QUEUE +
QMSS_MAX_STARVATION_COUNTER_QUEUE +
QMSS_MAX_INFRASTRUCTURE_QUEUE +
QMSS_MAX_TRAFFIC_SHAPING_QUEUE +
QMSS_MAX_GENERAL_PURPOSE_QUEUE ;
static int port = PORT_VAL;

/*Verify if we got NIMU_NUM_TX_DESC Tx Free Q*/
if ((count = Qmss_getQueueEntryCount (gTxFreeQHnd[port])) != num_tx_desc) {
NIMU_drv_log3 ("Verify_Init: Expected %d entry count for gTxFreeQHnd queue %d, found %d entries\n", num_tx_desc, gTxFreeQHnd[port], count);
printf ("Verify_Init: Expected %d entry count for gTxFreeQHnd queue %d, found %d entries\n", num_tx_desc, gTxFreeQHnd[port], count);
returnVal = -1;
}

/* Verify if we got NIMU_NUM_RX_DESC Rx FDQ */
if ((count = Qmss_getQueueEntryCount (gRxFreeQHnd[port])) != num_rx_desc) {
NIMU_drv_log3 ("Verify_Init: Expected %d entry count for gRxFreeQHnd queue %d, found %d entries\n", num_rx_desc, gRxFreeQHnd[port], count);
printf ("Verify_Init: Expected %d entry count for gRxFreeQHnd queue %d, found %d entries\n", num_rx_desc, gRxFreeQHnd[port], count);
returnVal = -1;
}

/* Verify if we got empty Tx completion Q*/
if ((count = Qmss_getQueueEntryCount (gTxReturnQHnd[port])) != 0) {
NIMU_drv_log2 ("Verify_Init: Expected 0 entry count for gTxReturnQHnd queue %d, found %d entries\n", gTxReturnQHnd[port], count);
printf ("Verify_Init: Expected 0 entry count for gTxReturnQHnd queue %d, found %d entries\n", gTxReturnQHnd[port], count);
returnVal = -1;
}

/* Verify if we got NIMU_NUM_RX_DESC Rx FDQ */
if ((count = Qmss_getQueueEntryCount (gRxQHnd[port])) != 0) {
NIMU_drv_log2 ("Verify_Init: Expected 0 entry count for gRxQHnd= %d, found %d entries\n", gRxQHnd[port], count);
printf ("Verify_Init: Expected 0 entry count for gRxQHnd= %d, found %d entries\n", gRxQHnd[port], count);
returnVal = -1;
}

for (i = 0; i < max_queue_number; i++ ) {
if ( (i == gRxFreeQHnd[port]) || (i == gTxFreeQHnd[port]) || (i == gTxCmdFreeQHnd[port]))
continue;

count = Qmss_getQueueEntryCount (i);
if (count != 0) {
NIMU_drv_log2 ("Verify_Init: Expected 0 entry count for Queue number = %d, found %d entries\n", i, count);
}
}
port--;

/* Verify_Init Done. Return success */
return (returnVal);
}

/** ============================================================================
* @n@b Add_MACAddress
*
* @b Description
* @n This API adds the switch MAC address to the PA PDSP Lookup table. This
* ensures that all packets destined for this MAC address get processed
* for forwarding to the host.
*
* @param[in]
* @n ethInfo Pointer to PA Ethernet Info table.
*
* @param[in]
* @n routeInfo Pointer to PA Route Info table.
*
* @n None
*
* @return int32_t
* -1 - Error
* 0 - Success
* =============================================================================
*/
int32_t Add_MACAddress( paEthInfo_t *ethInfo,
paRouteInfo_t *routeInfo,
int32_t port)
{
int32_t j;
uint16_t cmdSize;
Qmss_Queue cmdReplyQInfo;

paRouteInfo_t nFailInfo = { pa_DEST_DISCARD, /* Toss the packet */
0, /* Flow Id = dont care */
0, /* queue = dont care */
0, /* mutli route = dont care */
0, /* swinfo0 = dont care */
0, /* swinfo1 = dont care */
0, /* customType = pa_CUSTOM_TYPE_NONE */ \
0, /* customIndex: not used */ \
0, /* pkyType: for SRIO only */ \
NULL /* No commands */
};
paCmdReply_t cmdReplyInfo = { pa_DEST_HOST, /* Replies go to the host */
0, /* User chosen ID to go to swinfo0 */
0, /* Destination queue */
0 /* Flow ID */
};
paReturn_t retVal;
paEntryHandle_t retHandle;
int32_t handleType, cmdDest;
uint32_t psCmd = ((uint32_t)(4 << 5) << 24);
uint32_t myswinfo[] = {0x11112222, 0x33334444};
uint32_t myswinfo_orig[] = {0x00000000, 0x00000000, 0x00000000};;
uint8_t* pCmdDataBuffer;
Cppi_HostDesc* pHostDesc = NULL;
Qmss_Queue rxQInfo;
uint32_t count, cmdbuf_len = 320;
int32_t ret_val = 0;

printf("Add_MACAddress port %d\n",port);

/* Get a Tx free descriptor to send a command to the PA PDSP */
if ((NIMU_qmssQPop (gTxCmdFreeQHnd[port], QHANDLER_QPOP_FDQ_NO_ATTACHEDBUF, (Cppi_HostDesc **)&pHostDesc )) == -1)
{
NIMU_drv_log ("Error obtaining a Tx free descriptor \n");
return -1;
}

/* Allocate a Tx buffer and attach the command info to it. */
cmdbuf_len = NIMU_roundUp(cmdbuf_len, CACHE_LINESZ);
if ((pCmdDataBuffer = (Ptr) Osal_nimuMalloc (cmdbuf_len, CACHE_LINESZ)) == NULL)
{
NIMU_drv_log ("Error allocating memory for PA Command data buffer \n");
return -1;
}

/* Populate the Tx free descriptor with the buffer we just allocated. */
Cppi_setData (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, (uint8_t *)NIMU_convertCoreLocal2GlobalAddr((uint32_t)pCmdDataBuffer), cmdbuf_len);

/* Save original buffer information */
Cppi_setOriginalBufInfo (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, (uint8_t *)NIMU_convertCoreLocal2GlobalAddr((uint32_t)pCmdDataBuffer), cmdbuf_len);

cmdSize = pHostDesc->buffLen;
cmdReplyInfo.replyId = 0x11111111; /* unique for each add mac command */

/* Get the PA response queue number and populate the destination queue number
* in the PA response configuration.
*/
cmdReplyQInfo = Qmss_getQueueNumber (gPaCfgCmdRespQHnd[0]);
cmdReplyInfo.queue = cmdReplyQInfo.qNum;

/* Setup the Rx queue as destination for the packets */
rxQInfo = Qmss_getQueueNumber (gRxQHnd[port]);
routeInfo->queue = rxQInfo.qNum;

retVal = Pa_addMac (NIMU_getPAInstance(),
pa_LUT1_INDEX_NOT_SPECIFIED,
ethInfo,
routeInfo,
&nFailInfo,
&gPaL2Handles[0],
(paCmd_t) pHostDesc->buffPtr,
&cmdSize,
&cmdReplyInfo,
&cmdDest);
if (retVal != pa_OK)
{
NIMU_drv_log1 ("Pa_addMac returned error %d\n", retVal);
ret_val = -1;
goto return_fail;
}


/* This sets the extended info for descriptors, and this is required so PS info
* goes to the right spot
*/
Cppi_setSoftwareInfo (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, (uint8_t *)myswinfo);

/* Set the buffer length to the size used. It will be restored when the descriptor
* is returned
*/
Cppi_setPacketLen (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, cmdSize);
pHostDesc->buffLen = cmdSize;

/* Mark the packet as a configuration packet */
Cppi_setPSData (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, (uint8_t *)&psCmd, 4);

/* Send the command to the PA and wait for the return */
NIMU_qmssQPush (gPaTxQHnd[cmdDest - pa_CMD_TX_DEST_0],
pHostDesc,
pHostDesc->buffLen,
SIZE_HOST_DESC,
Qmss_Location_TAIL
);

/* Poll on the PA response queue to see if response from PA has come */
for (j = 0; j < 100; j++)
{
CycleDelay (1000);

/* Verify if we got empty Tx completion Q*/
count = Qmss_getQueueEntryCount (gTxCmdReturnQHnd[port]);

if (count != 0) {

if ((NIMU_qmssQPop (gTxCmdReturnQHnd[port], QHANDLER_QPOP_FDQ_ATTACHEDBUF, (Cppi_HostDesc **)&pHostDesc)) == -1)
{
ret_val = -1;
goto return_fail;
}

/* Restore the states */
Cppi_setSoftwareInfo(Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, (uint8_t *)myswinfo_orig);
Cppi_setPSData (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, NULL, NULL);
Cppi_setData (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, NULL, NULL);
Cppi_setOriginalBufInfo (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, NULL, NULL);
Cppi_setPacketLen (Cppi_DescType_HOST, (Cppi_Desc *)pHostDesc, NULL);
pHostDesc->buffLen = 0;

NIMU_qmssQPushDescSize (gTxCmdFreeQHnd[port], pHostDesc, SIZE_HOST_DESC);
}

if (Qmss_getQueueEntryCount (gPaCfgCmdRespQHnd[0]) > 0)
{

/* We have a response from PA PDSP for the command we submitted earlier for
* MAC address addition.
*/
if ((NIMU_qmssQPop (gPaCfgCmdRespQHnd[0], QHANDLER_QPOP_FDQ_NO_ATTACHEDBUF, (Cppi_HostDesc **)&pHostDesc)) == -1)
{
ret_val = -1;
goto return_fail;
}

if (pHostDesc->softwareInfo0 != cmdReplyInfo.replyId)
{
pHostDesc->buffLen = pHostDesc->origBufferLen;
NIMU_qmssQPush (gTxCmdFreeQHnd[port], pHostDesc, pHostDesc->buffLen, SIZE_HOST_DESC, Qmss_Location_TAIL);
ret_val = -1;
goto return_fail;

}

retVal = Pa_forwardResult (NIMU_getPAInstance(), (Ptr)pHostDesc->buffPtr, &retHandle, &handleType, &cmdDest);
if (retVal != pa_OK)
{
NIMU_drv_log ("PA sub-system rejected Pa_addMac command\n");
ret_val = -1;
goto return_fail;
}

/* Reset the buffer length and put the descriptor back on the Rx free queue */
pHostDesc->buffLen = pHostDesc->origBufferLen;
NIMU_qmssQPush (gRxFreeQHnd[port], pHostDesc, pHostDesc->buffLen, SIZE_HOST_DESC, Qmss_Location_TAIL);
break;
}
}

if (j == 100)
{
NIMU_drv_log ("Timeout waiting for reply from PA to Pa_addMac command\n");
ret_val = -1;
}

return_fail:

Osal_nimuFree (pCmdDataBuffer, cmdbuf_len);

return (ret_val);
}

Thank you,

Mounika