Part Number: TDA2
Tool/software: Linux
Hi Expert,
I'm running Linux Vision SDK v03.02.00(4.4.84) on TDA2Ex.
reference usecase: "chains_lvdsVipMultiCam_Sgx3Dsrv"
Modify as below:
The usual operation display is smooth.
However, increasing the amount of DSP operations will a serious delay in the display.
How can I continue to display images without being affected by DSP delay?
Only get the left image, Capture → Sync → Dup → ipc → Sgx3Dsrv. But it has not improved delay.
sgx3DsrvLink_drv.c, Int32 Sgx3DsrvLink_drvDoProcessFrames(Sgx3DsrvLink_Obj *pObj)
In addition, add Vps_printf in the capture, dup, sync link to observe each link's system_sendLinkCmd (, SYSTEM_CMD_NEW_DATA,
The sending interval will become longer when the DSP to increase the load. Why?
Could you please give some suggestion here?
Thanks in advance.