Tool/software: TI-RTOS
Hi Brijesh,
Thanks for the previous answer . For time being we have adjusted the Display buffer start area to the start of valid frame to resolve the first few blanking periods.I have two more questions as well.Please a
1. Also we have 1 or 2 pixel offset for every vertical lines.What could be the reason for the same?
Have another question on the image quality of frame .
2. Is there any options by which the received frame quality can be improved by adjusting any VIP setting .Currently our VIP setting is , incoming embedded sync in Y(4:2:0) is converted to RGB before putting into display buffer. Does it need VPE as well. Or it is purely dependent on the external Video Decoder.
With regards,
Jeyaseelan