Other Parts Discussed in Thread: THS7353
I recently purchased the TMDXEVM365 board and am suffering trouble out of the box.
I've followed the procedure listed in the TMX320DM365 Digital Video Evaluation Module BETA Setup Guide (2 page booklet).
The DIP switches SW4 / 5 are in their required positions and I have fed the unit various video inputs but no audio. I've provided:
[Input] 2 Sony handycams via composite and Svideo
[Input] 1 video pattern generator providing composite, NTSC/PAL and Svideo (adjusting SW5 for NTSC/PAL)
In all cases, I get no output from the module to my video sink. The RS232 dump states the following at the end of initializaiton:
audio_loopback: underrun occurred
ths7353_setvalue -start
ths7353_setvalue -end
ths7353_setvalue -start
setting data format
Detecting if driver supports COMPONENT
input.name = RAW
input.name = RAW-1
input.name = COMPOSITE
input.name = SVIDEO
input.name = COMPONENT
ths7353_setvalue -end
querystd, erorxxx, val = 1, val1 = 1
error: InitDevice:ioctl:VIDIOC_G_INPUT
Error in setting capture format
Failed to intialize capture
main : Leave
It appears the module is unable to lock/detect any video I am giving it. I have attached the complete bootup log form rs232.
I believe I have followed the instructions to the letter but no dice.