This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3359: ADC maximum clock frequency

Part Number: AM3359


The ADC maximum clock frequency shown in Table 5-16 on AM335x datasheet (SPRS717K) is 3 MHz. On the other hand, it shown in Table 12-2 on TRM (SPRUH73P) is 24 MHz.

Should the ADC clock frequency be used at up to 3 MHz?

Best regards,

Daisuke