This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/DRA75: How to Validate Late Attach Feature in Linux Kernel

Part Number: DRA75

Tool/software: Linux

Hi All,

We are using J6 and Vision SDK 3.04

IPU1 firmware is getting loaded by bootloader and it is verified.

We have integrated Following Early boot and Late attach patches to the Kernel

ti_components/os_tools/linux/kernel/linux-kernel-addon$ ls -l earlyboot-kernel-patches/


0001-dra7xx-Kernel-Optimizations-for-early-use-case-enabl.patch
0002-arm-mach-omap2-Remove-edma-related-nodes-from-hwmod-.patch
0003-arm-dts-infoadas-Late-attach-remoteprocs.patch
0004-config_fragments-Make-remoteproc-built-in-enable-use.patch
0005-arm-dts-Disable-DSS-PRCM-for-M4-display.patch

and verifying the late attach functionality at kernel side. dmesg reports that ipu1 will be late-attached

dmesg | grep lat-attach

map-rproc 58820000.ipu: device will be late-attached

We would like to know how we can confirm that late attach functionality is working fine. We are following this page: http://processors.wiki.ti.com/index.php/Early_Boot_and_Late_Attach_in_Linux and this suggest to look in to trace0

root@dra7xx-evm:~# cat /sys/kernel/debug/remoteproc/remoteproc0/trace0
[0][      0.000] Watchdog enabled: TimerBase = 0x68824000 SMP-Core = 0 Freq = 19200000
[0][      0.000] Watchdog enabled: TimerBase = 0x68826000 SMP-Core = 1 Freq = 19200000
[0][      0.000] Watchdog_restore registered as a resume callback
[0][      0.000] 18 Resource entries at 0x3000
[0][      0.000] messageq_single.c:main: MultiProc id = 2
[0][      0.000] Time at reset() is 51615 ticks
[0][      0.000] Time at startup()  is 51726 ticks
[0][      0.000] Time at main()  is 51804 ticks
[0][      0.000] registering rpmsg-proto:rpmsg-proto service on 61 with HOST
[0][      0.000] tsk1Fxn: created MessageQ: SLAVE_IPU1; QueueID: 0x20080
[0][      0.000] Awaiting sync message from host...

But we are not able to see the trace0 entry after integrating these patches.

root@mmt2020-a880:~# ls -l /sys/kernel/debug/remoteproc/remoteproc0/
-r--------    1 root     root             0 Jan  1 00:00 name
-r--------    1 root     root             0 Jan  1 00:00 recovery
-r--------    1 root     root             0 Jan  1 00:00 state
-r--------    1 root     root             0 Jan  1 00:00 version

and state indicate offline

cat /sys/kernel/debug/remoteproc/remoteproc0/state

offline

In normal (no early boot and late attach) case trace0 is available for IPU1

Can you please let us know how we can verify late- attach feature. Any Kernel changes needs to be done to enable trace0 ?

Any help will be appreciated.

Thanks

Sreeju

  • Hi Sreeju,

    I assume you're building Vision-SDK? The link mentioned above is late-attach feature for processor-SDK and not for Vision-SDK.
    As indicated in the below post, there are logs which are available as part of apps.out which will indicate when the remote proc was boot-strapped and if late attach has succeeded you will notice the Vision-SDK menu. If you follow the thread, example logs, clearly demonstrating the difference in time for early-boot and successful late-attach is also demonstrated.
    e2e.ti.com/.../765830

    Regards
    Shravan
  • https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/dtb.7zHi Shravan,

    I am attaching dtb file we are using.

    Regards,

    Sreeju

  • Hi Sreeju,

    Are you building the IPU firmware using Vision-SDK? If yes, you need to late-attach 9(which I notice you're doing), but also set the timer attribute in ipu1 to timer9 and timer11 in the DTB.

    Can you also provide the dmesg logs?

    Regards
    Shravan
  • dmesg_lateattach_logs.txtHi Shravan,

    Yes, building IPU1 firmware using Vision-SDK.

    We will set timer attribute of IPU1 and check

    dmesg log attached

    Regards,

    Sreeju

  • Hi Shravan,

    We have tried with the timer9 and timer11 in the dts for ipu1, still the state indicates offline.

    Regards,
    Sreeju
  • Hi Sreeju,

    Can you confirm your /lib/firmware folder has the dra7-ipu1-fw.xem4 file? This file should match the same firmware being loaded from bootloader (but shouldn't be compressed). Also are the states of all all remoteprocs offline (i.e cat /sys/kernel/debug/remoteproc/*/state is offline for all?). Can you please output the contents of the /lib/firmware contents of your SD card.

    Regards
    Shravan
  • Hi Shravan,

    Please find the inline reply below:

    1. Can you confirm your /lib/firmware folder has the dra7-ipu1-fw.xem4 file? 

    Yes, we have the dra7-ipu1-fw.xem4 binary present in /lib/firmware.

    root@mmt2020-a880:~# ls /lib/firmware/


    bcm89335          dra7-ipu2-fw.xem4.map
    dra7-ipu1-fw.xem4         dra7w.bgz
    dra7-ipu1-fw_old.xem4      mv8887
    dra7-ipu2-fw.xem4      mxt540_DM8.cfg
    dra7-ipu2-fw.xem4.ipumm-fw      mxt641T_SDM8.cfg

    2. Also are the states of all all remoteprocs offline (i.e cat /sys/kernel/debug/remoteproc/*/state is offline for all?

    Yes,all the remoteproc states are shown offline

    root@mmt2020-a880:~# cat /sys/kernel/debug/remoteproc/*/state

    offline (0)

    offline (0)

     

     Regards,

    Sneha

  • Hi Sneha,

    Couple of observations / comments:

    1. In your /lib/firmware folder I don't see DSP firmware, however, from the logs Sreeju sent, I notice that there's an DSP MDMA fault. Are the logs provided by Sreeju (earlier in this thread) consistent with your current observations?

    2. From Sreeju's logs it looks to me like the user-space firmware load fails. This is why you're seeing both remote-cores to be offline. Can you attach the output of the below command run on your target (attach config.txt file):

    zcat /proc/config.gz  > config.txt

    3. Can you revert this patch '0004-config_fragments-Make-remoteproc-built-in-enable-use.patch' and try again?

    Regards

    Shravan

  • config_remotecore_module.txtconfig_remotecore_inbuilt.txt

    Hi Shravan,

    Please find my observations below:

    1. In your /lib/firmware folder I don't see DSP firmware, however, from the logs Sreeju sent, I notice that there's an DSP MDMA fault. Are the logs provided by Sreeju (earlier in this thread) consistent with your current observations?

    The logs shared by Sreeju is consistent with my observations,and we aren't loading the DSP firmware  from /lib/firmware.

    2. From Sreeju's logs it looks to me like the user-space firmware load fails. This is why you're seeing both remote-cores to be offline. Can you attach the output of the below command run on your target (attach config.txt file):

    Actually according to this patch "0004-config_fragments-Make-remoteproc-built-in-enable-use.patch", we had made the remotecore built-in.

    But as suggested by you,I  have reverted the patch.Attaching the previous(config_remotecore_inbuilt) and the reverted(config_remotecore_module) kernel configs.

    As the Remotecore drivers are now loaded as modules,I observed that while booting its loading the firmware again.Is this behavior expected in case of Early boot - Late attach, since it was already loaded by bootloader? And why do we need to load it again?

    [    1.392830]  remoteproc0: powering up 58820000.ipu
    [    1.392845]  remoteproc0: Booting fw image dra7-ipu1-fw.xem4, size 21731188

    Regards,

    Sneha

  • Hello Shravan,


    Below the terminal output of /sbin/vsdkapps

    [HOST] OSA: MEM: 0: Mapped 0xa0100000 to 0xb68d7000 of size 0x00100000
    [HOST] OSA: MEM: 1: Mapped 0x84203000 to 0xb28d7000 of size 0x04000000
    [HOST] OSA: MEM: 2: Mapped 0xa0200000 to 0xb2817000 of size 0x00040000
    [HOST] OSA: MEM: 3: Mapped 0xa02c0000 to 0xb2857000 of size 0x00080000
    [HOST] OSA: MEM: 4: Mapped 0x00000000 to 0x00000000 of size 0x00000000
    [HOST] OSA: IPU1-0 Remote Log Shared Memory @ 0xa0200000
    [HOST] OSA: HOST Remote Log Shared Memory @ 0xa024f140
    ASSERT (system_ipc.c|System_ipcInit|119)
    [HOST] [HOST ] 22.606905 s: SYSTEM: System A15 Init in progress !!!
    [HOST] [HOST ] 22.607027 s: SYSTEM: IPC: Init in progress !!!
    [HOST] [HOST ] 22.607057 s: SYSTEM: IPC: Notify init in progress !!!
    [HOST] [HOST ] 22.607118 s: SYSTEM: IPC: [IPU1-0] socket bind failed (Invalid argument, 22) !!!
    [HOST] [HOST ] 22.607149 s: SYSTEM: IPC: [IPU1-0] Notify RX channel create failed (endpoint = 81) !!!
    [HOST] [HOST ] 22.602848 s: Enter 'e' to exit


    Regards,
    Sreeju
  • Hi Sreeju,

    The error (ASSERT (system_ipc.c|System_ipcInit|119)), could mean the memcache module isn't inserted. Can you run lsmod on your target after running vision_sdk_load.sh. Can you also provide the dmesg logs after reverting the patch mentioned.

    Regards
    Shravan
  • dmesg_lateattch_modules.txt

    Hi  Shravan,

    memcache module is inserted.

    below the lsmod output.

    root@mmt2020-a880:~# lsmod

    Module                  Size  Used by

    vfat                    9929  1

    fat                    56346  1 vfat

    sd_mod                 29404  2

    sd8xxx                460729  0

    cfg80211              475989  1 sd8xxx

    mlan                  400565  1 sd8xxx

    memcache                3386  2

    pvrsrvkm              420510  2

    cryptoloop              2331  0

    loop                   17903  1 cryptoloop

    ti_fpd3_serdes         12665  0

    smsc95xx               24465  0

    smsc75xx               30894  0

    asix                   29524  0

    usbnet                 32885  3 asix,smsc75xx,smsc95xx

    mii                     4959  4 asix,usbnet,smsc75xx,smsc95xx

    usb_storage            48552  1

    scsi_mod              154529  2 usb_storage,sd_mod

    rpmsg_proto             8283  4

    omap_remoteproc        14935  2

    rpmsg_rpc              29517  0

    virtio_rpmsg_bus       14717  2 rpmsg_rpc,rpmsg_proto

    remoteproc             32601  4 omap_remoteproc,virtio_rpmsg_bus,rpmsg_rpc,rpmsg_proto

    virtio                  6417  2 remoteproc,virtio_rpmsg_bus

    virtio_ring            13423  2 remoteproc,virtio_rpmsg_bus

    dwc3                   86589  0

    udc_core               13976  1 dwc3

    dwc3_omap               4636  0

    xhci_plat_hcd           5102  0

    xhci_hcd              175106  1 xhci_plat_hcd

    usbcore               214433  7 asix,usb_storage,xhci_plat_hcd,usbnet,smsc75xx,smsc95xx,xhci_hcd

    usb_common              4358  3 dwc3,udc_core,usbcore

    Attaching dmesg log

    Regards,

    Sreeju

  • Hello Shravan,

    We also tried again with remoteproc built in, but loaded firmware via sysfs

    echo 1 > /sys/class/firmware/dra7-ipu1-fw.xem4/loading
    cat /lib/firmware/dra7-ipu1-fw.xem4 > /sys/class/firmware/dra7-ipu1-fw.xem4/data
    echo 0 > /sys/class/firmware/dra7-ipu1-fw.xem4/loading

    and couldn't see any ipc error with vsdkapps, below the log:

    root@mmt2020-a880:~# /sbin/vsdkapps
    [HOST] OSA: MEM: 0: Mapped 0xa0100000 to 0xb68b7000 of size 0x00100000
    [HOST] OSA: MEM: 1: Mapped 0x84203000 to 0xb28b7000 of size 0x04000000
    [HOST] OSA: MEM: 2: Mapped 0xa0200000 to 0xb27f7000 of size 0x00040000
    [HOST] OSA: MEM: 3: Mapped 0xa02c0000 to 0xb2837000 of size 0x00080000
    [HOST] OSA: MEM: 4: Mapped 0x00000000 to 0x00000000 of size 0x00000000
    [HOST] OSA: IPU1-0 Remote Log Shared Memory @ 0xa0200000
    [HOST] OSA: HOST Remote Log Shared Memory @ 0xa024f140
    [HOST] [HOST ] 110.173122 s: DISP_DIST_SRC_6 : Init done - linkid-0x2000062
    [HOST] [HOST ] 110.173214 s: DISP_DIST_SRC_7 : Init done - linkid-0x2000063
    [HOST] [HOST ] 110.173366 s: ALGORITHM_0 : Init done - linkid-0x2000031
    [HOST] [HOST ] 110.173458 s: ALGORITHM_1 : Init done - linkid-0x2000032
    [HOST] [HOST ] 110.173580 s: ALGORITHM_2 : Init done - linkid-0x2000033
    [HOST] [HOST ] 110.173702 s: ALGORITHM_3 : Init done - linkid-0x2000034
    [HOST] [HOST ] 110.173793 s: ALGORITHM_4 : Init done - linkid-0x2000035
    [HOST] [HOST ] 110.173915 s: ALGORITHM_5 : Init done - linkid-0x2000036
    [HOST] [HOST ] 110.174037 s: ALGORITHM_6 : Init done - linkid-0x2000037
    [HOST] [HOST ] 110.174159 s: ALGORITHM_7 : Init done - linkid-0x2000038
    [HOST] [HOST ] 110.174312 s: DUP0 : Init done - linkid-0x0
    [HOST] [HOST ] 110.174495 s: DUP1 : Init done - linkid-0x0
    [HOST] [HOST ] 110.182608 s: NETWORK_CTRL: Starting Server (port=5000) !!!
    [HOST] [HOST ] 110.182699 s: NETWORK_CTRL: Starting Server ... DONE (port=5000) !!!
    [HOST] [HOST ] 110.183004 s: Enter 'e' to exit
    [HOST] [HOST ] 110.213383 s: IPC_OUT_0 : Create in progress !!!

    Regards,
    Sreeju
  • Hi Sreeju,

    Please use a debugger and step through the _init function as part of omap_hwmod.c file to root-cause the module causing the failure.

    Regards
    Shravan
  • Hello Shravan,

    We have used the debugger and step through the code as you suggested and found the _enable () for "dss_core" is causing the display off. trace is below.

    Display is going off at "_disable_optional_clocks()"

    Below the call traces.

    _disable_optional_clocks
    _enable_sysc
    _enable
    _setup_reset
    _setup
    _omap_hwmod_for_each
    _omap_hwmod_setup_all

    We also compared the file : omap_hwmod_7xx_data.c, found the flag HWMOD_CONTROL_OPT_CLKS_IN_RESET setting for dss in our case. Removed this flag according to the vision sdk change. Now display is not going off.

    Still we are unable to communicate with IPU1 (vsdkapps log output is same as before.)
    We also tried with modetest, there is no error reported, but no pattern got displayed on the screen.

    Can we look in to IPU1, DSS, VPE registers, or configuration specifically that enables A15 to IPU1 communication. ?


    Thanks,
    Sreeju
  • Hi Sreeju,

    Issue pertaining to late-attach is resolved. Closing this thread.

    Regards
    Shravan
  • Hello Shravan,

    Late attach is working with timer3 for IPU1, We have issue, when we are changing timer attribute to timer9 for IPU1, It is not working when we load both IPU1 and IPU2, we are unable to display in this case(it is working when we load IPU1 alone with timer9). Below the currently assigned timer attributes in dts for IPUs

    &ipu2 {
    status = "okay";
    memory-region = <&ipu2_cma_pool>;
    mboxes = <&mailbox6 &mbox_ipu2_ipc3x>;
    timers = <&timer3>;
    /* watchdog-timers = <&timer4>, <&timer9>; */
    };

    &ipu1 {
    status = "okay";
    memory-region = <&ipu1_cma_pool>;
    mboxes = <&mailbox5 &mbox_ipu1_ipc3x>;
    timers = <&timer9>, <&timer11>;
    /* watchdog-timers = <&timer7>, <&timer8>; */e2e.ti.com/.../777231
    };

    Suspect, there could be some conflict between IPU1 and IPU2, when timer9 is used for IPU1. even though timer 9 is not mentioned for IPU2 in dts.
    How we can confirm that IPU2 will not be using timer9 ?, How we can change timer attribute and rebuild the IPU2 firmware ?

    Regards,
    Sreeju
  • Hi Sreeju,

    Can you first halt at bootloader (don't load kernel) and see if your IPU firmware is running? Are you able to modify your firwmare (using VSDK) to use timer3? I realized there were some issues in changing the timer being used in VSDK.

    Can we please create a new thread for this. I will answer on the new thread. Issue with late-attach specifically is resolved.

    Regards
    Shravan
  • Hello Shravan,

    Yes IPU1 firmware is loading from the Bootloader. If I load IPU1 alone, there is no issue, it is working fine.
    Issue is only with below case:
    IPU1 with timer9 load from bootloader, and IPU2 from /lib/firmware (no late attach for IPU2 and its attributes)

    Yes I will create a new thread for this.

    Regards,
    Sreeju