This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5718: AM5718 PCB limitation

Part Number: AM5718

Hi Champs,

I would like to confirm following point

*Previous thread discussion, AM5718 6layer through hole Via has no application note.

 However, 1.5GHz frequency affect higher power consumption for 6layer.

*Do you have any idea to use 1.5GHz operation with 6 layers ?

If this is still difficult,

*Is this possible AM5718@1.5GHz 8layer with  through hole Via (PTH via) ?

*According to this application note, maximum Via hole at 0.8mm pitch is 10mil.

http://www.ti.com/lit/an/spraca4/spraca4.pdf (Table 2. PCB Typical Feature Sizes For Standard (non-Via Channel) BGA Arrays)

If we would like to use 0.3mm (11.8mil) VIA size for 0.8mm pitch package, what kind of concern do you have ?

Regards,

Kz777