This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice/AM3894: IBIS model

Part Number: AM3894
Other Parts Discussed in Thread: TINA-TI, , TMS320DM8168

Tool/software: TINA-TI or Spice Models

Hi,

Can anybody tell me if IBIS model for AM3894 is available or not? If not will TI provide it?

Thanks.

Nilam

  • Hi Nilam,

    This is an older part. It will take me a little time to check and see if the IBIS is available.

    Regards, Bill

  • Hi Bill,
    Please update me, if you get it. Actually it's PCIe IBIS model is required.

    Thanks,
    Nilam
  • Hi Nilam,

    After checking around I found the IBIS model for the TMS320DM8168 can be used to simulate the AM3894. Some of the pin names are different but the IO characteristics of the same for the two parts. Unfortunately, that PCIE signals are not supported in that model. Support for PCIE serdes signals would require an IBIS AMI model and I don't see that model anywhere in our system. Due to the age of the part, I doubt that it is available. I'm sorry I don't have a better answer for you.

    Regards, Bill