This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3354: boot and programming NAND Flash.

Part Number: AM3354

Our boot configuration is SYSBOOT[4:0] = "10100", which is boot from NAND Flash first and EMAC1 last, with this configuration, 

1. We can program the NAND Flash from or via the network (TFTP server or so) onto a fresh board (or brand new board), right?

2. We should also be able re-program or update the image onto the NAND Flash on a working board afterward, right? 

3. Do we need or or to do any special software for these? 

4. What if we have a board that only have uboot running. Could we still re-program or update the images to the NAND via the network? 

Thank you.