This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5728: Debug dual-camera demo through Qt

Part Number: AM5728

Tool/software: Linux

I have test the dual- camera demo on the Metrix and it worked well. Now, I want to develop a camera project base the dual-camera demo. But, when I debug the project through the Qt, the project shows a error like following:

ERROR:drm_init_dss:840: ret from drmModeAtomicCommit = -13

This is familiar to https://e2e.ti.com/support/processors/f/791/t/692581?tisearch=e2e-sitesearch&keymatch=dual%20camera.

And he remove the the Matrix start up script in rc2.d and run dual camera demo stand alone when the EVM is up to make it woke. And what should I do? If remove the files, which files should I remove?

S01networking         S19nfscommon          S70lighttpd                         
S02dbus-1             S20atd                S87redis-server                     
S03uim-sysfs          S20bluetooth          S90crond                            
S08rc.pvr             S20hwclock.sh         S90snmpd                            
S09weston             S20syslog             S95gdbserverproxy                   
S10dropbear           S20thttpd             S98thermal-zone-init                
S10telnetd            S21avahi-daemon       S99bt-enable.sh                     
S12rpcbind            S30rng-tools          S99gplv3-notice                     
S15mountnfs.sh        S56kdump              S99rmnologin.sh