Part Number: AM4378
Other Parts Discussed in Thread: TPS65218
Tool/software: Linux
Dear sir,
Currently I have a problem to make a right system file . After booting up from the MMC mode, I got the message of ** File not found /boot/zImage **.
So I made a test to decompress the original file, which can correctly boot up from the chip , by typing the command "tar zxvf rootfs.tar.gz".
In the mean time, the file was compressed back to rootfs.tar.gz whithout any change to its original contents by typing the command "tar zcvf rootfs.tar.gz rootfs"
It is found that the size of the new rootfs.tar.gz is a little bit different from its original rootfs.tar.gz (whcih is supposed to be the same, but not).
The original rootfs.tar.gz was then replaced by the new rootfs.tar.gz and made a complete update by typing "./updatesys.sh".
Then the problem of ** File not found /boot/zImage ** was found after booting up from the MMC.
So the problem can be duplicated by decompressing and compressing the system file. Do you have any idea what the problem it is ?