Part Number: PROCESSOR-SDK-AM65X
Tool/software: Linux
Hi.
We have tested the SDK5.3, the Ethernet is still buggy.
please see the below log.
Thanks.
BR Rio
root@am65xx-evm:~# iperf -c 10.1.42.11 -w128K -d -i1 -t5
------------------------------------------------------------
Server listening on TCP port 5001
TCP window size: 256 KByte (WARNING: requested 128 KByte)
------------------------------------------------------------
------------------------------------------------------------
Client connecting to 10.1.42.11, TCP port 5001
TCP window size: 256 KByte (WARNING: requested 128 KByte)
------------------------------------------------------------
[ 5] local 10.1.42.24 port 60964 connected with 10.1.42.11 port 5001
[ 4] local 10.1.42.24 port 5001 connected with 10.1.42.11 port 40121
[ ID] Interval Transfer Bandwidth
[ 5] 0.0- 1.0 sec 3.12 MBytes 26.2 Mbits/sec
[ 4] 0.0- 1.0 sec 92.1 MBytes 773 Mbits/sec
[ 258.844909] skbuff: skb_over_panic: text:ffff0000014e2b54 len:1584 put:1584 head:ffff8008440b5000 data:ffff8008440b5082 tail:0x6b2 end:0x680 dev:eth4
[ 258.858382] ------------[ cut here ]------------
[ 258.862992] kernel BUG at /oe/bld/build-AARCH64_1/arago-tmp-external-linaro-toolchain/work-shared/am65xx-evm/kernel-source/net/core/skbuff.c:104!
[ 258.876009] Internal error: Oops - BUG: 0 [#1] PREEMPT SMP
[ 258.881482] Modules linked in: sha512_arm64 md5 des_generic cbc xhci_plat_hcd xhci_hcd usbcore rpmsg_proto virtio_rpmsg_bus rpmsg_core xfrm_user dwc3 udc_core usb_common ti_am335x_adc kfifo_buf xfrm4_tunnel tunnel4 ipcomp xfrm_ipcomp esp4 ah4 af_key xfrm_algo ti_k3_r5_remoteproc pruss_soc_bus pvrsrvkm(O) pci_endpoint_test m_can dwc3_of_simple omap_rng phy_omap_usb2 rng_core sa2ul can_dev ti_am335x_tscadc at24 authenc icssg_prueth pru_rproc pruss pruss_intc remoteproc crc32_ce gpio_decoder crct10dif_ce input_polldev sch_fq_codel cryptodev(O) ipv6
[ 258.929835] CPU: 0 PID: 0 Comm: swapper/0 Tainted: G O 4.14.79-ge669d52447 #1
[ 258.938079] Hardware name: Texas Instruments AM654 Base Board (DT)
[ 258.944246] task: ffff000008b3b280 task.stack: ffff000008b00000
[ 258.950162] PC is at skb_panic+0x48/0x50
[ 258.954075] LR is at skb_panic+0x48/0x50
[ 258.957987] pc : [<ffff000008683c38>] lr : [<ffff000008683c38>] pstate: 20000145
[ 258.965363] sp : ffff00000800fd80
[ 258.968666] x29: ffff00000800fd90 x28: ffff0000087e0110
[ 258.973968] x27: ffff800841ffd9c0 x26: ffff8008443ee500
[ 258.979269] x25: ffff800845c5c200 x24: ffff800841ffdaf0
[ 258.984571] x23: 0000000000000040 x22: 0000000000000630
[ 258.989872] x21: ffff800841ffd900 x20: ffff800841ffd000
[ 258.995173] x19: 0000000000000000 x18: 0000000000000010
[ 259.000474] x17: 0000ffff9f140810 x16: ffff00000867cf20
[ 259.005776] x15: ffffffffffffffff x14: 30383678303a646e
[ 259.011077] x13: 652032623678303a x12: ffff000008b33a30
[ 259.016378] x11: ffff000008478a98 x10: 38666666663a6174
[ 259.021680] x9 : 0000000000000016 x8 : 3034343830303866
[ 259.026981] x7 : 6666663a64616568 x6 : 00000000000001c2
[ 259.032284] x5 : 0000000000000001 x4 : 0000000000000004
[ 259.037584] x3 : 0000000000000000 x2 : 0000000000000040
[ 259.042885] x1 : ffff000008b3b280 x0 : 0000000000000089
[ 259.048189] Process swapper/0 (pid: 0, stack limit = 0xffff000008b00000)
[ 259.054873] Call trace:
[ 259.057314] Exception stack(0xffff00000800fc40 to 0xffff00000800fd80)
[ 259.063743] fc40: 0000000000000089 ffff000008b3b280 0000000000000040 0000000000000000
[ 259.071557] fc60: 0000000000000004 0000000000000001 00000000000001c2 6666663a64616568
[ 259.079370] fc80: 3034343830303866 0000000000000016 38666666663a6174 ffff000008478a98
[ 259.087184] fca0: ffff000008b33a30 652032623678303a 30383678303a646e ffffffffffffffff
[ 259.094997] fcc0: ffff00000867cf20 0000ffff9f140810 0000000000000010 0000000000000000
[ 259.102810] fce0: ffff800841ffd000 ffff800841ffd900 0000000000000630 0000000000000040
[ 259.110625] fd00: ffff800841ffdaf0 ffff800845c5c200 ffff8008443ee500 ffff800841ffd9c0
[ 259.118439] fd20: ffff0000087e0110 ffff00000800fd90 ffff000008683c38 ffff00000800fd80
[ 259.126253] fd40: ffff000008683c38 0000000020000145 ffff0000014e2b54 0000000000000630
[ 259.134067] fd60: 0000ffffffffffff ffff8008440b5000 ffff00000800fd90 ffff000008683c38
[ 259.141881] [<ffff000008683c38>] skb_panic+0x48/0x50
[ 259.146835] [<ffff000008685b20>] pskb_put+0x0/0x38
[ 259.151647] [<ffff0000014e2b54>] emac_napi_rx_poll+0x1b4/0x2b0 [icssg_prueth]
[ 259.158772] [<ffff00000869df54>] net_rx_action+0xf4/0x2b0
[ 259.164162] [<ffff0000080811ec>] __do_softirq+0x12c/0x228
[ 259.169551] [<ffff0000080acd10>] irq_exit+0xc8/0xf8
[ 259.174421] [<ffff0000080fd8c0>] __handle_domain_irq+0x60/0xb0
[ 259.180242] [<ffff000008080fc4>] gic_handle_irq+0x7c/0x178
[ 259.185715] Exception stack(0xffff000008b0fdf0 to 0xffff000008b0ff30)
[ 259.192141] fde0: 0000000000000000 00008008773c0000
[ 259.199954] fe00: 0000000000000000 ffff000008af3930 ffff000008af3908 ffff000008b0ff20
[ 259.207769] fe20: 00008008773c0000 0000000000000000 0000000000000002 ffff000008b0feb0
[ 259.215582] fe40: 0000000000000920 0000000000000001 000000396684b913 0000000000000000
[ 259.223396] fe60: 002bcca204681cc1 0000560bf0616fcb ffff00000867cf20 0000ffff9f140810
[ 259.231210] fe80: 000000000000010f ffff000008b33ac4 ffff000008b33a30 ffff000008af0018
[ 259.239023] fea0: ffff000008b3b280 ffff80087ffff480 ffff000008ae0028 0000000000000000
[ 259.246837] fec0: 00000000ffef3ce0 0000000000000400 0000000080a90018 ffff000008b0ff30
[ 259.254650] fee0: ffff000008084e2c ffff000008b0ff30 ffff000008084e30 0000000060000145
[ 259.262465] ff00: 0000000000000000 00000000ffef3ce0 ffffffffffffffff ffff000008123f84
[ 259.270278] ff20: ffff000008b0ff30 ffff000008084e30
[ 259.275145] [<ffff000008082a30>] el1_irq+0xb0/0x124
[ 259.280013] [<ffff000008084e30>] arch_cpu_idle+0x10/0x18
[ 259.285313] [<ffff0000080e5ee0>] do_idle+0xd8/0x118
[ 259.290180] [<ffff0000080e60b4>] cpu_startup_entry+0x24/0x28
[ 259.295831] [<ffff00000879621c>] rest_init+0xcc/0xd8
[ 259.300792] [<ffff000008a90b50>] start_kernel+0x378/0x38c
[ 259.306183] Code: a90023eb aa0a03e1 912f6120 97e9e357 (d4210000)
[ 259.312271] ---[ end trace 3026f6f051d27fb8 ]---
[ 259.316877] Kernel panic - not syncing: Fatal exception in interrupt
[ 259.323216] SMP: stopping secondary CPUs
[ 259.327139] Kernel Offset: disabled
[ 259.330618] CPU features: 0x080200c
[ 259.334096] Memory Limit: none
[ 259.337144] ---[ end Kernel panic - not syncing: Fatal exception in interrupt