HI TI team,
Regarding power calculations for your SMV320C6727B-SP part, I notice for CVDD typical power is listed at 800 mA. I inputted your conditions as it states in note 2 of the datasheet into your power calculator spreadsheet for this part and get 568 mA for CVDD. I think this is because the calculator I have is for your commercial part. Is there a correlation to this commercial spreadsheet to your space qualified part?
Also what you have listed is a typical power in the datasheet. I'm interested in what would be the max continuous for operations if that is available for CVDD and DVDD? As of right now for max continuous I'm adding 30% to typical numbers of the spreadsheet after i scale it to the space parts 800 mA CVDD and 76 mA DVDD and am hoping for a more accurate approach.
Regards,
Will S.